This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: eMMC boot display issue

Part Number: AM5728

Tool/software: Linux

The system on the SD card displays normal.

But when we burn the system to eMMC, then boot from eMMC, the screen displayed Please wait... all the time.

Then executed the following instructions:

/etc/init.d/weston restart

/etc/init.d/matrix-gui-2.0 start

It can be displayed normally.

The version of SDK we used is 03.01.00.06

  • Hello zhengguang,

    For some reason SystemD doesn't start weson while booting from eMMC. Can you attach the complete bootlog too see why?

    Best regards,
    Kemal

  • Hi Kemal:

    bootlog as follow:

    [    0.000000] Booting Linux on physical CPU 0x0
    [    0.000000] Initializing cgroup subsys cpuset
    [    0.000000] Initializing cgroup subsys cpu
    [    0.000000] Initializing cgroup subsys cpuacct
    [    0.000000] Linux version 4.4.19-gf3417ba1aa (adv@45a80431ff1b) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #1 SMP PREEMPT Thu Dec 21 15:43:40 UTC 2017
    [    0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
    [    0.000000] Machine model: TI AM5728 ROM7510
    [    0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
    [    0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
    [    0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x000000009d000000, size 32 MiB
    [    0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x000000009f000000, size 8 MiB
    [    0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
    [    0.000000] cma: Reserved 24 MiB at 0x00000000fd400000
    [    0.000000] Forcing write-allocate cache policy for SMP
    [    0.000000] Memory policy: Data cache writealloc
    [    0.000000] OMAP4: Map 0x00000000fed00000 to fe600000 for dram barrier
    [    0.000000] DRA752 ES2.0
    [    0.000000] PERCPU: Embedded 11 pages/cpu @eed55000 s14848 r8192 d22016 u45056
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 468544
    [    0.000000] Kernel command line: console=ttyS2,115200n8 root=PARTUUID=1974817f-02 rw rootfstype=ext4 rootwait
    [    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
    [    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
    [    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
    [    0.000000] Memory: 1664316K/1881088K available (6759K kernel code, 302K rwdata, 2376K rodata, 332K init, 289K bss, 28356K reserved, 188416K cma-reserved, 1266688K highmem)
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    [    0.000000]     vmalloc : 0xf0800000 - 0xff800000   ( 240 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xf0000000   ( 768 MB)
    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
    [    0.000000]       .text : 0xc0008000 - 0xc08f409c   (9137 kB)
    [    0.000000]       .init : 0xc08f5000 - 0xc0948000   ( 332 kB)
    [    0.000000]       .data : 0xc0948000 - 0xc09939d0   ( 303 kB)
    [    0.000000]        .bss : 0xc0995000 - 0xc09dd5c8   ( 290 kB)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
    [    0.000000] Preemptible hierarchical RCU implementation.
    [    0.000000]  Build-time adjustment of leaf fanout to 32.
    [    0.000000] NR_IRQS:16 nr_irqs:16 16
    [    0.000000] OMAP clockevent source: timer1 at 32786 Hz
    [    0.000000] Architected cp15 timer(s) running at 6.14MHz (virt).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
    [    0.000004] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
    [    0.000015] Switching to timer-based delay loop, resolution 162ns
    [    0.000337] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
    [    0.000345] OMAP clocksource: 32k_counter at 32768 Hz
    [    0.000760] Console: colour dummy device 80x30
    [    0.000782] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
    [    0.000796] pid_max: default: 32768 minimum: 301
    [    0.000888] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.000899] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.001439] Initializing cgroup subsys io
    [    0.001456] Initializing cgroup subsys memory
    [    0.001479] Initializing cgroup subsys devices
    [    0.001492] Initializing cgroup subsys freezer
    [    0.001503] Initializing cgroup subsys perf_event
    [    0.001514] Initializing cgroup subsys pids
    [    0.001538] CPU: Testing write buffer coherency: ok
    [    0.001738] /cpus/cpu@0 missing clock-frequency property
    [    0.001755] /cpus/cpu@1 missing clock-frequency property
    [    0.001764] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    [    0.001802] Setting up static identity map for 0x800082c0 - 0x80008318
    [    0.080086] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
    [    0.080148] Brought up 2 CPUs
    [    0.080161] SMP: Total of 2 processors activated (24.59 BogoMIPS).
    [    0.080167] CPU: All CPU(s) started in SVC mode.
    [    0.080539] devtmpfs: initialized
    [    0.107840] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
    [    0.108799] omap_hwmod: l3_main_2 using broken dt data from ocp
    [    0.219913] omap_hwmod: dcan2: _wait_target_disable failed
    [    0.314503] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    [    0.318378] pinctrl core: initialized pinctrl subsystem
    [    0.319230] NET: Registered protocol family 16
    [    0.320141] DMA: preallocated 256 KiB pool for atomic coherent allocations
    [    0.350240] cpuidle: using governor ladder
    [    0.380265] cpuidle: using governor menu
    [    0.389497] OMAP GPIO hardware version 0.1
    [    0.396006] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
    [    0.423043] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
    [    0.423054] hw-breakpoint: maximum watchpoint size is 8 bytes.
    [    0.423514] omap4_sram_init:Unable to allocate sram needed to handle errata I688
    [    0.423523] omap4_sram_init:Unable to get sram pool needed to handle errata I688
    [    0.424104] OMAP DMA hardware revision 0.0
    [    0.454582] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver
    [    0.455741] edma 43300000.edma: memcpy is disabled
    [    0.460601] edma 43300000.edma: TI EDMA DMA engine driver
    [    0.464376] omap-iommu 40d01000.mmu: 40d01000.mmu registered
    [    0.464563] omap-iommu 40d02000.mmu: 40d02000.mmu registered
    [    0.464720] omap-iommu 58882000.mmu: 58882000.mmu registered
    [    0.464872] omap-iommu 55082000.mmu: 55082000.mmu registered
    [    0.465152] omap-iommu 41501000.mmu: 41501000.mmu registered
    [    0.465330] omap-iommu 41502000.mmu: 41502000.mmu registered
    [    0.468261] palmas 0-0058: Irq flag is 0x00000008
    [    0.481878] palmas 0-0058: Muxing GPIO ff, PWM 0, LED 0
    [    0.561760] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
    [    0.562377] omap_i2c 48060000.i2c: bus 2 rev0.12 at 100 kHz
    [    0.562743] omap_i2c 4807a000.i2c: bus 3 rev0.12 at 100 kHz
    [    0.563219] omap_i2c 4807c000.i2c: bus 4 rev0.12 at 100 kHz
    [    0.563425] media: Linux media interface: v0.10
    [    0.563477] Linux video capture interface: v2.00
    [    0.563518] pps_core: LinuxPPS API ver. 1 registered
    [    0.563525] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.563553] PTP clock support registered
    [    0.563601] EDAC MC: Ver: 3.0.0
    [    0.564357] omap-mailbox 4883c000.mailbox: omap mailbox rev 0x400
    [    0.564644] omap-mailbox 4883e000.mailbox: omap mailbox rev 0x400
    [    0.564933] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
    [    0.565225] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
    [    0.565557] Advanced Linux Sound Architecture Driver Initialized.
    [    0.566068] Bluetooth: Core ver 2.21
    [    0.566101] NET: Registered protocol family 31
    [    0.566108] Bluetooth: HCI device and connection manager initialized
    [    0.566121] Bluetooth: HCI socket layer initialized
    [    0.566135] Bluetooth: L2CAP socket layer initialized
    [    0.566167] Bluetooth: SCO socket layer initialized
    [    0.566496] clocksource: Switched to clocksource arch_sys_counter
    [    0.577041] NET: Registered protocol family 2
    [    0.577534] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
    [    0.577597] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
    [    0.577722] TCP: Hash tables configured (established 8192 bind 8192)
    [    0.577768] UDP hash table entries: 512 (order: 2, 16384 bytes)
    [    0.577799] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
    [    0.577940] NET: Registered protocol family 1
    [    0.578204] RPC: Registered named UNIX socket transport module.
    [    0.578213] RPC: Registered udp transport module.
    [    0.578220] RPC: Registered tcp transport module.
    [    0.578226] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.579279] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
    [    0.581707] futex hash table entries: 512 (order: 3, 32768 bytes)
    [    0.589511] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.590166] NFS: Registering the id_resolver key type
    [    0.590200] Key type id_resolver registered
    [    0.590208] Key type id_legacy registered
    [    0.590275] ntfs: driver 2.1.32 [Flags: R/O].
    [    0.591949] bounce: pool size: 64 pages
    [    0.592104] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248)
    [    0.592118] io scheduler noop registered
    [    0.592128] io scheduler deadline registered
    [    0.592160] io scheduler cfq registered (default)
    [    0.597697] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
    [    0.601721] PCI host bridge /ocp/axi@0/pcie@51000000 ranges:
    [    0.601732]   No bus range found for /ocp/axi@0/pcie@51000000, using [bus 00-ff]
    [    0.601764]    IO 0x20003000..0x20012fff -> 0x00000000
    [    0.601785]   MEM 0x20013000..0x2fffffff -> 0x20013000
    [    0.632395] dra7-pcie 51000000.pcie: link is not up
    [    0.632570] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
    [    0.632583] pci_bus 0000:00: root bus resource [bus 00-ff]
    [    0.632593] pci_bus 0000:00: root bus resource [io  0x0000-0xffff]
    [    0.632603] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
    [    0.633007] PCI: bus0: Fast back to back transfers disabled
    [    0.633129] PCI: bus1: Fast back to back transfers enabled
    [    0.633179] irq: no irq domain found for /ocp/axi@0/pcie@51000000/interrupt-controller !
    [    0.633212] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
    [    0.633226] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
    [    0.633237] pci 0000:00:00.0: PCI bridge to [bus 01]
    [    0.633457] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
    [    0.634020] PCI host bridge /ocp/axi@1/pcie@51800000 ranges:
    [    0.634029]   No bus range found for /ocp/axi@1/pcie@51800000, using [bus 00-ff]
    [    0.634061]    IO 0x30003000..0x30012fff -> 0x00000000
    [    0.634081]   MEM 0x30013000..0x3fffffff -> 0x30013000
    [    0.666058] dra7-pcie 51800000.pcie: link is not up
    [    0.666232] dra7-pcie 51800000.pcie: PCI host bridge to bus 0001:00
    [    0.666244] pci_bus 0001:00: root bus resource [bus 00-ff]
    [    0.666256] pci_bus 0001:00: root bus resource [io  0x10000-0x1ffff] (bus address [0x0000-0xffff])
    [    0.666265] pci_bus 0001:00: root bus resource [mem 0x30013000-0x3fffffff]
    [    0.666676] PCI: bus0: Fast back to back transfers disabled
    [    0.666795] PCI: bus1: Fast back to back transfers enabled
    [    0.666841] irq: no irq domain found for /ocp/axi@0/pcie@51000000/interrupt-controller !
    [    0.666876] irq: no irq domain found for /ocp/axi@1/pcie@51800000/interrupt-controller !
    [    0.666902] pci 0001:00:00.0: BAR 0: assigned [mem 0x30100000-0x301fffff]
    [    0.666917] pci 0001:00:00.0: BAR 1: assigned [mem 0x30020000-0x3002ffff]
    [    0.666928] pci 0001:00:00.0: PCI bridge to [bus 01]
    [    0.667140] pcieport 0001:00:00.0: Signaling PME through PCIe PME interrupt
    [    0.668498] backlight supply power not found, using dummy regulator
    [    0.728838] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
    [    0.732122] console [ttyS2] disabled
    [    0.732173] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 303, base_baud = 3000000) is a 8250
    [    1.820494] console [ttyS2] enabled
    [    1.824860] 4806e000.serial: ttyS3 at MMIO 0x4806e000 (irq = 304, base_baud = 3000000) is a 8250
    [    1.834537] 48066000.serial: ttyS4 at MMIO 0x48066000 (irq = 305, base_baud = 3000000) is a 8250
    [    1.844658] [drm] Initialized drm 1.1.0 20060810
    [    1.851388] OMAP DSS rev 6.1
    [    1.855140] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
    [    1.863635] omapdss_dss 58000000.dss: bound 58040000.encoder (ops hdmi5_component_ops)
    [    1.873063] ch7055_init
    [    1.881568] loop: module loaded
    [    1.887408] spi spi1.1: not using DMA for McSPI (-19)
    [    1.893826] m25p80 spi32766.0: found w25q32, expected w25q128
    [    1.899624] m25p80 spi32766.0: w25q32 (4096 Kbytes)
    [    1.906439] libphy: Fixed MDIO Bus: probed
    [    1.911111] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.3.0-k
    [    1.918118] igb: Copyright (c) 2007-2014 Intel Corporation.
    [    1.966527] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
    [    1.972652] davinci_mdio 48485000.mdio: detected phy mask ffffffef
    [    1.981362] libphy: 48485000.mdio: probed
    [    1.985391] davinci_mdio 48485000.mdio: phy[4]: device 48485000.mdio:04, driver Atheros 8035 ethernet
    [    1.995316] cpsw 48484000.ethernet: Detected MACID = 00:04:9f:01:30:e0
    [    2.002736] PPP generic driver version 2.4.2
    [    2.007244] PPP BSD Compression module registered
    [    2.011974] PPP Deflate Compression module registered
    [    2.017106] PPP MPPE Compression module registered
    [    2.021926] NET: Registered protocol family 24
    [    2.027306] mousedev: PS/2 mouse device common for all mice
    [    2.049259] rtc-s35390a 2-0030: rtc core: registered rtc-s35390a as rtc0
    [    2.056040] i2c /dev entries driver
    [    2.077173] i2c i2c-4: Added multiplexed i2c bus 5
    [    2.082413] i2c i2c-4: Added multiplexed i2c bus 6
    [    2.089545] pca953x 7-0022: interrupt support not compiled in
    [    2.095351] i2c i2c-4: Added multiplexed i2c bus 7
    [    2.100465] i2c i2c-4: Added multiplexed i2c bus 8
    [    2.105279] pca954x 4-0070: registered 4 multiplexed busses for I2C switch pca9545
    [    2.114619] lm75 0-0048: hwmon0: sensor 'tmp112'
    [    2.246519] adv-wdt-i2c 2-0029: Advantech Watchdog Timer enabled. timeout=60s (nowayout=0), Ver.17
    [    2.256568] omap_hsmmc 4809c000.mmc: Got CD GPIO
    [    2.297211] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
    [    2.304656] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
    [    2.313223] vdd_3v3: supplied by regen1
    [    2.360992] ledtrig-cpu: registered to indicate activity on CPUs
    [    2.369272] aic_dvdd_fixed: supplied by vdd_3v3
    [    2.379452] NET: Registered protocol family 10
    [    2.394637] sit: IPv6 over IPv4 tunneling driver
    [    2.399911] NET: Registered protocol family 17
    [    2.404508] Bluetooth: RFCOMM TTY layer initialized
    [    2.409465] Bluetooth: RFCOMM socket layer initialized
    [    2.414691] Bluetooth: RFCOMM ver 1.11
    [    2.418542] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
    [    2.423880] Bluetooth: BNEP filters: protocol multicast
    [    2.429150] Bluetooth: BNEP socket layer initialized
    [    2.434157] mmc1: MAN_BKOPS_EN bit is not set
    [    2.438569] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
    [    2.444544] Bluetooth: HIDP socket layer initialized
    [    2.449795] Key type dns_resolver registered
    [    2.454200] omap_voltage_late_init: Voltage driver support not added
    [    2.461195] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
    [    2.467457] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
    [    2.473890] mmc1: new DDR MMC card at address 0001
    [    2.479239] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
    [    2.485450] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
    [    2.489236] mmcblk0: mmc1:0001 Q2J55L 7.09 GiB
    [    2.489490] mmcblk0boot0: mmc1:0001 Q2J55L partition 1 16.0 MiB
    [    2.499743] mmcblk0boot1: mmc1:0001 Q2J55L partition 2 16.0 MiB
    [    2.503736]  mmcblk0: p1 p2 p3 p4 < p5 p6 >
    [    2.514331] Power Management for TI OMAP4+ devices.
    [    2.519455] Registering SWP/SWPB emulation handler
    [    2.526148] dmm 4e000000.dmm: initialized all PAT entries
    [    2.549296] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [    2.555939] [drm] No driver support for vblank timestamp query.
    [    2.830329] [drm] Enabling DMM ywrap scrolling
    [    2.881267] Console: switching to colour frame buffer device 240x67
    [    2.903535] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
    [    2.936858] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0
    [    2.954862] asoc-simple-card sound@0: tlv320aic3x-hifi <-> 48468000.mcasp mapping ok
    [    2.965088] input: gpio_keys as /devices/platform/gpio_keys/input/input0
    [    2.973355] rtc-s35390a 2-0030: setting system clock to 2018-01-19 16:53:45 UTC (1516380825)
    [    2.993777] aic_dvdd_fixed: disabling
    [    2.997683] ldousb: disabling
    [    3.001141] ALSA device list:
    [    3.004122]   #0: BeagleBoard-X15
    [    3.211243] EXT4-fs (mmcblk0p2): recovery complete
    [    3.216335] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    [    3.224518] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [    3.232516] devtmpfs: mounted
    [    3.235696] Freeing unused kernel memory: 332K (c08f5000 - c0948000)
    [    3.242099] This architecture does not have kernel memory protection.
    [    3.379846] random: systemd: uninitialized urandom read (16 bytes read, 26 bits of entropy available)
    [    3.391338] random: systemd: uninitialized urandom read (16 bytes read, 26 bits of entropy available)
    [    3.402778] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
    [    3.421262] systemd[1]: Detected architecture arm.
    
    Welcome to Arago 2016.08!
    
    [    3.447103] systemd[1]: Set hostname to <am57xxrom7510a2>.
    [    3.508696] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 28 bits of entropy available)
    [    3.531478] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 28 bits of entropy available)
    [    3.541892] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 28 bits of entropy available)
    [    3.553885] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 29 bits of entropy available)
    [    3.576893] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 30 bits of entropy available)
    [    3.591106] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 31 bits of entropy available)
    [    3.634950] random: systemd: uninitialized urandom read (16 bytes read, 33 bits of entropy available)
    [    3.644447] random: systemd: uninitialized urandom read (16 bytes read, 33 bits of entropy available)
    [    3.881346] systemd[1]: Configuration file /etc/systemd/system/multi-user.target.wants/ota-start.service is marked executable. Please remove executable permission bits. Proceeding anyway.
    [    3.954049] systemd[1]: sysinit.target: Found ordering cycle on sysinit.target/start
    [    3.961886] systemd[1]: sysinit.target: Found dependency on alignment.service/start
    [    3.969608] systemd[1]: sysinit.target: Found dependency on basic.target/start
    [    3.976921] systemd[1]: sysinit.target: Found dependency on sysinit.target/start
    [    3.984357] systemd[1]: sysinit.target: Breaking ordering cycle by deleting job alignment.service/start
    [    3.993818] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with sysinit.target/start
    [ SKIP ] Ordering cycle found, skipping alignment.service
    [    4.029000] systemd[1]: Reached target Remote File Systems.
    [  OK  ] Reached target Remote File Systems.
    [    4.046876] systemd[1]: Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Network Service Netlink Socket.
    [    4.076893] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [  OK  ] Started Forward Password Requests to Wall Directory Watch.
    [    4.107926] systemd[1]: Created slice System Slice.
    [  OK  ] Created slice System Slice.
    [    4.127260] systemd[1]: Created slice system-serial\x2dgetty.slice.
    [  OK  ] Created slice system-serial\x2dgetty.slice.
    [    4.147209] systemd[1]: Created slice User and Session Slice.
    [  OK  ] Created slice User and Session Slice.
    [    4.166641] systemd[1]: Reached target Swap.
    [  OK  ] Reached target Swap.
    [    4.186655] systemd[1]: Reached target Slices.
    [  OK  ] Reached target Slices.
    [    4.206737] systemd[1]: Listening on Syslog Socket.
    [  OK  ] Listening on Syslog Socket.
    [    4.226743] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
    [  OK  ] Listening on /dev/initctl Compatibility Named Pipe.
    [    4.256735] systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    [    4.276686] systemd[1]: Listening on udev Kernel Socket.
    [  OK  ] Listening on udev Kernel Socket.
    [    4.305062] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
    [  OK  ] Started Dispatch Password Requests to Console Directory Watch.
    [    4.336656] systemd[1]: Reached target Paths.
    [  OK  ] Reached target Paths.
    [    4.357274] systemd[1]: Created slice system-getty.slice.
    [  OK  ] Created slice system-getty.slice.
    [    4.376722] systemd[1]: Listening on Journal Socket (/dev/log).
    [  OK  ] Listening on Journal Socket (/dev/log).
    [    4.396796] systemd[1]: Listening on Journal Socket.
    [  OK  ] Listening on Journal Socket.
    [    4.446733] systemd[1]: Mounting Temporary Directory...
             Mounting Temporary Directory...
    [    4.470524] systemd[1]: Starting Load Kernel Modules...
             Starting Load Kernel Modules...
    [    4.483898] CMEMK module: reference Linux version 4.4.19
    [    4.489973] allocated heap buffer 0x40500000 of size 0x100000
    [    4.495765] cmemk initialized
    [    4.501467] systemd[1]: Mounting POSIX Message Queue File System...
             Mounting POSIX Message Queue File System...
    [    4.521009] cryptodev: driver 1.8 loaded.
    [    4.529346] systemd[1]: Starting Remount Root and Kernel File Systems...
             Starting Remount Root and Kernel File Systems...
    [    4.547299] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
    [    4.559022] systemd[1]: Mounting Debug File System...
             Mounting Debug File System...
    [    4.588939] systemd[1]: Starting Journal Service...
             Starting Journal Service...
    [    4.609207] systemd[1]: Starting Create list of required static device nodes for the current kernel...
             Starting Create list of required st... nodes for the current kernel...
    [    4.648845] systemd[1]: Starting Setup Virtual Console...
             Starting Setup Virtual Console...
    [    4.683078] systemd[1]: Mounted Debug File System.
    [  OK  ] Mounted Debug File System.
    [    4.706851] systemd[1]: Mounted POSIX Message Queue File System.
    [  OK  ] Mounted POSIX Message Queue File System.
    [    4.726718] systemd[1]: Mounted Temporary Directory.
    [  OK  ] Mounted Temporary Directory.
    [    4.746883] systemd[1]: Started Journal Service.
    [  OK  ] Started Journal Service.
    [  OK  ] Started Load Kernel Modules.
    [  OK  ] Started Remount Root and Kernel File Systems.
    [  OK  ] Started Create list of required sta...ce nodes for the current kernel.
    [  OK  ] Started Setup Virtual Console.
             Starting Create Static Device Nodes in /dev...
             Starting udev Coldplug all Devices...
             Starting Apply Kernel Variables...
             Starting Flush Journal to Persistent Storage...
    [  OK  ] Started Create Static Device Nodes in /dev.
    [  OK  ] Started Apply Kernel Variables.
    [    5.367408] systemd-journald[146]: Received request to flush runtime journal from PID 1
    [  OK  ] Started Flush Journal to Persistent Storage.
             Starting udev Kernel Device Manager...
    [  OK  ] Reached target Local File Systems (Pre).
             Mounting /media/ram...
             Mounting /var/volatile...
    [  OK  ] Mounted /var/volatile.
    [  OK  ] Mounted /media/ram.
    [  OK  ] Started udev Kernel Device Manager.
    [    5.715979] omap-rproc 58820000.ipu: assigned reserved memory node ipu1_cma@9d000000
    [    5.756638]  remoteproc0: 58820000.ipu is available
    [    5.771857]  remoteproc0: Note: remoteproc is still under development and considered experimental.
    [    5.783781]  remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yetguaranteed.
    [  OK  ] Started udev Coldplug all Devices.
    [    5.795806] omap-rproc 55020000.ipu: assigned reserved memory node ipu2_cma@95800000
    [    5.808749]  remoteproc1: 55020000.ipu is available
    [    5.815534]  remoteproc1: Note: remoteproc is still under development and considered experimental.
    [    5.824887]  remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [    5.858293] omap-rproc 40800000.dsp: assigned reserved memory node dsp1_cma@99000000
    [    5.877710]  remoteproc2: 40800000.dsp is available
    [    5.888103]  remoteproc2: Note: remoteproc is still under development and considered experimental.
             Starting Load/Save Random Seed...
    [    5.920344]  remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [    5.954750] omap-rproc 41000000.dsp: assigned reserved memory node dsp2_cma@9f000000
    [  OK  ] Found device /dev/ttyS2.
    [    5.980713]  remoteproc3: 41000000.dsp is available
    [  OK  ] Started Load/Save Random Seed.
    [    6.005812]  remoteproc3: Note: remoteproc is still under development and considered experimental.
    [    6.037770]  remoteproc3: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [    6.057120]  remoteproc0: registered virtio0 (type 7)
    [    6.149910]  remoteproc1: registered virtio1 (type 7)
    [    6.180395] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
    [    6.191061] CAN device driver interface
    [    6.228187] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
    [    6.273142] c_can_platform 48480000.can: c_can_platform device registered (regs=fa480000, irq=361)
    [    6.360159] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin
    [    6.440307] watchdog: OMAP Watchdog: cannot register miscdev on minor=130 (err=-16).
    [    6.452061] watchdog: OMAP Watchdog: a legacy watchdog module is probably present.
    [    6.463711] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
    [    6.499538] SCSI subsystem initialized
    [    6.510420] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
    [    6.519548] ti-pruss 4b200000.pruss: creating PRU cores and other child platform devices
    [    6.529082] irq: no irq domain found for /ocp/pruss@4b200000/intc@4b220000 !
    [    6.537551] irq: no irq domain found for /ocp/pruss@4b200000/intc@4b220000 !
    [    6.545542] ti-pruss 4b280000.pruss: creating PRU cores and other child platform devices
    [    6.557132] irq: no irq domain found for /ocp/pruss@4b280000/intc@4b2a0000 !
    [    6.565172] irq: no irq domain found for /ocp/pruss@4b280000/intc@4b2a0000 !
    [    6.579638] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
    [    6.586225] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
    [    6.606746] vpe 489d0000.vpe: Device registered as /dev/video0
    [    6.628070]  remoteproc4: 4b234000.pru0 is available
    [    6.639872]  remoteproc4: Note: remoteproc is still under development and considered experimental.
    [    6.654614] ahci 4a140000.sata: SSS flag set, parallel bus scan disabled
    [    6.672643] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
    [    6.687701]  remoteproc4: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [    6.701576] ahci 4a140000.sata: flags: 64bit ncq sntf stag pm led clo only pmp pio slum part ccc apst
    [    6.728351] scsi host0: ahci
    [    6.733292] omap-hdmi-audio omap-hdmi-audio.0.auto: snd-soc-dummy-dai <-> 58040000.encoder mapping ok
    [    6.745339] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 352
    [    6.772513] [drm] Initialized pvr 1.14.3699939 20110701 on minor 1
    [    6.779090]  remoteproc4: registered virtio2 (type 7)
    [    6.784211] pru-rproc 4b234000.pru0: PRU rproc node /ocp/pruss@4b200000/pru0@4b234000 probed successfully
    [  OK  ] Created slice system-systemd\x2dbacklight.sli[    6.805699]  remoteproc5: 4b238000.pru1 is available
    ce.
    [    6.819230]  remoteproc5: Note: remoteproc is still under development and considered experimental.
    [    6.836470]  remoteproc5: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [    6.852316] vip 48970000.vip: loading firmware vpdma-1b8.bin
    [    6.860546] vip 48990000.vip: loading firmware vpdma-1b8.bin
    [    6.876553] vip 48990000.vip: VPDMA firmware loaded
    [    6.876590] vip 48970000.vip: VPDMA firmware loaded
    [    6.910718]  remoteproc5: registered virtio3 (type 7)
    [    6.919395] pru-rproc 4b238000.pru1: PRU rproc node /ocp/pruss@4b200000/pru1@4b238000 probed successfully
             Starting Load/Save Screen Backlight...htness of backlight:backli[    6.940990]  remoteproc6: 4b2b4000.pru0 is available
    ght...
    [  OK  ] Started Load/Save Screen Backlight Brightness of backlight:backlight.
    [    6.967879]  remoteproc6: Note: remoteproc is still under development and considered experimental.
    [    7.018373]  remoteproc6: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [    7.106567] ata1: SATA link down (SStatus 0 SControl 300)
    [    7.137019]  remoteproc6: registered virtio4 (type 7)
    [    7.137039]  remoteproc3: registered virtio5 (type 7)
    [    7.154859] pru-rproc 4b2b4000.pru0: PRU rproc node /ocp/pruss@4b280000/pru0@4b2b4000 probed successfully
    [    7.165300]  remoteproc7: 4b2b8000.pru1 is available
    [  OK  ] Reached target Sound Card.
    [    7.178241]  remoteproc7: Note: remoteproc is still under development and considered experimental.
    [    7.192761]  remoteproc7: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [    7.219894]  remoteproc7: registered virtio6 (type 7)
    [    7.225022] pru-rproc 4b2b8000.pru1: PRU rproc node /ocp/pruss@4b280000/pru1@4b2b8000 probed successfully
    [    7.280066]  remoteproc2: registered virtio7 (type 7)
    [  OK  ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
    [    7.566402] EXT4-fs (mmcblk0p6): Ignoring removed nomblk_io_submit option
    [    7.593058] EXT4-fs (mmcblk0p6): mounting ext3 file system using the ext4 subsystem
    [    7.648345] EXT4-fs (mmcblk0p6): recovery complete
    [    7.655198] EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
    [  OK  ] Reached target Local File Systems.
    [    7.692764] EXT4-fs (mmcblk0p5): mounting ext3 file system using the ext4 subsystem
    [    7.732480] EXT4-fs (mmcblk0p5): recovery complete
    [    7.741340] EXT4-fs (mmcblk0p3): mounting ext3 file system using the ext4 subsystem
    [    7.756263] EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: (null)
             Starting Create Volatile Files and Directories...
    [    7.797435] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
    [    7.829417] EXT4-fs (mmcblk0p3): recovery complete
    [    7.834243] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)
    [  OK  ] Started Create Volatile Files and Directories.
    [    7.967231]  remoteproc0: powering up 58820000.ipu
    [    8.001620]  remoteproc0: Booting fw image dra7-ipu1-fw.xem4, size 4866940
    [    8.043935] omap-iommu 58882000.mmu: 58882000.mmu: version 2.1
    [    8.071174]  remoteproc0: remote processor 58820000.ipu is now up
    [    8.091645] virtio_rpmsg_bus virtio0: rpmsg host is online
    [    8.097228] virtio_rpmsg_bus virtio0: creating channel rpmsg-client-sample addr 0x32
    [    8.105761] virtio_rpmsg_bus virtio0: creating channel rpmsg-client-sample addr 0x33
    [    8.113930] virtio_rpmsg_bus virtio0: creating channel rpmsg-omx addr 0x3c
    [    8.121083] virtio_rpmsg_bus virtio0: creating channel rpmsg-rpc addr 0x65
    [    8.129055]  remoteproc1: powering up 55020000.ipu
    [    8.141113]  remoteproc1: Booting fw image dra7-ipu2-fw.xem4, size 4866940
    [    8.148134] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
    [    8.174714]  remoteproc1: remote processor 55020000.ipu is now up
    [    8.184336] virtio_rpmsg_bus virtio1: rpmsg host is online
    [    8.189907] virtio_rpmsg_bus virtio1: creating channel rpmsg-client-sample addr 0x32
    [    8.197889]  remoteproc4: powering up 4b234000.pru0
    [    8.202914]  remoteproc4: Booting fw image am57xx-pru1_0-fw, size 75308
    [    8.209905] virtio_rpmsg_bus virtio1: creating channel rpmsg-client-sample addr 0x33
    [    8.218088] virtio_rpmsg_bus virtio1: creating channel rpmsg-omx addr 0x3c
    [    8.225332] ti-pruss 4b200000.pruss: configured system_events = 0x0000000000030000 intr_channels = 0x00000005 host_intr = 0x00000005
    [    8.237341] virtio_rpmsg_bus virtio1: creating channel rpmsg-rpc addr 0x65
    [    8.244595]  remoteproc4: remote processor 4b234000.pru0 is now up
    [    8.250933] virtio_rpmsg_bus virtio2: rpmsg host is online
    [    8.256463] virtio_rpmsg_bus virtio2: creating channel rpmsg-pru addr 0x1e
    [    8.263727]  remoteproc5: powering up 4b238000.pru1
    [    8.268781]  remoteproc5: Booting fw image am57xx-pru1_1-fw, size 75308
    [    8.275539] ti-pruss 4b200000.pruss: configured system_events = 0x00000000000c0000 intr_channels = 0x0000000a host_intr = 0x0000000a
    [    8.296567]  remoteproc5: remote processor 4b238000.pru1 is now up
    [    8.316548] virtio_rpmsg_bus virtio3: rpmsg host is online
    [    8.316574] virtio_rpmsg_bus virtio3: creating channel rpmsg-pru addr 0x1f
    [    8.337324]  remoteproc6: powering up 4b2b4000.pru0
    [    8.342369]  remoteproc6: Booting fw image am57xx-pru2_0-fw, size 75308
    [    8.356665] ti-pruss 4b280000.pruss: configured system_events = 0x0000000000030000 intr_channels = 0x00000005 host_intr = 0x00000005
    [  OK  ] Found device /dev/disk/by-label/cache.
    [    8.377014]  remoteproc6: remote processor 4b2b4000.pru0 is now up
    [    8.383349] virtio_rpmsg_bus virtio4: rpmsg host is online
    [    8.388901] virtio_rpmsg_bus virtio4: creating channel rpmsg-pru addr 0x20
    [    8.407191]  remoteproc3: powering up 41000000.dsp
    [    8.464038]  remoteproc3: Booting fw image dra7-dsp2-fw.xe66, size 21637112
    [    8.493164] omap_hwmod: mmu0_dsp2: _wait_target_disable failed
    [    8.499059] omap-iommu 41501000.mmu: 41501000.mmu: version 3.0
    [    8.504989] omap-iommu 41502000.mmu: 41502000.mmu: version 3.0
    [    8.521335]  remoteproc3: remote processor 41000000.dsp is now up
    [    8.530196] virtio_rpmsg_bus virtio5: rpmsg host is online
    [    8.535733] virtio_rpmsg_bus virtio5: creating channel rpmsg-proto addr 0x3d
    [    8.546468]  remoteproc7: powering up 4b2b8000.pru1
    [    8.551771]  remoteproc7: Booting fw image am57xx-pru2_1-fw, size 75308
    [    8.563109] ti-pruss 4b280000.pruss: configured system_events = 0x00000000000c0000 intr_channels = 0x0000000a host_intr = 0x0000000a
             Starting Network Time Synchronization...
             [    8.587438]  remoteproc7: remote processor 4b2b8000.pru1 is now up
    Starting Update UTMP about System Boot/Shutdown...
    [    8.595726] virtio_rpmsg_bus virtio6: rpmsg host is online
    [    8.604398] virtio_rpmsg_bus virtio6: creating channel rpmsg-pru addr 0x21
    [    8.630003]  remoteproc2: powering up 40800000.dsp
    [  OK  ] Started Network Time Synchronization.
    [    8.671156]  remoteproc2: Booting fw image dra7-dsp1-fw.xe66, size 21637112
    [    8.697001] omap_hwmod: mmu0_dsp1: _wait_target_disable failed
    [    8.702893] omap-iommu 40d01000.mmu: 40d01000.mmu: version 3.0
    [    8.708816] omap-iommu 40d02000.mmu: 40d02000.mmu: version 3.0
    [  OK  ] Reached target System Time Synchronized.
    [    8.728084]  remoteproc2: remote processor 40800000.dsp is now up
    [    8.739086] virtio_rpmsg_bus virtio7: rpmsg host is online
    [    8.739165] virtio_rpmsg_bus virtio7: creating channel rpmsg-proto addr 0x3d
    [    8.766221] rpmsg_pru rpmsg8: new rpmsg_pru device: /dev/rpmsg_pru30
             Starting Synchronize System and HW clocks...
    [    8.781042] rpmsg_pru rpmsg9: new rpmsg_pru device: /dev/rpmsg_pru31
    [    8.782597] rpmsg_rpc rpmsg3: probing service rpc_example_2 with src 1024 dst 101
    [    8.782779] rpmsg_rpc rpmsg7: probing service rpc_example_1 with src 1024 dst 101
    [    8.783285] rpmsg_rpc rpmsg3: published functions = 8
    [    8.783735] rpmsg_rpc rpmsg7: published functions = 8
    [    8.784786] usbcore: registered new interface driver usbfs
    [    8.784840] usbcore: registered new interface driver hub
    [    8.784917] usbcore: registered new device driver usb
    [    8.809797] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
    [    8.809815] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1
    [    8.813523] NET: Registered protocol family 41
    [    8.820068] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x00010010
    [    8.820112] xhci-hcd xhci-hcd.1.auto: irq 526, io mem 0x488d0000
    [    8.827221] hub 1-0:1.0: USB hub found
    [    8.827252] hub 1-0:1.0: 1 port detected
    [    8.827578] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
    [    8.827590] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
    [    8.827674] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
    [    8.828962] hub 2-0:1.0: USB hub found
    [    8.828988] hub 2-0:1.0: 1 port detected
    [    8.829379] dwc3 48890000.usb: otg: primary host xhci-hcd.2.auto registered
    [    8.829384] dwc3 48890000.usb: otg: shared host xhci-hcd.2.auto registered
    [    8.829388] dwc3 48890000.usb: otg: can't start till gadget registers
    [    8.918919] rpmsg_pru rpmsg10: new rpmsg_pru device: /dev/rpmsg_pru32
    [    8.925606]rpmsg_pru rpmsg12: new rpmsg_pru device: /dev/rpmsg_pru33
    [  OK  ] Started Update UTMP about System Boot/Shutdown.
    [  OK  ] Started Synchronize System and HW clocks.
    [  OK  ] Reached target System Initialization.
    [  OK  ] Listening on dropbear.socket.
    [  OK  ] Listening on RPCbind Server Activation Socket.
    [  OK  ] Started Daily Cleanup of Temporary Directories.
    [  OK  ] Reached target Timers.
    [  OK  ] Listening on D-Bus System Message Bus Socket.
    .    9.136513] usb 1-1: new high-speed USB device number 2 using xhci-hcd
    [  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
    [  OK  ] Reached target Sockets.
    [  OK  ] Reached target Basic System.
             Starting Avahi mDNS/DNS-SD Stack...
    [  OK  ] Started D-Bus System Message Bus.
    [    9.307874] hub 1-1:1.0: USB hub found
    [    9.311720] hub 1-1:1.0: 4 ports detected
    [  OK  ] Started Avahi mDNS/DNS-SD Stack.
             Starting Network Service...
             Starting uim-sysfs.service...
    [    9.415612] net eth0: initializing cpsw version 1.15 (0)
             [    9.425666] net eth0: initialized cpsw ale version 1.4
    Starting Save/Restore Sound Card State...
    [    9.434324] net eth0: ALE Table size 1024
    [    9.445511] libphy: PHY 48485000.mdio:01 not found
    [  OK  ] Started Kernel Logging Service.
    [    9.458683] net eth0: phy "48485000.mdio:01" not found on slave 0, err -19
             Starting Permit User Sessions...
    [    9.580455] net eth0: phy found : id is : 0x4dd072
    [  OK  ] Started System Logging Service.
    [    9.602451] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    [  OK  ] Started strongSwan IPsec IKEv1/IKEv2 daemon using ipsec.conf.
             Starting Login Service...
             Starting Print notice about GPLv3 packages...
             Starting Telephony service...
    [    9.702019] random: nonblocking pool is initialized
    [  OK  ] Started Network Service.
    [  OK  ] Started Save/Restore Sound Card State.
    [  OK  ] Started Permit User Sessions.
    [    9.785290] NET: Registered protocol family 15
    [    9.946123] Initializing XFRM netlink socket
    [  OK  ] Started Telephony service.
    [  OK  ] Started Login Service.
    [  OK  ] Started Getty on tty1.
    [  OK  ] Started Serial Getty on ttyS2.
    [  OK  ] Reached target Network.
             Starting Network Name Resolution...
             Starting Lightning Fast Webserver With Light System Requirements...
    [  OK  ] Started Network Name Resolution.
    [  OK  ] Started Lightning Fast Webserver With Light System Requirements.
    [  OK  ] Started uim-sysfs.service.
             Starting rc.pvr.service...
    [   10.986881] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ]
    [  OK  ] Started rc.pvr.service.
             Starting weston.service...
    [  OK  ] Started weston.service.
             Starting tiipclad-daemon.service...
             Starting telnetd.service...
    [  OK  ] Started telnetd.service.
    [  OK  ] Started tiipclad-daemon.service.
    ***************************************************************
    ***************************************************************
    NOTICE: This file system contains the following GPLv3 packages:
            autoconf-archive
            autoconf
            binutils-dev
            binutils
            bison-dev
            bison
            cpp-symlinks
            cpp
            diffutils
            dosfstools
            g++-symlinks
            g++
            gawk-dev
            gawk
            gcc-symlinks
            gcc
            gdb
            gdbc6x
            gdbserver
            grep
            gstreamer1.0-libav
            hidapi
            libcairo-perf-utils
            libgmp10
            libidn11
            libmpc3
            libmpfr4
            make
            nettle
            parted
            patch
            sed
            swig-dev
            swig
    
    If you do not wish to distribute GPLv3 components please remove
    the above packages prior to distribution.  This can be done using
    the opkg remove command.  i.e.:
        opkg remove <package>
    Where <package> is the name printed in the list above
    
    NOTE: If the package is a dependency of another package you
          will be notified of the dependent packages.  You should
          use the --force-removal-of-dependent-packages option to
          also remove the dependent packages as well
    ***************************************************************
    ***************************************************************
             Starting thttpd.service...
    [  OK  ] Started Print notice about GPLv3 packages.
    [  OK  ] Started thttpd.service.
             Starting rng-tools.service...
    [  OK  ] Started rng-tools.service.
             Starting mqtt.service...
    [  OK  ] Started mqtt.service.
             Starting gdbserverproxy.service...
    [  OK  ] Started gdbserverproxy.service.
             Starting matrix-gui-2.0.service...
    [  OK  ] Started matrix-gui-2.0.service.
             Starting thermal-zone-init.service...
    [  OK  ] Started thermal-zone-init.service.
    
     _____                    _____           _         _
    |  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
    |     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
    |__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
                  |___|                    |___|
    
    Arago Project http://arago-project.org am57xxrom7510a2 ttyS2
    
    Arago 2016.08 Yocto 2.1 (krogoth) am57xxrom7510a2 ttyS2
    
    am57xxrom7510a2 login: [   19.043352] omap_hwmod: mmu1_dsp1: _wait_target_disable failed
    [   19.056840] omap_hwmod: mmu0_dsp1: _wait_target_disable failed
    [   19.083802] omap_hwmod: mmu1_dsp2: _wait_target_disable failed
    [   19.096951] omap_hwmod: mmu0_dsp2: _wait_target_disable failed
    

  • Can you also attach the /var/log/weston.log file?

  • Date: 2018-01-19 UTC
    [17:56:34.193] weston 1.9.0
                   http://wayland.freedesktop.org
                   Bug reports to: https://bugs.freedesktop.org/enter_bug.cgi?product=Wayland&component=weston&version=1.9.0
                   Build: 1.8.93-2-gb05cdb8 configure.ac: bump to version 1.9.0 for the official release (2015-09-21 18:11:26 -0700)
    [17:56:34.193] OS: Linux, 4.4.19-gf3417ba1aa, #1 SMP PREEMPT Thu Dec 21 15:43:40 UTC 2017, armv7l
    [17:56:34.194] Using config file '/etc//weston.ini'
    [17:56:34.199] Loading module '/usr/lib/weston/drm-backend.so'
    [17:56:34.214] Output repaint window is 7 ms maximum.
    [17:56:34.214] initializing drm backend
    [17:56:34.224] using /dev/dri/card0
    [17:56:34.225] Loading module '/usr/lib/weston/gl-renderer.so'
    failed to load module: /usr/lib/gbm/gbm_dri.so: cannot open shared object file: No such file or directory
    failed to load module: /usr/lib/gbm/gbm_gallium_drm.so: cannot open shared object file: No such file or directory
    loaded module : gbm_pvr.so
    found valid GBM backend : gbm_pvr.so
    [17:56:34.264] warning: either no EGL_EXT_platform_base support or specific platform support; falling back to eglGetDisplay.
    [17:56:34.273] warning: EGL_EXT_buffer_age not supported. Performance could be affected.
    [17:56:34.273] Retrieving EGL client extension string failed.
    [17:56:34.276] input device 'gpio_keys', /dev/input/event0 is tagged by udev as: Keyboard
    [17:56:34.276] input device 'gpio_keys', /dev/input/event0 is a keyboard
    [17:56:34.640] EGL version: 1.4 build 1.14@3699939 (MAIN)
    [17:56:34.640] EGL vendor: Imagination Technologies
    [17:56:34.640] EGL client APIs: OpenGL_ES 
    [17:56:34.640] EGL extensions: EGL_IMG_client_api_ogl EGL_KHR_image
                   EGL_KHR_image_base EGL_KHR_gl_texture_2D_image
                   EGL_KHR_gl_texture_cubemap_image EGL_KHR_gl_renderbuffer_image
                   EGL_KHR_vg_parent_image EGL_IMG_cl_image EGL_KHR_fence_sync
                   EGL_IMG_context_priority EGL_IMG_hibernate_process
                   EGL_IMG_image_plane_attribs EGL_KHR_surfaceless_context
                   EGL_KHR_wait_sync EGL_KHR_create_context
                   EGL_WL_bind_wayland_display
    [17:56:34.641] GL version: OpenGL ES 2.0 build 1.14@3699939 (MAIN)
    [17:56:34.641] GLSL version: OpenGL ES GLSL ES 1.00 build 1.14@3699939 (MAIN)
    [17:56:34.641] GL vendor: Imagination Technologies
    [17:56:34.641] GL renderer: PowerVR SGX 544MP
    [17:56:34.641] GL extensions: GL_OES_rgb8_rgba8 GL_OES_depth24
                   GL_OES_vertex_half_float GL_OES_texture_float
                   GL_OES_texture_half_float GL_OES_element_index_uint
                   GL_OES_mapbuffer GL_OES_fragment_precision_high
                   GL_OES_compressed_ETC1_RGB8_texture GL_OES_EGL_image
                   GL_OES_EGL_image_external GL_OES_required_internalformat
                   GL_OES_depth_texture GL_OES_get_program_binary
                   GL_OES_packed_depth_stencil GL_OES_standard_derivatives
                   GL_OES_vertex_array_object GL_OES_egl_sync GL_OES_texture_npot
                   GL_OES_surfaceless_context GL_EXT_discard_framebuffer
                   GL_EXT_blend_minmax GL_EXT_multi_draw_arrays
                   GL_EXT_multisampled_render_to_texture GL_EXT_shader_texture_lod
                   GL_EXT_texture_format_BGRA8888 GL_EXT_occlusion_query_boolean
                   GL_EXT_texture_rg GL_EXT_draw_buffers
                   GL_EXT_shader_framebuffer_fetch GL_IMG_shader_binary
                   GL_IMG_texture_compression_pvrtc
                   GL_IMG_texture_compression_pvrtc2 GL_IMG_texture_npot
                   GL_IMG_texture_format_BGRA8888 GL_IMG_read_format
                   GL_IMG_program_binary GL_IMG_uniform_buffer_object
                   GL_IMG_multisampled_render_to_texture GL_KHR_debug
    [17:56:34.641] GL ES 2 renderer features:
                   read-back format: RGBA
                   wl_shm sub-image to texture: no
                   EGL Wayland extension: yes
    [17:56:34.641] Chosen EGL config details:
                   RGBA bits: 8 8 8 8
                   swap interval range: 1 - 1
    [17:56:34.641] cursor buffers unavailable, using gl cursors
    [17:56:34.641] Initialized backlight, device /sys/class/backlight/backlight
    [17:56:34.642] EDID data 'PHL', 'PHL 234E5', 'UHB160203202'
    [17:56:34.642] Output HDMI-A-1, (connector 32, crtc 34)
                   mode 1920x1080@60.0, preferred, current
                   mode 1920x1080@59.9
                   mode 1920x1080@60.0
                   mode 1920x1080@59.9
                   mode 1920x1080@50.0
                   mode 1920x1080@50.0
                   mode 1680x1050@59.9
                   mode 1280x1024@75.0
                   mode 1280x1024@60.0
                   mode 1440x900@75.0
                   mode 1440x900@59.9
                   mode 1280x720@60.0
                   mode 1280x720@59.9
                   mode 1280x720@50.0
                   mode 1024x768@75.1
                   mode 1024x768@60.0
                   mode 800x600@75.0
                   mode 800x600@60.3
                   mode 720x576@50.0
                   mode 720x576@50.0
                   mode 720x480@60.0
                   mode 720x480@59.9
                   mode 720x480@60.0
                   mode 720x480@59.9
                   mode 640x480@75.0
                   mode 640x480@72.8
                   mode 640x480@66.7
                   mode 640x480@60.0
                   mode 640x480@59.9
                   mode 720x400@70.1
                   mode 1920x1080@60.0, preferred
    [17:56:34.675] Chosen EGL config details:
                   RGBA bits: 8 8 8 8
                   swap interval range: 1 - 1
    [17:56:34.675] cursor buffers unavailable, using gl cursors
    [17:56:34.675] Failed to initialize backlight
    [17:56:34.675] Output Unknown-1, (connector 36, crtc 38)
                   mode 1920x1080@65.4, preferred, current
                   mode 1920x1080@65.4, preferred
    [17:56:34.675] Compositor capabilities:
                   arbitrary surface rotation: yes
                   screen capture uses y-flip: yes
                   presentation clock: CLOCK_MONOTONIC, id 1
    [17:56:34.676] Loading module '/usr/lib/weston/desktop-shell.so'
    [17:56:34.679] launching '/usr/libexec/weston-keyboard'
    [17:56:34.680] launching '/usr/libexec/weston-desktop-shell'
    [17:56:34.804] VBlank is pending for connector = 36, frame = 2
    [17:56:35.019] VBlank is pending for connector = 32, frame = 13
    [17:56:35.050] VBlank is pending for connector = 36, frame = 19
    [17:56:35.066] VBlank is pending for connector = 36, frame = 20
    [17:56:35.083] VBlank is pending for connector = 36, frame = 21
    [17:56:35.106] VBlank is pending for connector = 32, frame = 19
    [17:56:35.122] VBlank is pending for connector = 32, frame = 20
    [17:56:35.138] VBlank is pending for connector = 32, frame = 21
    [17:56:35.154] VBlank is pending for connector = 32, frame = 22
    [17:56:35.188] VBlank is pending for connector = 36, frame = 28
    [17:56:35.220] VBlank is pending for connector = 36, frame = 30
    [17:56:35.262] VBlank is pending for connector = 36, frame = 33
    [17:56:35.290] VBlank is pending for connector = 32, frame = 30
    [17:56:35.305] VBlank is pending for connector = 32, frame = 31
    [17:56:35.321] VBlank is pending for connector = 32, frame = 32
    [17:56:35.338] VBlank is pending for connector = 32, frame = 33
    [17:56:35.387] VBlank is pending for connector = 36, frame = 41
    [17:56:35.430] VBlank is pending for connector = 36, frame = 44
    [17:56:35.450] VBlank is pending for connector = 36, frame = 45
    [17:56:35.757] Chosen EGL config details:
                   RGBA bits: 8 8 8 8
                   swap interval range: 1 - 1
    [17:56:35.757] cursor buffers unavailable, using gl cursors
    [17:56:35.758] Initialized backlight, device /sys/class/backlight/backlight
    [17:56:35.758] EDID data 'PHL', 'PHL 234E5', 'UHB160203202'
    [17:56:35.758] Output HDMI-A-1, (connector 32, crtc 34)
                   mode 1920x1080@60.0, preferred, current
                   mode 1920x1080@59.9
                   mode 1920x1080@60.0
                   mode 1920x1080@59.9
                   mode 1920x1080@50.0
                   mode 1920x1080@50.0
                   mode 1680x1050@59.9
                   mode 1280x1024@75.0
                   mode 1280x1024@60.0
                   mode 1440x900@75.0
                   mode 1440x900@59.9
                   mode 1280x720@60.0
                   mode 1280x720@59.9
                   mode 1280x720@50.0
                   mode 1024x768@75.1
                   mode 1024x768@60.0
                   mode 800x600@75.0
                   mode 800x600@60.3
                   mode 720x576@50.0
                   mode 720x576@50.0
                   mode 720x480@60.0
                   mode 720x480@59.9
                   mode 720x480@60.0
                   mode 720x480@59.9
                   mode 640x480@75.0
                   mode 640x480@72.8
                   mode 640x480@66.7
                   mode 640x480@60.0
                   mode 640x480@59.9
                   mode 720x400@70.1
                   mode 1920x1080@60.0, preferred
    [17:56:35.758] connector 32 connected
    [17:56:35.788] Chosen EGL config details:
                   RGBA bits: 8 8 8 8
                   swap interval range: 1 - 1
    [17:56:35.788] cursor buffers unavailable, using gl cursors
    [17:56:35.788] Failed to initialize backlight
    [17:56:35.788] Output Unknown-1, (connector 36, crtc 38)
                   mode 1920x1080@65.4, preferred, current
                   mode 1920x1080@65.4, preferred
    [17:56:35.788] connector 36 connected
    [17:56:35.833] destroy output while page flip pending
    

  • The eMMC loads the files too fast compared to the SD card then if there is a /etc/udev/rules.d/ws-calibrate.rules (will be there if the touch screen has already calibrated before) the /etc/init.d/weston script hits exit 0 and this kills the running openvt -c 4 -f runWeston. If this command is executed in 2 seconds later stage the exit 0 will not kill the openvt -c 4 -f runWeston. To tune this up if you add sleep 2 to /etc/init.d/weston in line 42 before first openvt -c 4 -f runWeston this will keep the openvt -c 4 -f runWeston running and the display will function normally.

  • Thank you very much!