Part Number: AM5716
Tool/software: Linux
Hi,
We are using AM5716 processor's MII1 port and is interfaced with KSZ8091MLX PHY. We have connected the MDI side to DHCP network and see that link is up on ifconfig eth1 up command. However, it doesn't get the ip address after udhcpc -i eth1 command. We have verified the pin-mux settings and hardware connections and is fine.
Can you please point us to a document or reference design where MII interface is used and what all settings are required to be done in AM5716 to support MII1 interface apart from Pin-Mux?
Please note that we have also used RGMII0 port and this works fine with the same setup.
Regards
Raja