Part Number: AM3358
Tool/software: Linux
I have been googling but my knowledge about linux is limited and cannot find anything about this issue (even on TI forum). I attach environment variables from uboot and UART0 console output.
This is little overview steps I have done.
- My dev kit is BBBW.
- I set up a virtual machine (Ubuntu 12.04) under virtualbox where I want to set all tools needed for development.
- I followed the TI official wiki pages about building U-boot and Linux.
- All servers (DHCP, TFTP, NFS) are running and I am able to mount the rootpath and read and write from/to it.
- ufw inactive.
- /etc/exports
- /export/rootfs/ *(rw,nohide,insecure,no_subtree_check,async,no_root_squash)
- U-boot has static IP 192.168.2.3 and this IP is also passed to kernel.
- I had to add USB-Ether gadget driver into kernel so it can mount NSF FS.
- I didn't add initramfs into kernel due to mounting FS via NFS.
- As a filesystem I'm using original tarball from sdk (tisdk-rootfs-image-am335x-evm.tar.xz). If I create a SD with this filesystem it boots properly!
- I installed modules from kernel to filesystem.
- BBBW loads successfully u-boot, zImage and dtb via TFTP. It also mounts filesystem via NFS (at first place).
And these are my results and observation.
- It freezes in boot process with this message: [ 25.922728] nfs: server 192.168.2.1 not responding, still trying
- The kernel stuck right after message [ OK ] Started Network Service.
- Targets heartbeat led is blinking aprox 2 times faster.
- Some files and folders required by BBBW over NFS are not placed in rootpath. (Ex.: /etc/ld.so.preload, /etc/inird-release, /proc/self, /proc/vz, /etc/adjtime, /systemd/system.conf.d,... )
- If i tried to use initramfs as NFS filesystem, target booted properly.
Could it be caused by using virtual machine as a host? I would appreciate any help including tutorials how to get deeper into embedded Linux development.
Many thanks
U-Boot 2017.01-00444-g4e7f4689e5-dirty (Jan 18 2018 - 15:10:52 +0100)
CPU : AM335X-GP rev 2.1
Model: TI AM335x BeagleBone Black
DRAM: 512 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
MMC: no card present
** Bad device mmc 0 **
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
Net: Could not get PHY for cpsw: addr 0
cpsw, usb_ether
Hit any key to stop autoboot: 0
Booting from network ...
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC 50:65:83:d5:08:dc
HOST MAC de:ad:be:af:00:00
RNDIS ready
musb-hdrc: peripheral reset irq lost!
high speed config #2: 2 mA, Ethernet Gadget, using RNDIS
USB RNDIS network up!
Using usb_ether device
TFTP from server 192.168.2.1; our IP address is 192.168.2.3
Filename 'zImage'.
Load address: 0x82000000
Loading: #################################################################
#################################################################
#################################################################
###########################################################
881.8 KiB/s
done
Bytes transferred = 3728160 (38e320 hex)
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC 50:65:83:d5:08:dc
HOST MAC de:ad:be:af:00:00
RNDIS ready
high speed config #2: 2 mA, Ethernet Gadget, using RNDIS
USB RNDIS network up!
Using usb_ether device
TFTP from server 192.168.2.1; our IP address is 192.168.2.3
Filename 'am335x-boneblack.dtb'.
Load address: 0x88000000
Loading: ###
821.3 KiB/s
done
Bytes transferred = 37857 (93e1 hex)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8fff3000, end 8ffff3e0 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.9.59-ga75d8e9305 (root@host-VirtualBox) (gcc version 6.2.1 20161016 (Linaro GCC 6.2-2016.11) ) #8 PREEMPT Mon Jan 22 15:57:07 CET 2018
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt:Machine model: TI AM335x BeagleBone Black
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0x9d000000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon)
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129920
[ 0.000000] Kernel command line: console=ttyO0,115200n8 g_ether.dev_addr=50:65:83:d5:08:dc nfsrootdebug root=/dev/nfs nfsroot=192.168.2.1:/export/rootfs,nolock rw ip=192.168.2.3:192.168.2.1::255.255.25f
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 456940K/524288K available (8192K kernel code, 288K rwdata, 2444K rodata, 1024K init, 281K bss, 18196K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0900000 (9184 kB)
[ 0.000000] .init : 0xc0c00000 - 0xc0d00000 (1024 kB)
[ 0.000000] .data : 0xc0d00000 - 0xc0d48310 ( 289 kB)
[ 0.000000] .bss : 0xc0d48310 - 0xc0d8eab4 ( 282 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000012] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000031] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000040] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000189] clocksource_probe: no matching clocksources found
[ 0.000342] Console: colour dummy device 80x30
[ 0.000368] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000373] This ensures that you still see kernel messages. Please
[ 0.000378] update your kernel commandline.
[ 0.000399] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.089240] pid_max: default: 32768 minimum: 301
[ 0.089357] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089367] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.090075] CPU: Testing write buffer coherency: ok
[ 0.090412] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.091158] EFI services will not be available.
[ 0.092307] devtmpfs: initialized
[ 0.102732] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.103058] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.103082] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.106351] pinctrl core: initialized pinctrl subsystem
[ 0.107475] NET: Registered protocol family 16
[ 0.109161] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.122151] omap_hwmod: debugss: _wait_target_disable failed
[ 0.199231] cpuidle: using governor ladder
[ 0.229221] cpuidle: using governor menu
[ 0.234654] OMAP GPIO hardware version 0.1
[ 0.247959] No ATAGs?
[ 0.247984] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.286439] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.289204] usbcore: registered new interface driver usbfs
[ 0.289431] usbcore: registered new interface driver hub
[ 0.289527] usbcore: registered new device driver usb
[ 0.289880] omap_i2c 44e0b000.i2c: could not find pctldev for node /0000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.289928] omap_i2c 4819c000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c2_pins, deferring probe
[ 0.290025] media: Linux media interface: v0.10
[ 0.290072] Linux video capture interface: v2.00
[ 0.290111] pps_core: LinuxPPS API ver. 1 registered
[ 0.290117] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.290138] PTP clock support registered
[ 0.290171] EDAC MC: Ver: 3.0.0
[ 0.291137] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.291441] Advanced Linux Sound Architecture Driver Initialized.
[ 0.292606] clocksource: Switched to clocksource timer1
[ 0.301696] NET: Registered protocol family 2
[ 0.302383] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.302427] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.302465] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.302526] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.302542] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.302721] NET: Registered protocol family 1
[ 0.303109] RPC: Registered named UNIX socket transport module.
[ 0.303120] RPC: Registered udp transport module.
[ 0.303126] RPC: Registered tcp transport module.
[ 0.303131] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.303992] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.306085] workingset: timestamp_bits=14 max_order=17 bucket_order=3
[ 0.312871] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.313708] NFS: Registering the id_resolver key type
[ 0.313747] Key type id_resolver registered
[ 0.313755] Key type id_legacy registered
[ 0.313796] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.315487] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[ 0.315505] io scheduler noop registered
[ 0.315512] io scheduler deadline registered
[ 0.315652] io scheduler cfq registered (default)
[ 0.316845] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.371483] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.374914] ial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
[ 0.994611] console [ttyS0] enabled
[ 0.999692] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[ 1.006510] [drm] Initialized
[ 1.021719] brd: module loaded
[ 1.030522] loop: module loaded
[ 1.035729] libphy: Fixed MDIO Bus: probed
[ 1.043580] 47401300.usb-phy supply vcc not found, using dummy regulator
[ 1.055036] 47401b00.usb-phy supply vcc not found, using dummy regulator
[ 1.070739] using random self ethernet address
[ 1.075296] using random host ethernet address
[ 1.079767] using self ethernet address: 50:65:83:d5:08:dc[ 1.085755] usb0: HOST MAC aa:08:38:2f:51:be
[ 1.090140] usb0: MAC 50:65:83:d5:08:dc
[ 1.094053] using random self ethernet address
[ 1.098515] using random host ethernet address
[ 1.103155] g_ether gadget: Ethernet Gadget, version: Memorial Day 2008
[ 1.109797] g_ether gadget: g_ether ready
[ 1.114354] mousedev: PS/2 mouse device common for all mice
[ 1.120438] i2c /dev entries driver
[ 1.125739] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.133495] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.253865] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.266115] NET: Registered protocol family 10
[ 1.271824] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 1.278795] NET: Registered protocol family 17
[ 1.283654] Key type dns_resolver registered
[ 1.288286] omap_voltage_late_init: Voltage driver support not added
[ 1.338294] random: fast init done
[ 1.344199] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[ 1.350167] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.358457] mmc1: new high speed MMC card at address 0001
[ 1.364683] mmcblk1: mmc1:0001 S10004 3.56 GiB
[ 1.369520] mmcblk1boot0: mmc1:0001 S10004 partition 1 4.00 MiB
[ 1.375746] mmcblk1boot1: mmc1:0001 S10004 partition 2 4.00 MiB
[ 1.382959] mmcblk1: p1
[ 1.504936] tda998x 0-0070: found TDA19988
[ 1.510260] tilcdc 4830e000.lcdc: bound 0-0070 (ops tda998x_ops)
[ 1.516358] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.523012] [drm] No driver support for vblank timestamp query.
[ 1.529268] tilcdc 4830e000.lcdc: No connectors reported connected with modes
[ 1.536477] [drm] Cannot find any crtc or sizes - going 1024x768
[ 1.550460] Console: switching to colour frame buffer device 128x48
[ 1.561615] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.590456] g_ether gadget: high-speed config #1: CDC Ethernet (ECM)
[ 1.597842] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.723427] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 100 kHz
[ 1.731015] hctosys: unable to open rtc device (rtc0)
[ 1.762756] IP-Config: Complete:
[ 1.766016] device=usb0, hwaddr=50:65:83:d5:08:dc, ipaddr=192.168.2.3, mask=255.255.255.0, gw=255.255.255.255
[ 1.776432] host=192.168.2.3, domain=, nis-domain=(none)
[ 1.782203] bootserver=192.168.2.1, rootserver=192.168.2.1, rootpath=
[ 1.789434] ALSA device list:
[ 1.792419] No soundcards found.
[ 7.289874] VFS: Mounted root (nfs filesystem) on device 0:15.
[ 7.297031] devtmpfs: mounted
[ 7.303978] Freeing unused kernel memory: 1024K
[ 7.946828] systemd[1]: System time before build time, advancing clock.
[ 8.050755] systemd[1]: systemd 230 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[ 8.069625] systemd[1]: Detected architecture arm.
Welcome to Arago 2017.10!
[ 8.107209] systemd[1]: Set hostname to <am335x-evm>.
[ 8.848771] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 8.883391] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 8.923184] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 9.005321] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 9.034551] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 9.063250] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ 9.102884] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ OK ] Created slice System Slice.
[ OK ] Created slice system-getty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ OK ] Reached target Slices.
[ OK ] Listening on Journal Socket.
Starting Setup Virtual Console...
Starting Load Kernel Modules...
Starting Create list of required st... nodes for the current kernel...
Mounting Temporary Directory...
[ OK ] Listening on Network Service Netlink Socket.
[ 9.563107] cryptodev: loading out-of-tree module taints kernel.
[ 9.587726] cryptodev: driver 1.8 loaded.
[ OK ] Listening on udev Kernel Socket.
Starting Remount Root and Kernel File Systems...
[ OK ] Reached target Remote File Systems.
[ OK ] Listening on Journal Socket (/dev/log).
Starting Journal Service...
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ OK ] Reached target Paths.
Mounting Debug File System...
[ 9.788394] random: crng init done
Mounting POSIX Message Queue File System...
[ OK ] Mounted Temporary Directory.
[ OK ] Started Setup Virtual Console.
[ OK ] Started Load Kernel Modules.
[ OK ] Started Create list of required sta...ce nodes for the current kernel.
[ OK ] Started Remount Root and Kernel File Systems.
[ OK ] Mounted Debug File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Started Journal Service.
Starting Flush Journal to Persistent Storage...
Starting udev Coldplug all Devices...
Starting Create Static Device Nodes in /dev...
Mounting Configuration File System...
Starting Apply Kernel Variables...
[ OK ] Mounted Configuration File System.
[ 10.677053] systemd-journald[100]: Received request to flush runtime journal from PID 1
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Load/Save Random Seed.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Create Volatile Files and Directories.
Starting Update UTMP about System Boot/Shutdown...
Starting Network Time Synchronization...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Synchronized.
[ 13.002105] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ OK ] Started udev Coldplug all Devices.
[ 13.105475] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[ OK ] Reached target System Initialization.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
Starting telnetd.service...
[ OK ] Started System Logging Service.
Starting Print notice about GPLv3 packages...
Starting Login Service...
[ OK ] Started D-Bus System Message Bus.
[ 15.259999] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 15.484199] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 15.496096] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 15.514550] remoteproc remoteproc0: wkup_m3 is available
[ 15.532999] omap-aes 53500000.aes: will run requests pump with realtime priority
Starting Network Service...
[ 15.797578] asoc-simple-card sound: hdmi-hifi.0 <-> 48038000.mcasp mapping ok
[ 15.839295] remoteproc remoteproc0: powering up wkup_m3
[ OK ] Started Kernel Logging Service.
[ 15.978616] PM: Cannot get wkup_m3_ipc handle
[ 16.017251] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 224268
[ 16.017529] remoteproc remoteproc0: remote processor wkup_m3 is now up
[ 16.017553] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
Starting Save/Restore Sound Card State...
[ OK ] Started telnetd.service.
[ OK ] Found device /dev/ttyS0.
[ OK ] Started Network Service.
[ 25.922684] nfs: server 192.168.2.1 not responding, still trying
arch=arm
args_mmc=run finduuid;setenv bootargs console=${console} ${optargs} root=PARTUUID=${uuid} rw rootfstype=${mmcrootfstype}
baudrate=115200
board=prusa_pro
board_name=A335BNLT
board_rev=BWA5
board_serial=1650BBWG0826
boot_a_script=load ${devtype} ${devnum}:${distro_bootpart} ${scriptaddr} ${prefix}${script}; source ${scriptaddr}
boot_efi_binary=load ${devtype} ${devnum}:${distro_bootpart} ${kernel_addr_r} efi/boot/bootarm.efi; if fdt addr ${fdt_addr_r}; then bootefi ${kernel_addr_r} ${fdt_addr_r};else bootefi ${kernel_addr_r} ${fi
boot_extlinux=sysboot ${devtype} ${devnum}:${distro_bootpart} any ${scriptaddr} ${prefix}extlinux/extlinux.conf
boot_fdt=try
boot_fit=0
boot_net_usb_start=usb start
boot_prefixes=/ /boot/
boot_script_dhcp=boot.scr.uimg
boot_scripts=boot.scr.uimg boot.scr
boot_targets=mmc0 legacy_mmc0 mmc1 legacy_mmc1 nand0 pxe dhcp
bootcmd=echo Booting from network ...; setenv autoload no; run netloadimage; run findfdt; run netloadfdt; run netargs; bootz ${loadaddr} - ${fdtaddr}
bootcmd_dhcp=run boot_net_usb_start; if dhcp ${scriptaddr} ${boot_script_dhcp}; then source ${scriptaddr}; fi;setenv efi_fdtfile ${fdtfile}; if test -z "${fdtfile}" -a -n "${soc}"; then setenv efi_fdtfile;
bootcmd_legacy_mmc0=setenv mmcdev 0; setenv bootpart 0:2 ; run mmcboot
bootcmd_legacy_mmc1=setenv mmcdev 1; setenv bootpart 1:2 ; run mmcboot
bootcmd_mmc0=setenv devnum 0; run mmc_boot
bootcmd_mmc1=setenv devnum 1; run mmc_boot
bootcmd_nand=run nandboot
bootcmd_pxe=run boot_net_usb_start; dhcp; if pxe get; then pxe boot; fi
bootcount=1
bootdelay=2
bootdir=/boot
bootenvfile=uEnv.txt
bootfile=zImage
bootm_size=0x10000000
bootpart=0:2
bootscript=echo Running bootscript from mmc${mmcdev} ...; source ${loadaddr}
console=ttyO0,115200n8
cpu=armv7
dfu_alt_info_emmc=rawemmc raw 0 3751936
dfu_alt_info_mmc=boot part 0 1;rootfs part 0 2;MLO fat 0 1;MLO.raw raw 0x100 0x100;u-boot.img.raw raw 0x300 0x1000;u-env.raw raw 0x1300 0x200;spl-os-args.raw raw 0x1500 0x200;spl-os-image.raw raw 0x1700 01
dfu_alt_info_nand=SPL part 0 1;SPL.backup1 part 0 2;SPL.backup2 part 0 3;SPL.backup3 part 0 4;u-boot part 0 5;u-boot-spl-os part 0 6;kernel part 0 8;rootfs part 0 9
dfu_alt_info_ram=kernel ram 0x80200000 0x4000000;fdt ram 0x80f80000 0x80000;ramdisk ram 0x81000000 0x400t in ${boot_targets}; do run bootcmd_${target}; done
efi_dtb_prefixes=/ /dtb/ /dtb/current/
envboot=mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadbootscript; then run bootscript;else if run loadbootenv; then echo Loaded env from ${bootenvfile};run import;
eth1addr=50:65:83:d5:08:de
ethact=cpsw
ethaddr=50:65:83:d5:08:dc
fdt_addr_r=0x88000000
fdtaddr=0x88000000
fdtcontroladdr=9df294f8
fdtfile=undefined
findfdt=if test $board_name = A335BONE; then setenv fdtfile am335x-bone.dtb; fi; if test $board_name = A335BNLT; then setenv fdtfile am335x-boneblack.dtb; fi; if test $board_name = BBBW; then setenv fdtfi
finduuid=part uuid mmc ${bootpart} uuid
fit_bootfile=fitImage
fit_loadaddr=0x87000000
importbootenv=echo Importing environment from mmc${mmcdev} ...; env import -t ${loadaddr} ${filesize}
init_console=if test $board_name = A335_ICE; then setenv console ttyO3,115200n8;else setenv console ttyO0,115200n8;fi;
ipaddr=192.168.2.3
kernel_addr_r=0x82000000
load_efi_dtb=load ${devtype} ${devnum}:${distro_bootpart} ${fdt_addr_r} ${prefix}${efi_fdtfile}
loadaddr=0x82000000
loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenvfile}
loadbootscript=load mmc ${mmcdev} ${loadaddr} boot.scr
loadfdt=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
loadfit=run args_mmc; bootm ${loadaddr}#${fdtfile};
loadimage=load ${devtype} ${bootpart} ${loadaddr} ${bootdir}/${bootfile}
loadramdisk=load mmc ${mmcdev} ${rdaddr} ramdisk.gz
mmc_boot=if mmc dev ${devnum}; then setenv devtype mmc; run scan_dev_for_boot_part; fi
mmcboot=mmc dev ${mmcdev}; setenv devnum ${mmcdev}; setenv devtype mmc; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadimage; then if test ${boot_fit} -eq 1; then run loadfit; else r;
mmcdev=0
mmcloados=run args_mmc; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdtaddr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot lo;
mmcrootfstype=ext4 rootwait
mtdids=nand0=nand.0
mtdparts=mtdparts=nand.0:128k(NAND.SPL),128k(NAND.SPL.backup1),128k(NAND.SPL.backup2),128k(NAND.SPL.backup3),256k(NAND.u-boot-spl-os),1m(NAND.u-boot),128k(NAND.u-boot-env),128k(NAND.u-boot-env.backup1),8m)
nandargs=setenv bootargs console=${console} ${optargs} root=${nandroot} rootfstype=${nandrootfstype}
nandboot=echo Booting from nand ...; run nandargs; nand read ${fdtaddr} NAND.u-boot-spl-os; nand read ${loadaddr} NAND.kernel; bootz ${loadaddr} - ${fdtaddr}
nandroot=ubi0:rootfs rw ubi.mtd=NAND.file-system,2048
nandrootfstype=ubifs rootwait=1
netargs=setenv bootargs console=${console} ${optargs} root=/dev/nfs nfsroot=${serverip}:${rootpath},${nfsopts} rw ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}::off
netboot=echo Booting from network ...; setenv autoload no; dhcp; run netloadimage; run netloadfdt; run netargs; bootz ${loadaddr} - ${fdtaddr}
netloadfdt=tftp ${fdtaddr} ${fdtfile}
netloadimage=tftp ${loadaddr} ${bootfile}
netmask=255.255.255.0
nfsopts=nolock
optargs=g_ether.dev_addr=50:65:83:d5:08:dc nfsrootdebug
partitions=uuid_disk=${uuid_gpt_disk};name=rootfs,start=2MiB,size=-,uuid=${uuid_gpt_rootfs}
pxefile_addr_r=0x80100000
ramargs=setenv bootargs console=${console} ${optargs} root=${ramroot} rootfstype=${ramrootfstype}
ramboot=echo Booting from ramdisk ...; run ramargs; bootz ${loadaddr} ${rdaddr} ${fdtaddr}
ramdisk_addr_r=0x88080000
ramroot=/dev/ram0 rw
ramrootfstype=ext2
rdaddr=0x88080000
rootpath=/export/rootfs
scan_dev_for_boot=echo Scanning ${devtype} ${devnum}:${distro_bootpart}...; for prefix in ${boot_prefixes}; do run scan_dev_for_extlinux; run scan_dev_for_scripts; done;run scan_dev_for_efi;
scan_dev_for_boot_part=part list ${devtype} ${devnum} -bootable devplist; env exists devplist || setenv devplist 1; for distro_bootpart in ${devplist}; do if fstype ${devtype} ${devnum}:${distro_bootpart}e
scan_dev_for_efi=setenv efi_fdtfile ${fdtfile}; if test -z "${fdtfile}" -a -n "${soc}"; then setenv efi_fdtfile ${soc}-${board}${boardver}.dtb; fi; for prefix in ${efi_dtb_prefixes}; do if test -e ${devtye
scan_dev_for_extlinux=if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefix}extlinux/extlinux.conf; then echo Found ${prefix}extlinux/extlinux.conf; run boot_extlinux; echo SCRIPT FAILED: continuingi
scan_dev_for_scripts=for script in ${boot_scripts}; do if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefix}${script}; then echo Found U-Boot script ${prefix}${script}; run boot_a_script; echo SCRIe
scriptaddr=0x80000000
serverip=192.168.2.1
soc=am33xx
spiargs=setenv bootargs console=${console} ${optargs} root=${spiroot} rootfstype=${spirootfstype}
spiboot=echo Booting from spi ...; run spiargs; sf probe ${spibusno}:0; sf read ${loadaddr} ${spisrcaddr} ${spiimgsize}; bootz ${loadaddr}
spibusno=0
spiimgsize=0x362000
spiroot=/dev/mtdblock4 rw
spirootfstype=jffs2
spisrcaddr=0xe0000
static_ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}::off
stderr=serial@44e09000
stdin=serial@44e09000
stdout=serial@44e09000
update_to_fit=setenv loadaddr ${fit_loadaddr}; setenv bootfile ${fit_bootfile}
usb_boot=usb start; if usb dev ${devnum}; then setenv devtype usb; run scan_dev_for_boot_part; fi
usbnet_devaddr=50:65:83:d5:08:dc
vendor=ti
ver=U-Boot 2017.01-00444-g4e7f4689e5-dirty (Jan 18 2018 - 15:10:52 +0100)