Part Number: OMAP-L138
Other Parts Discussed in Thread: OMAPL138, TCA6416
Tool/software: Code Composer Studio
Hi all,
I am trying to load one of the I2C example codes provided with Starterware_1_10_04_01 ("i2cLedBlink"), and am having an error appear that there are undefined symbols (_I2CPinMuxSetup, etc) . In addition, when running other example codes we consistently get identifier is undefined. I was hoping to get this code up and running to understand I2C on the device and hopefully get it to connect to an external microcontroller such as Arduino.
For reference, I am using CCv5.5.0.00077
Any help would be appreciated; thank you in advance!