Part Number: AM5K2E02
My customer is using the AM5K2E02. I'm looking to get a few questions answered for the customer before they proceed with this processor:
- Is the programming done over the JTAG?
- Is external program memory needed? If so which is the best interface to use for it?
- Is this the same as boot memory mentioned in the documents? SPI interface or EMIF16 interface?
- For the EMIF16 interface, it says the interface runs at CPU CLK/6. For the 1.4Ghz part, that would be 233Mhz. There doesn’t seem to be any industrial grade NAND or NOR parallel Flash that run at that speed.
- Is the 60-pin emulation connector a standard pin out for connection to a specific emulator?
- Can the PCIe be setup to act like a DMA interface, with handshaking done with the GPIO?
- What external chips are required for the USB 3.0 and 1GBE interfaces to external connectors?
- If we are storing multiple GUI page layouts in memory, is the NAND Flash the best for this?
- What special connections do we have to have to use all the GPIO for handshaking to external devices? Some of the GPIO must be pin-strapped during boot to set certain modes?