This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM388: YUV 24bit capture on VIP1

Part Number: DM388

Hi All,

I am using DM388 evm with IPNC 3.9.1 rdk.

Is it possible to capture 24 bit YUV on VIP1 port?

For creating YUV 24 bit below mentioned not support yet?

ti_tools/hdvpss_01_00_01_37/packages/ti/psp/vps/core/src/vpscore_vipResCommon.c

if (Vcore_vipResIsInSrcSingleChYuv444 ( pObj->resParams.inSrc ) )
    {
        /*
         * input source is single-channel RGB - NOT SUPPORTED AS OF NOW
         */
         status = FVID2_EFAIL;
     }

Can you confirm RGB888 only support on 24bit capture?

Regards,

RAJM