Other Parts Discussed in Thread: OMAP-L138
Tool/software: TI-RTOS
Hello Community,
i have a Mity-DSP with OMAP-L138 here and see some difficulties when running my application from SPI-Flash.
It is the NDK Clientexample wit server.
If i run the applicatioon with the mity-DSP gel file after resetted Device all works fine.
I then successfull flashed the application to the SPI via u-boot and started from there.
My Programm looks like:
Main
{
blink some LED
UARTOUT some Debug Info
BIOSStart()
}
alivetask
{
Blink LED
}
After some investigations i found out that SYS/Bios is not started .
To verify that i excluded the NDK Functionality so that only the alive task is left.
I see Blinking LED and UART-communication before SYS/BIOS Start.
But even with only one task SYS/Bios will not start.
Can someone tell me what i am missing?
Many thanks in advance for any help.
Regards Martin