This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3352: Kernel boot issue

Part Number: AM3352

Tool/software: Linux

Hi All,

First Version:

We have made a customised board with AM3352 processor, 1GB DDR3 and 512MB NAND flash. On our First version customised board we have made the setup working due to some hardware issue in the Ethernet section we have gone for the  second version.  We made SD Card booting done in first revision. 

SYSBOOT :  0000001000110011 - NAND   NANDI2C  MMC0  UART0

Second Version:

We have made a customised board with AM3352 processor, 1GB DDR3 and 8GB eMMC flash. This is our second revision customised Board. Changes are done in Ethernet section and changed from NAND Flash to eMMC Flash. 

SYSBOOT :  0000000000110111  - MMC0   SPI0  UART0   USB0

But when we are using the same setup the Booting Hangs in Starting Kernel....  . 


What can be the issue ?

Any changes has to be done in U-boot or kernel?

  • What Linux version are you using? Where is the eMMC connected? Do you still boot from SD card on the second board?
  • Hi Biser,

    1. What Linux version are you using?

    Linux Version - 4.4.41

    2. Where is the eMMC connected?

    eMMC is connected to MMC1

    SD card is connected to MMC0

    3. Do you still boot from SD card on the second board?

    Yes.

    Regards,

    Avinash N

  • Can you share the bootlog & the output of printenv in u-boot prompt?

    Best Regards,
    Yordan
  • Also, stopping your boot at "Starting kernel..." usually indicates erroneous dtb. Can you also share the old & the new version of your dts?

    Best Regards,
    Yordan
  • Hi Yordan,

    1. Bootlog:

    U-Boot SPL 2017.11-rc3-00022-g43ede0b-dirty (Nov 07 2017 - 13:14:21)
    Trying to boot from MMC1
    *** Warning - bad CRC, using default environment

    reading u-boot.img
    reading u-boot.img
    reading u-boot.img
    reading u-boot.img


    U-Boot 2017.01-00319-geae4602-dirty (Jan 24 2018 - 11:56:36 +0530)

    CPU : AM3352
    DRAM: 1 GiB
    WARNING: Caches not enabled
    MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
    *** Error - No Valid Environment Area found
    *** Warning - bad CRC, using default environment

    In: serial@44e09000
    Out: serial@44e09000
    Err: serial@44e09000
    <ethaddr> not set. Validating first E-fuse MAC
    Net: Enabling MII Mode ....Done.
    i = 5
    Detected PHY ID = 0x221450
    Phy ID = 0x221450
    cpsw connected to Generic PHY
    cpsw
    Hit any key to stop autoboot: 0
    =>
    =>
    => boot
    switch to partitions #0, OK
    mmc0 is current device
    SD/MMC found on device 0
    reading boot.scr
    ** Unable to read file boot.scr **
    reading uEnv.txt
    ** Unable to read file uEnv.txt **
    switch to partitions #0, OK
    mmc0 is current device
    Scanning mmc 0:1...
    switch to partitions #0, OK
    mmc0 is current device
    SD/MMC found on device 0
    3049432 bytes read in 495 ms (5.9 MiB/s)
    35728 bytes read in 35 ms (996.1 KiB/s)
    ## Flattened Device Tree blob at 88000000
    Booting using the fdt blob at 0x88000000
    Loading Device Tree to 8fff4000, end 8ffffb8f ... OK

    Starting kernel ...

    2. Printenv :

    arch=arm
    args_mmc=run finduuid;setenv bootargs console=${console} ${optargs} root=PARTUUID=${uuid} rw rootfstype=${mmcrootfstype}
    baudrate=115200
    board_name=A335BNLT
    board_rev=000C
    board_serial=1315BBBK1334
    boot_a_script=load ${devtype} ${devnum}:${distro_bootpart} ${scriptaddr} ${prefix}${script}; source ${scriptaddr}
    boot_efi_binary=load ${devtype} ${devnum}:${distro_bootpart} ${kernel_addr_r} efi/boot/bootarm.efi; if fdt addr ${fdt_addr_r}; then bootefi ${kernel_addr_r} ${fdt_addr_r};else bootefi ${kernel_addr_r} ${fdtc
    ontroladdr};fi
    boot_extlinux=sysboot ${devtype} ${devnum}:${distro_bootpart} any ${scriptaddr} ${prefix}extlinux/extlinux.conf
    boot_fdt=try
    boot_fit=0
    boot_net_usb_start=usb start
    boot_prefixes=/ /boot/
    boot_script_dhcp=boot.scr.uimg
    boot_scripts=boot.scr.uimg boot.scr
    boot_targets=mmc0 legacy_mmc0 mmc1 legacy_mmc1 nand0 pxe dhcp
    bootcmd=if test ${boot_fit} -eq 1; then run update_to_fit;fi;run findfdt; run init_console; run envboot; run distro_bootcmd
    bootcmd_dhcp=run boot_net_usb_start; if dhcp ${scriptaddr} ${boot_script_dhcp}; then source ${scriptaddr}; fi;setenv efi_fdtfile ${fdtfile}; if test -z "${fdtfile}" -a -n "${soc}"; then setenv efi_fdtfile ${
    soc}-${board}${boardver}.dtb; fi; setenv efi_old_vci ${bootp_vci};setenv efi_old_arch ${bootp_arch};setenv bootp_vci PXEClient:Arch:00010:UNDI:003000;setenv bootp_arch 0xa;if dhcp ${kernel_addr_r}; then tftp
    boot ${fdt_addr_r} dtb/${efi_fdtfile};if fdt addr ${fdt_addr_r}; then bootefi ${kernel_addr_r} ${fdt_addr_r}; else bootefi ${kernel_addr_r} ${fdtcontroladdr};fi;fi;setenv bootp_vci ${efi_old_vci};setenv boot
    p_arch ${efi_old_arch};setenv efi_fdtfile;setenv efi_old_arch;setenv efi_old_vci;
    bootcmd_legacy_mmc0=setenv mmcdev 0; setenv bootpart 0:2 ; run mmcboot
    bootcmd_legacy_mmc1=setenv mmcdev 1; setenv bootpart 1:2 ; run mmcboot
    bootcmd_mmc0=setenv devnum 0; run mmc_boot
    bootcmd_mmc1=setenv devnum 1; run mmc_boot
    bootcmd_nand=run nandboot
    bootcmd_pxe=run boot_net_usb_start; dhcp; if pxe get; then pxe boot; fi
    bootcount=1
    bootdelay=2
    bootdir=/boot
    bootenvfile=uEnv.txt
    bootfile=zImage
    bootm_size=0x10000000
    bootpart=0:2
    bootscript=echo Running bootscript from mmc${mmcdev} ...; source ${loadaddr}
    console=ttyO0,115200n8
    cpu=armv7
    dfu_alt_info_emmc=rawemmc raw 0 3751936
    dfu_alt_info_mmc=boot part 0 1;rootfs part 0 2;MLO fat 0 1;MLO.raw raw 0x100 0x100;u-boot.img.raw raw 0x300 0x400;spl-os-args.raw raw 0x80 0x80;spl-os-image.raw raw 0x900 0x2000;spl-os-args fat 0 1;spl-os-im
    age fat 0 1;u-boot.img fat 0 1;uEnv.txt fat 0 1
    dfu_alt_info_nand=SPL part 0 1;SPL.backup1 part 0 2;SPL.backup2 part 0 3;SPL.backup3 part 0 4;u-boot part 0 5;u-boot-spl-os part 0 6;kernel part 0 8;rootfs part 0 9
    dfu_alt_info_ram=kernel ram 0x80200000 0x4000000;fdt ram 0x80f80000 0x80000;ramdisk ram 0x81000000 0x4000000
    distro_bootcmd=for target in ${boot_targets}; do run bootcmd_${target}; done
    efi_dtb_prefixes=/ /dtb/ /dtb/current/
    envboot=mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadbootscript; then run bootscript;else if run loadbootenv; then echo Loaded env from ${bootenvfile};run importboo
    tenv;fi;if test -n $uenvcmd; then echo Running uenvcmd ...;run uenvcmd;fi;fi;fi;
    eth1addr=38:d2:69:ac:d0:bd
    ethact=cpsw
    ethaddr=38:d2:69:ac:d0:bb
    fdt_addr_r=0x88000000
    fdtaddr=0x88000000
    fdtcontroladdr=bdf45780
    fdtfile=undefined
    findfdt=if test $board_name = A335BONE; then setenv fdtfile am335x-bone.dtb; fi; if test $board_name = A335BNLT; then setenv fdtfile am335x-boneblack.dtb; fi; if test $board_name = BBG1; then setenv fdtfile
    am335x-bonegreen.dtb; fi; if test $board_name = A33515BB; then setenv fdtfile am335x-evm.dtb; fi; if test $board_name = A335X_SK; then setenv fdtfile am335x-evmsk.dtb; fi; if test $board_name = A335_ICE; the
    n setenv fdtfile am335x-icev2.dtb; fi; if test $fdtfile = undefined; then echo WARNING: Could not determine device tree to use; fi;
    finduuid=part uuid mmc ${bootpart} uuid
    fit_bootfile=fitImage
    fit_loadaddr=0x87000000
    importbootenv=echo Importing environment from mmc${mmcdev} ...; env import -t ${loadaddr} ${filesize}
    init_console=if test $board_name = A335_ICE; then setenv console ttyO3,115200n8;else setenv console ttyO0,115200n8;fi;
    kernel_addr_r=0x82000000
    load_efi_dtb=load ${devtype} ${devnum}:${distro_bootpart} ${fdt_addr_r} ${prefix}${efi_fdtfile}
    loadaddr=0x82000000
    loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenvfile}
    loadbootscript=load mmc ${mmcdev} ${loadaddr} boot.scr
    loadfdt=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
    loadfit=run args_mmc; bootm ${loadaddr}#${fdtfile};
    loadimage=load ${devtype} ${bootpart} ${loadaddr} ${bootdir}/${bootfile}
    loadramdisk=load mmc ${mmcdev} ${rdaddr} ramdisk.gz
    mmc_boot=if mmc dev ${devnum}; then setenv devtype mmc; run scan_dev_for_boot_part; fi
    mmcboot=mmc dev ${mmcdev}; setenv devnum ${mmcdev}; setenv devtype mmc; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadimage; then if test ${boot_fit} -eq 1; then run loadfit; else run
    mmcloados;fi;fi;fi;
    mmcdev=0
    mmcloados=run args_mmc; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdtaddr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load
    the DT; fi; fi; else bootz; fi;
    mmcrootfstype=ext4 rootwait
    mtdids=nand0=nand.0
    mtdparts=mtdparts=nand.0:128k(NAND.SPL),128k(NAND.SPL.backup1),128k(NAND.SPL.backup2),128k(NAND.SPL.backup3),256k(NAND.u-boot-spl-os),1m(NAND.u-boot),128k(NAND.u-boot-env),128k(NAND.u-boot-env.backup1),8m(NA
    ND.kernel),-(NAND.file-system)
    nandargs=setenv bootargs console=${console} ${optargs} root=${nandroot} rootfstype=${nandrootfstype}
    nandboot=echo Booting from nand ...; run nandargs; nand read ${fdtaddr} NAND.u-boot-spl-os; nand read ${loadaddr} NAND.kernel; bootz ${loadaddr} - ${fdtaddr}
    nandroot=ubi0:rootfs rw ubi.mtd=NAND.file-system,2048
    nandrootfstype=ubifs rootwait=1
    netargs=setenv bootargs console=${console} ${optargs} root=/dev/nfs nfsroot=${serverip}:${rootpath},${nfsopts} rw ip=dhcp
    netboot=echo Booting from network ...; setenv autoload no; dhcp; run netloadimage; run netloadfdt; run netargs; bootz ${loadaddr} - ${fdtaddr}
    netloadfdt=tftp ${fdtaddr} ${fdtfile}
    netloadimage=tftp ${loadaddr} ${bootfile}
    nfsopts=nolock
    partitions=uuid_disk=${uuid_gpt_disk};name=rootfs,start=2MiB,size=-,uuid=${uuid_gpt_rootfs}
    pxefile_addr_r=0x80100000
    ramargs=setenv bootargs console=${console} ${optargs} root=${ramroot} rootfstype=${ramrootfstype}
    ramboot=echo Booting from ramdisk ...; run ramargs; bootz ${loadaddr} ${rdaddr} ${fdtaddr}
    ramdisk_addr_r=0x88080000
    ramroot=/dev/ram0 rw
    ramrootfstype=ext2
    rdaddr=0x88080000
    rootpath=/export/rootfs
    scan_dev_for_boot=echo Scanning ${devtype} ${devnum}:${distro_bootpart}...; for prefix in ${boot_prefixes}; do run scan_dev_for_extlinux; run scan_dev_for_scripts; done;run scan_dev_for_efi;
    scan_dev_for_boot_part=part list ${devtype} ${devnum} -bootable devplist; env exists devplist || setenv devplist 1; for distro_bootpart in ${devplist}; do if fstype ${devtype} ${devnum}:${distro_bootpart} bo
    otfstype; then run scan_dev_for_boot; fi; done
    scan_dev_for_efi=setenv efi_fdtfile ${fdtfile}; if test -z "${fdtfile}" -a -n "${soc}"; then setenv efi_fdtfile ${soc}-${board}${boardver}.dtb; fi; for prefix in ${efi_dtb_prefixes}; do if test -e ${devtype}
    ${devnum}:${distro_bootpart} ${prefix}${efi_fdtfile}; then run load_efi_dtb; fi;done;if test -e ${devtype} ${devnum}:${distro_bootpart} efi/boot/bootarm.efi; then echo Found EFI removable media binary efi/b
    oot/bootarm.efi; run boot_efi_binary; echo EFI LOAD FAILED: continuing...; fi; setenv efi_fdtfile
    scan_dev_for_extlinux=if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefix}extlinux/extlinux.conf; then echo Found ${prefix}extlinux/extlinux.conf; run boot_extlinux; echo SCRIPT FAILED: continuing...
    ; fi
    scan_dev_for_scripts=for script in ${boot_scripts}; do if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefix}${script}; then echo Found U-Boot script ${prefix}${script}; run boot_a_script; echo SCRIPT
    FAILED: continuing...; fi; done
    scriptaddr=0x80000000
    soc=am33xx
    spiargs=setenv bootargs console=${console} ${optargs} root=${spiroot} rootfstype=${spirootfstype}
    spiboot=echo Booting from spi ...; run spiargs; sf probe ${spibusno}:0; sf read ${loadaddr} ${spisrcaddr} ${spiimgsize}; bootz ${loadaddr}
    spibusno=0
    spiimgsize=0x362000
    spiroot=/dev/mtdblock4 rw
    spirootfstype=jffs2
    spisrcaddr=0xe0000
    static_ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}::off
    stderr=serial@44e09000
    stdin=serial@44e09000
    stdout=serial@44e09000
    update_to_fit=setenv loadaddr ${fit_loadaddr}; setenv bootfile ${fit_bootfile}
    usb_boot=usb start; if usb dev ${devnum}; then setenv devtype usb; run scan_dev_for_boot_part; fi
    usbnet_devaddr=38:d2:69:ac:d0:bb
    ver=U-Boot 2017.01-00319-geae4602-dirty (Jan 24 2018 - 11:56:36 +0530)

    Environment size: 9097/131067 bytes

    3. DTB:

    We are using the same DTB for old and new board.

    Regards,
    Avinash N

  • Hi,

    3. DTB:

    We are using the same DTB for old and new board.


    You should change the dts file to match your new board, that is reflect the hardware changes:
    "We have made a customised board with AM3352 processor, 1GB DDR3 and 8GB eMMC flash. This is our second revision customised Board. Changes are done in Ethernet section and changed from NAND Flash to eMMC Flash. "

    Best Regards,
    Yordan
  • Hi Yordan,

    What changes has to be done in DTB. In our second revision boards we enabled the eMMC flash section. 

    Can you provide any sample DTB for the eMMC enabled DTB files.

    Regards,

    Avinash N

  • Can you share your dts & dtsi files?

    Best Regards,
    Yordan
  • Hi Yordan,

    I Have attached the dts and dtsi filesU-BOOT_DTS.zip. 

  • The dts seems ok. Can you confirm that you haven't modified anything else in your board (some power supply or something like that)?

    Can you enable the early debug prints in menuconfig:
    Kernel hacking->
    [*] Kernel low-level debugging functions
    [*] Early printk

    Best Regards,
    Yordan