This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2EXEVM: TDA2Ex UART Short issue

Part Number: TDA2EXEVM

When the UART Line(D26,D28) is short with BAT+(12V), then both SoC's Core_VDD and VDD_1V8 are short. which Core_VDD(PMIC PIN 9 10 11) and VDD_1V8(PMIC PIN 17 18 19 ) are from PMIC TPS65917

is this normal operation?