This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2L06: IQN2 with custom signal packets

Part Number: 66AK2L06

Hello,

So I am attempting to get the IQNET2 on our board running along with the DFE and the JESD interface to receive custom packets that we are receiving (non-LTE and non-WCDMA). Which settings for IQN2 should I use since it appears most of them are split up in to either WCDMA or LTE. Which of these should I use in order to set up reception of my custom length and data packets?

Thanks so much!