Part Number: AM5726
Other Parts Discussed in Thread: AM5729, AM5728, BEAGLEBOARD-X15, TPS659037
Hi Sitara Team,
I have a customer currently working on a design utilizing the AM5726.
They are using the Yocto Linux build on the BeagleBoard x15 rev. B1 (AM5729) to familiarize themselves with the AM57x family.
One issue they've noticed, is detecting a loss-of-power condition using the VSYS_MON interrupt from the x15’s TPS65903x.
They have tried creating a generic-uio device with a gpio1_0 interrupt in the device tree, but the existing tps659038 device in the .dts already uses gpio1_0 (presumably for the palmas RTC), so the uio_pdrv_genirq module is unable to create my device as /dev/uio0.
Any answers or resources you can point us to would be incredibly helpful. They can provide snippets of the current device tree if it would be useful. So far they’ve been able to resolve most of their issues by searching for answers on the TI E2E forums, but they haven’t found much information on handling interrupts on PMIC_INT connected to the Wakeup0 line in the Beagle x15.
Thanks!
Barend