Other Parts Discussed in Thread: OMAP3530
Hi,all
I downloaded the CE2.24 and build the source code under "codec_engine_2_24\packages\ti\sdo\ce\ipc\dsplink" following the Readme.txt , and when build it , errors below turn up:
E:\CE_WinCE\codec_engine_2_24\packages\ti\sdo\ce\ipc\dsplink>gmake
E:/CE_WinCE/xdctools_3_10_05_61/xdc XDCPATH="E:/CE_WinCE/codec_engine_2_24/examp
les;E:/CE_WinCE/codec_engine_2_24/cetools/packages;E:/CE_WinCE/codec_engine_2_24
/packages;E:/CE_WinCE/codec_engine_2_24/cetools/packages" all
making package.mak (because of package.bld) ...
config.bld: Running the version from Codec Engine Examples.
js: "E:/CE_WinCE/codec_engine_2_24/examples/ti/sdo/ce/examples/buildutils/Platfo
rms.xs", line 75: TypeError: Cannot call method "match" of undefined (E:/CE_WinC
E/codec_engine_2_24/examples/ti/sdo/ce/examples/buildutils/Platforms.xs#75)
"E:/CE_WinCE/codec_engine_2_24/examples/config.bld", line 138
all files complete.
Would someone give me some help to fix it?
Thanks & Best Regards,
Stephen