Part Number: AM3352
Hi,
Could you please provide us the Adjusted Peak Performance(APP) of AM335x?
Device: AM3352BZCZA100 (1GHz Version)
Best Regards
Paddu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Paddu
Sorry for the late response
AM335x at 1 GHz Adjusted Peak Performance (APP) = 0.0003 WT
- NEON can only do 32b fp operations
- Therefore VFPv4 is the item to measure, and it can do 1FMA/cycle = 1 DP FLOPS / cycle
- AM335x (Single Cortex A8) APP = 1x 1 FLOPS/cyc * 1.0GHz * 0.3 / 1000 = .0003 WT (Weighted TeraFlops)
- Assumption is that VFP is a non-vector processing unit (based on the official definition in the Practitioner’s Guide) so using the 0.3 scale factor.