This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5718: Slowing down A15 when running DSP at max speed

Part Number: AM5718

Hello everybody , 

please I need to run DSP at max speed ,  while A15 is very low charged  ( ideally I can go < 10% usage )  .

So I would like  , keeping DSP at max speed , to use on A15 at  "slow clock " to save power  :  do you see any limitation in doing this , like a min ratio between the two or something similar ? 

I have linux on A15 and Tirtos on DSP 

thank you 

regards

Carlo