Part Number: TMS320C6670
Tool/software: Code Composer Studio
Hi , I have a custom board using 6670.6670 connect to two FPGA ,6670 SRIO lane 0 and lane1 connect to FPGA1,lane 2 and lane 3 connect to FPGA 2.
SRIO ref_clk is 250MHz,serial rate is 3.125Gbps. I wang to set two X2 mode. I use SRIO_LoopbackDioIsrexampleproject demo.
// Set MPY to 6.25x
CSL_BootCfgSetSRIOSERDESConfigPLL (0x233);
//3.125G
/* Configure the SRIO SERDES Receive Configuration. */
CSL_BootCfgSetSRIOSERDESRxConfig (0, 0x00440495);
CSL_BootCfgSetSRIOSERDESRxConfig (1, 0x00440495);
CSL_BootCfgSetSRIOSERDESRxConfig (2, 0x00440495);
CSL_BootCfgSetSRIOSERDESRxConfig (3, 0x00440495);
/* Configure the SRIO SERDES Transmit Configuration. */
CSL_BootCfgSetSRIOSERDESTxConfig (0, 0x00180795);
CSL_BootCfgSetSRIOSERDESTxConfig (1, 0x00080795);
CSL_BootCfgSetSRIOSERDESTxConfig (2, 0x00180795);
CSL_BootCfgSetSRIOSERDESTxConfig (3, 0x00080795);
/* Configure the path mode for the ports. */
for(i = 0; i < 4; i++)
CSL_SRIO_SetPLMPortPathControlMode (hSrio, i, 3);
This will result DSP can transmit SWRITE packet to FPGA1,but cannot receive SWRITE packet from FPGA1.
However,DSP can receive SWRITE packet from FPGA2.
I dont know how to cimplement two X2 mode , please help me.
Regards,
Tian