This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6437 boot



Dear all

 I have some questions about the boot loader.Some programs I can correctly boot through SPI24,such as the program "client" which is a program of ndk.Although I wrote one program can be programmed in to Flash, but can not be properly boot.Then I connected CCS,and restarted any program(only "restart" not download the program),so the program which burned in Flash can running correctly.I guess this problem  caused by the document of gel.Did anybody encountered a similar situation? Thank you!

-allan

  • Hi allan

    Once I builded a program (blink a led) without the gel file. After this, I runed the gel file just to burn the program into the NOR, and the program runed without problem after boot!

    Marcio