Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5726: IPU crash

Part Number: AM5726

Tool/software: Linux

Hello,

I am using am5726 custom board. In this i am running g-streamer application which uses ducatijpegdec and ducatih264enc module.

Application get stops after 3 days and throw below message on dmesg.

[113442.967982]  remoteproc1: crash detected in 55020000.ipu: type watchdog
[113442.974856]  remoteproc1: handling crash #1 in 55020000.ipu
[113442.980694]  remoteproc1: recovering 55020000.ipu
[113442.986441]  remoteproc1: can't stop rproc: -22
[113447.967977]  remoteproc1: crash detected in 55020000.ipu: type watchdog


Please help me to resolve the issue.

Regards,

Prerak