This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DRA722: DRA722

Part Number: DRA722

Tool/software: Linux

Hi Sir,

I need to program spi nor flash device and I have added new device, "is25wp064q" as below, in the m25p80.c. And I have enabled its driver with insert mode in the "device drivers/Memory Technology Device (MTD) support/Self-contained MTD device drivers/Support most SPI Flash chips (AT26DF, M25P, W25X, ...) by "make linux_menuconfig" command. After building kernel image, I can see the " m25p80.ko" but I cannot see the mtd device by "cat /proc/mtd" after inserting "m25p80.ko".  How should I do if I want to program SPI nor flash in user space? 

static const struct spi_device_id m25p_ids[] = {
/* ISSI -- is25wp0xxa */
{ "is25wp064q", INFO(0x9D7017, 0, 64 * 1024, 128, 0) },...

{ },
};

Best Regards

Kevin