This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2HG: 12bit Camera to 16/24 Bit VIP interface connection

Part Number: TDA2HG

Greetings

I want to interface 12bit cameras/FPD Link Deserializers to VIP1, 2 and 3 port on TDA2x

I suppose we configure VIP as a 16 bit port but only connect 12pins.

Do I use Vinx_d0 to Vinx_d11 and connect the remaining 4 pins to GND or do I use Vinx_d4 to Vinx_d16 and connect Vin_d0 to -d3 to GND?

Can I even use the remaining 4 pins for GPIO?

Regards