This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368IPNC - increase DDR size



Hi,

I would like to change DDR size from 128MB to 256MB on DM368IPNC_IMX036 ver 2.0.0 reference design based board.
What software changes need to be done.
I looked at u-boot code in davinci_dm368_ipnc.h  :

/* Memory Info */
/*=============*/
#define CFG_MALLOC_LEN  (0x40000 + 128*1024)  /* malloc () len */
#define CFG_GBL_DATA_SIZE 128  /* reserved for initial data */
#define CFG_MEMTEST_START 0x82000000 /* memtest start address  */
#define CFG_MEMTEST_END  0x90000000 /* 16MB RAM test      */
#define CONFIG_NR_DRAM_BANKS 1  /* we have 1 bank of DRAM */
#define CONFIG_STACKSIZE (256*1024) /* regular stack   */
#define PHYS_SDRAM_1  0x80000000 /* DDR Start     */
#define PHYS_SDRAM_1_SIZE 0x8000000 /* DDR size 128MB    */

Is there sufficient just to increase PHYS_SDRAM_1_SIZE to 256MB.
Do i need  to change any other code in bootloaders or Linux.

Best regards,
Marko.