Part Number: AM3352
Hi,
a customer has EMI issues on AM3352 PCLK (harmonics of the PCLK pixel clock at 25MHz) and is trying to mititgate with series reisistor and setting the slew rate in the register for the PCLK.
We are looking at the register
conf_lcd_pclk at offset 0x8E8
Bit 6 is the slew rate either fast or slow.
If we set the bit to 1 for slow slew rate, the behavior is NOT changing. Can someone confirm that this bit can be set and will have an effect on the slew rate of PCLK?
Thanks!
--Gunter