Part Number: TDA2EXEVM
Tool/software: Linux
hi
I use the TDA2EG chip,tansfer linux 4.4 to our own board,the log as follow:
I have some question:
Q1: failed to load ....
[11:17:48][ 61.524405] remoteproc0: failed to load dra7-ipu1-fw.xem4
[11:17:48][ 61.604375] remoteproc1: failed to load dra7-ipu2-fw.xem4
[11:17:48][ 61.704374] remoteproc2: failed to load dra7-dsp1-fw.xe66
in the /lib/firware has load dra7-ipu1-fw.xem4、dra7-ipu2-fw.xem4、dra7-dsp1-fw.xe66 files。why don't load?
Q2: Failed to start Load Kernel Modules. why?
Q3: [11:28:51][ 724.609768] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[11:33:24][ 997.196820] EXT4-fs (mmcblk1p2): recovery complete
[11:33:24][ 997.213590] EXT4-fs (mmcblk1p2): mounted filesystem
why remount cosume too much time? 5min,
Q4: [11:44:22][ 1655.715224] random: nonblocking pool is initialized
dead when start ?