Part Number: AM5726
Tool/software: Linux
Hello,
We are working on AM5726 custom board.
Ethernet link is working fine with 100Mbps, but when it's connected to the 1Gbps it's link is continuously toggling.
Please find below log message for the same.
[ 92.195355] cpsw 48484000.ethernet eth0: Link is Down
[ 93.206387] cpsw 48484000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 103.215356] cpsw 48484000.ethernet eth0: Link is Down
[ 105.226388] cpsw 48484000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 111.235346] cpsw 48484000.ethernet eth0: Link is Down
[ 113.246387] cpsw 48484000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 119.255345] cpsw 48484000.ethernet eth0: Link is Down
[ 121.266387] cpsw 48484000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 126.275345] cpsw 48484000.ethernet eth0: Link is Down
Please do the needful and let me know in case of any more information required.
Regards,
Ronak