Part Number: AM5726
Hi Support,
my customer is facing issues in adopting DDR3 with ECC with AM5726.
In particular, they generate all four pinmux files, they use the ‘BOARD=evmAM572x’ make option so all custom modifications are done for evmAM572x specific sources.
They have successfully built and tested SBL loaded from SDMMC and performed a DRAM size detection and memtest. But when they enable ECC (they re-used code from idkAM572x sources) the SBL crashes on ‘Board_init(boardCfg)’ function call with ‘BOARD_INIT_DDR_ECC’ flag enabled (not used JTAG debugger to find the specific failing code position yet).
Can you help me finding out the root of this issue? I have sources in case of need.
Thanks in advance,
regards,
Alberto