This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS: VisionSDK - IPU2 Display Server + Camera & IPU1 Multimedia

Tool/software: TI-RTOS

Hi all,

We are using vision sdk IPU2 for camera & also as Display-server.(VisonSDK 3 dot 1 version).

We have two questions. 

1. Consider IPU1 is used for Multimedia. & IPU2 for Display Server (GFX) + camera (VID1) .


In this case , it is possible to send the decoded data directly to IPU2 from IPU1 without USING WAYLAND-buffer OF a15 in a separate Pipeline line ?


2. Consider IPU2 is used with Multimedia,along with Display Server & camera.

Is it possible to send show the decoded data in IPU2 directly without resending to A15(waylandsink) ?

Currenlty we are using following gstreamer command from A15. Instead of wayalndsink, is it possible to have a gstreamer-plugin to handle in IPU2 ?

gst-launch-1.0 filesrc location=/tmp/SDCard_Slot-1/test.MP4 ! qtdemux ! h264parse ! ducatih264dec ! waylandsink

Regards,

Gokul