This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: USB Host and Device on GP EVM

Guru 20755 points
Part Number: AM5728

Tool/software: Linux

Hello,

We need to use both usb host and usb device with am572x EVB.

I see in dwc3 wiki, that examples are for configuring both as host or both as client, so I am not sure if it's possible (to use one port as host and the other as client) .

in the wiki it is said

"AM57xx-evm use USB1 as Super-Speed host port and have a on-board Super-Speed hub which provides 3 Super-Speed Host (Type-A) ports. USB2 is used as High-Speed peripheral port. VBUS detection for USB2 port is provided through Power Management IC (palmas). " , so the assumption is that both should work at the same time, Right ?

Best Regards,

Ran