Hello,
I have a question about setting sensor clock.
If I have HD/VD as input, do I need to set any clock rate on DM6446 side to sync. with sensor or I just leave it as a slave since all clock and signals come from sensor side?
I also read from data sheet, that CCDC supports 75 MHz sensor clock and may up to 90MHz in turbo mode. Do I need to turn this 90MHz ON or I just let 90MHz clock input into DM6446 and it works automatically?
Thanks
Bell Hsu