Part Number: DRA750
Other Parts Discussed in Thread: DRA752
Tool/software: Linux
Dear Sir,
We use TPS65917 PMIC and DRA752 CPU on our customized board.
We cannot bring up successfully and no any message output on the console.
So we tried to add some debug message in MLO, we found out it should be PMIC issue.
The error message as below:
U-Boot SPL 2014.07 (Sep 05 2017 - 17:07:20)
DRA752-GP ES2.0
before do_io_settings
before prcm_init
|-before enable_basic_clocks
Enable clock domain - 4a009700
Enable clock domain - 4a009300
Enable clock domain - 4a008b00
Enable clock domain - 4a008d00
Enable clock domain - 4a0093c0
Enable clock domain - 4a008700
Enable clock module - 4a008728
Enable clock module - 4a008b30
Enable clock module - 4a008b38
Enable clock module - 4a008d20
Enable clock module - 4ae07838
Enable clock module - 4a009760
Enable clock module - 4a009768
Enable clock module - 4a009770
Enable clock module - 4a009778
Enable clock module - 4a009780
Enable clock module - 4a009810
Enable clock module - 4a009818
Enable clock module - 4a008778
Enable clock module - 4a008780
Enable clock module - 4ae07840
Enable clock module - 4a009328
Enable clock module - 4a009330
Enable clock module - 4a009738
Enable clock module - 4ae07830
Enable clock module - 4a009850
Enable clock module - 4a0097a0
Enable clock module - 4a0093d0
Enable clock module - 4a009838
Enable clock domain - 4a009700
Enable clock domain - 4a009300
Enable clock domain - 4a008b00
Enable clock domain - 4a008d00
Enable clock domain - 4a0093c0
Enable clock domain - 4a008700
|-before timer_init
|-before scale_vcores
|-before vcores->core
optimize_vcore_voltage:efuse 0x4a0025f4 bits=16 Vnom=1030, using efuse value 1045
|-before core
do_scale_vcore: volt - 1045 offset_code - 0x3d
The boot flow to "do_scale_vcore: volt - 1045 offset_code - 0x3d", it will reboot.
Could you give me some directions to debug further? maybe we need to modify efuse voltage in MLO?
Thanks for your support in advance.
Best Regards,
Bowei