Hello,
I am a complete newbie with the TI DM processors. As part of the university project, I want to evaluate using DM3x processors for building a FPV system.
The basic requirement for now is to have a 720p video streaming at 30fps or less.
Could anyone let me know the following :
1. which evaluation/development board should I be looking at for such a system. As per the TI announcements, it is advised to not begin any new development on TI DM3555 processor as the support is limited.
2. what kind of camera interfaces would be suitable for the DM3x boards.
3. for initial development, I would like to stream the video over WiFi. Would it be a good option to use the same DM3x for streaming as well.
4. are there any reference examples available with the DM3 boards, that can be used for an FPV system.
Thanks in advance.