This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3354: NAND bad block management

Part Number: AM3354

Tool/software: Linux

Hi:

        i was recently trying to study how AM3354 linux BSP works on the nand flash bad block management.

        we are using AM3354 and we are using kernel 4.4.32 extracted from ti sdk 03.02.00.05.

        we also use the kernel 3.2.0 extract from ti sdk 06.00.00.00 for some older products.

       Now i found a strange thing that i can not understand regarding nand flash bad block management.Either kernel 3.2.0 or 4.4.32 have the same behavior on this.

       when the kernel is starting.I suppose it should look for the nand flash bad block table .Right? find out where it's located.And be able to update the table when the block_markbad() function is called in the future when a new bad block is discovered.

       But strange thing is:

       in drivers/mtd/nand/omap2.c omap_nand_probe()

       after nand_scan_tail() is called. the nand driver did not call nand_default_bbt() to scan the bbt.Or disable the NAND_SKIP_BBTSCAN flag.

       instead it defines in the omap_nand_probe():

      info->nand.options |= NAND_SKIP_BBTSCAN;

      to skip the scan.thus nand_scan_tail() will not call default scan_bbt callback and also the driver itself did not call scan_bbt independently.

       i have products running on freescale cpu.and their driver will call nand_default_bbt() in the probe function of the driver.And when kernel is starting.I can see something in the kernel starting log like this:
Bad block table found at page 131008, version 0x01
Bad block table found at page 130944, version 0x01

   

     So my questions .without calling the nand_default_bbt() . (both 3.2.0 kernel and 4.4.32 kernel)  How is the bad block managed by kernel in the AM3354 BSP?

      

thank you

yan dong

  • /*
     * Copyright © 2004 Texas Instruments, Jian Zhang <jzhang@ti.com>
     * Copyright © 2004 Micron Technology Inc.
     * Copyright © 2004 David Brownell
     *
     * This program is free software; you can redistribute it and/or modify
     * it under the terms of the GNU General Public License version 2 as
     * published by the Free Software Foundation.
     */
    
    #include <linux/platform_device.h>
    #include <linux/dma-mapping.h>
    #include <linux/delay.h>
    #include <linux/module.h>
    #include <linux/interrupt.h>
    #include <linux/jiffies.h>
    #include <linux/sched.h>
    #include <linux/mtd/mtd.h>
    #include <linux/mtd/nand.h>
    #include <linux/mtd/partitions.h>
    #include <linux/io.h>
    #include <linux/slab.h>
    
    #include <plat/dma.h>
    #include <plat/gpmc.h>
    #include <plat/nand.h>
    #include <plat/elm.h>
    
    #define	DRIVER_NAME	"omap2-nand"
    #define	OMAP_NAND_TIMEOUT_MS	5000
    
    #define NAND_Ecc_P1e		(1 << 0)
    #define NAND_Ecc_P2e		(1 << 1)
    #define NAND_Ecc_P4e		(1 << 2)
    #define NAND_Ecc_P8e		(1 << 3)
    #define NAND_Ecc_P16e		(1 << 4)
    #define NAND_Ecc_P32e		(1 << 5)
    #define NAND_Ecc_P64e		(1 << 6)
    #define NAND_Ecc_P128e		(1 << 7)
    #define NAND_Ecc_P256e		(1 << 8)
    #define NAND_Ecc_P512e		(1 << 9)
    #define NAND_Ecc_P1024e		(1 << 10)
    #define NAND_Ecc_P2048e		(1 << 11)
    
    #define NAND_Ecc_P1o		(1 << 16)
    #define NAND_Ecc_P2o		(1 << 17)
    #define NAND_Ecc_P4o		(1 << 18)
    #define NAND_Ecc_P8o		(1 << 19)
    #define NAND_Ecc_P16o		(1 << 20)
    #define NAND_Ecc_P32o		(1 << 21)
    #define NAND_Ecc_P64o		(1 << 22)
    #define NAND_Ecc_P128o		(1 << 23)
    #define NAND_Ecc_P256o		(1 << 24)
    #define NAND_Ecc_P512o		(1 << 25)
    #define NAND_Ecc_P1024o		(1 << 26)
    #define NAND_Ecc_P2048o		(1 << 27)
    
    #define TF(value)	(value ? 1 : 0)
    
    #define P2048e(a)	(TF(a & NAND_Ecc_P2048e)	<< 0)
    #define P2048o(a)	(TF(a & NAND_Ecc_P2048o)	<< 1)
    #define P1e(a)		(TF(a & NAND_Ecc_P1e)		<< 2)
    #define P1o(a)		(TF(a & NAND_Ecc_P1o)		<< 3)
    #define P2e(a)		(TF(a & NAND_Ecc_P2e)		<< 4)
    #define P2o(a)		(TF(a & NAND_Ecc_P2o)		<< 5)
    #define P4e(a)		(TF(a & NAND_Ecc_P4e)		<< 6)
    #define P4o(a)		(TF(a & NAND_Ecc_P4o)		<< 7)
    
    #define P8e(a)		(TF(a & NAND_Ecc_P8e)		<< 0)
    #define P8o(a)		(TF(a & NAND_Ecc_P8o)		<< 1)
    #define P16e(a)		(TF(a & NAND_Ecc_P16e)		<< 2)
    #define P16o(a)		(TF(a & NAND_Ecc_P16o)		<< 3)
    #define P32e(a)		(TF(a & NAND_Ecc_P32e)		<< 4)
    #define P32o(a)		(TF(a & NAND_Ecc_P32o)		<< 5)
    #define P64e(a)		(TF(a & NAND_Ecc_P64e)		<< 6)
    #define P64o(a)		(TF(a & NAND_Ecc_P64o)		<< 7)
    
    #define P128e(a)	(TF(a & NAND_Ecc_P128e)		<< 0)
    #define P128o(a)	(TF(a & NAND_Ecc_P128o)		<< 1)
    #define P256e(a)	(TF(a & NAND_Ecc_P256e)		<< 2)
    #define P256o(a)	(TF(a & NAND_Ecc_P256o)		<< 3)
    #define P512e(a)	(TF(a & NAND_Ecc_P512e)		<< 4)
    #define P512o(a)	(TF(a & NAND_Ecc_P512o)		<< 5)
    #define P1024e(a)	(TF(a & NAND_Ecc_P1024e)	<< 6)
    #define P1024o(a)	(TF(a & NAND_Ecc_P1024o)	<< 7)
    
    #define P8e_s(a)	(TF(a & NAND_Ecc_P8e)		<< 0)
    #define P8o_s(a)	(TF(a & NAND_Ecc_P8o)		<< 1)
    #define P16e_s(a)	(TF(a & NAND_Ecc_P16e)		<< 2)
    #define P16o_s(a)	(TF(a & NAND_Ecc_P16o)		<< 3)
    #define P1e_s(a)	(TF(a & NAND_Ecc_P1e)		<< 4)
    #define P1o_s(a)	(TF(a & NAND_Ecc_P1o)		<< 5)
    #define P2e_s(a)	(TF(a & NAND_Ecc_P2e)		<< 6)
    #define P2o_s(a)	(TF(a & NAND_Ecc_P2o)		<< 7)
    
    #define P4e_s(a)	(TF(a & NAND_Ecc_P4e)		<< 0)
    #define P4o_s(a)	(TF(a & NAND_Ecc_P4o)		<< 1)
    
    #define MAX_HWECC_BYTES_OOB_64     24
    #define JFFS2_CLEAN_MARKER_OFFSET  0x2
    
    #define BCH_ECC_POS			0x2
    #define BCH_JFFS2_CLEAN_MARKER_OFFSET	0x3a
    #define OMAP_BCH8_ECC_SECT_BYTES	14
    
    /* oob info generated runtime depending on ecc algorithm and layout selected */
    static struct nand_ecclayout omap_oobinfo;
    /* Define some generic bad / good block scan pattern which are used
     * while scanning a device for factory marked good / bad blocks
     */
    static uint8_t scan_ff_pattern[] = { 0xff };
    static struct nand_bbt_descr bb_descrip_flashbased = {
    	.options = NAND_BBT_SCANEMPTY | NAND_BBT_SCANALLPAGES,
    	.offs = 0,
    	.len = 1,
    	.pattern = scan_ff_pattern,
    };
    
    
    struct omap_nand_info {
    	struct nand_hw_control		controller;
    	struct omap_nand_platform_data	*pdata;
    	struct mtd_info			mtd;
    	struct nand_chip		nand;
    	struct platform_device		*pdev;
    
    	int				gpmc_cs;
    	unsigned long			phys_base;
    	struct completion		comp;
    	int				dma_ch;
    	int				gpmc_irq;
    	enum {
    		OMAP_NAND_IO_READ = 0,	/* read */
    		OMAP_NAND_IO_WRITE,	/* write */
    	} iomode;
    	u_char				*buf;
    	int				buf_len;
    	int				ecc_opt;
    	int (*ctrlr_suspend) (void);
    	int (*ctrlr_resume) (void);
    };
    
    /**
     * omap_hwcontrol - hardware specific access to control-lines
     * @mtd: MTD device structure
     * @cmd: command to device
     * @ctrl:
     * NAND_NCE: bit 0 -> don't care
     * NAND_CLE: bit 1 -> Command Latch
     * NAND_ALE: bit 2 -> Address Latch
     *
     * NOTE: boards may use different bits for these!!
     */
    static void omap_hwcontrol(struct mtd_info *mtd, int cmd, unsigned int ctrl)
    {
    	struct omap_nand_info *info = container_of(mtd,
    					struct omap_nand_info, mtd);
    
    	if (cmd != NAND_CMD_NONE) {
    		if (ctrl & NAND_CLE)
    			gpmc_nand_write(info->gpmc_cs, GPMC_NAND_COMMAND, cmd);
    
    		else if (ctrl & NAND_ALE)
    			gpmc_nand_write(info->gpmc_cs, GPMC_NAND_ADDRESS, cmd);
    
    		else /* NAND_NCE */
    			gpmc_nand_write(info->gpmc_cs, GPMC_NAND_DATA, cmd);
    	}
    }
    
    /**
     * omap_read_buf8 - read data from NAND controller into buffer
     * @mtd: MTD device structure
     * @buf: buffer to store date
     * @len: number of bytes to read
     */
    static void omap_read_buf8(struct mtd_info *mtd, u_char *buf, int len)
    {
    	struct nand_chip *nand = mtd->priv;
    
    	ioread8_rep(nand->IO_ADDR_R, buf, len);
    }
    
    /**
     * omap_write_buf8 - write buffer to NAND controller
     * @mtd: MTD device structure
     * @buf: data buffer
     * @len: number of bytes to write
     */
    static void omap_write_buf8(struct mtd_info *mtd, const u_char *buf, int len)
    {
    	struct omap_nand_info *info = container_of(mtd,
    						struct omap_nand_info, mtd);
    	u_char *p = (u_char *)buf;
    	u32	status = 0;
    
    	while (len--) {
    		iowrite8(*p++, info->nand.IO_ADDR_W);
    		/* wait until buffer is available for write */
    		do {
    			status = gpmc_read_status(GPMC_STATUS_BUFFER);
    		} while (!status);
    	}
    }
    
    /**
     * omap_read_buf16 - read data from NAND controller into buffer
     * @mtd: MTD device structure
     * @buf: buffer to store date
     * @len: number of bytes to read
     */
    static void omap_read_buf16(struct mtd_info *mtd, u_char *buf, int len)
    {
    	struct nand_chip *nand = mtd->priv;
    
    	ioread16_rep(nand->IO_ADDR_R, buf, len / 2);
    }
    
    /**
     * omap_write_buf16 - write buffer to NAND controller
     * @mtd: MTD device structure
     * @buf: data buffer
     * @len: number of bytes to write
     */
    static void omap_write_buf16(struct mtd_info *mtd, const u_char * buf, int len)
    {
    	struct omap_nand_info *info = container_of(mtd,
    						struct omap_nand_info, mtd);
    	u16 *p = (u16 *) buf;
    	u32	status = 0;
    	/* FIXME try bursts of writesw() or DMA ... */
    	len >>= 1;
    
    	while (len--) {
    		iowrite16(*p++, info->nand.IO_ADDR_W);
    		/* wait until buffer is available for write */
    		do {
    			status = gpmc_read_status(GPMC_STATUS_BUFFER);
    		} while (!status);
    	}
    }
    
    /**
     * omap_read_buf_pref - read data from NAND controller into buffer
     * @mtd: MTD device structure
     * @buf: buffer to store date
     * @len: number of bytes to read
     */
    static void omap_read_buf_pref(struct mtd_info *mtd, u_char *buf, int len)
    {
    	struct omap_nand_info *info = container_of(mtd,
    						struct omap_nand_info, mtd);
    	uint32_t r_count = 0;
    	int ret = 0;
    	u32 *p = (u32 *)buf;
    
    	/* take care of subpage reads */
    	if (len % 4) {
    		if (info->nand.options & NAND_BUSWIDTH_16)
    			omap_read_buf16(mtd, buf, len % 4);
    		else
    			omap_read_buf8(mtd, buf, len % 4);
    		p = (u32 *) (buf + len % 4);
    		len -= len % 4;
    	}
    
    	/* configure and start prefetch transfer */
    	ret = gpmc_prefetch_enable(info->gpmc_cs,
    			PREFETCH_FIFOTHRESHOLD_MAX, 0x0, len, 0x0);
    	if (ret) {
    		/* PFPW engine is busy, use cpu copy method */
    		if (info->nand.options & NAND_BUSWIDTH_16)
    			omap_read_buf16(mtd, (u_char *)p, len);
    		else
    			omap_read_buf8(mtd, (u_char *)p, len);
    	} else {
    		do {
    			r_count = gpmc_read_status(GPMC_PREFETCH_FIFO_CNT);
    			r_count = r_count >> 2;
    			ioread32_rep(info->nand.IO_ADDR_R, p, r_count);
    			p += r_count;
    			len -= r_count << 2;
    		} while (len);
    		/* disable and stop the PFPW engine */
    		gpmc_prefetch_reset(info->gpmc_cs);
    	}
    }
    
    /**
     * omap_write_buf_pref - write buffer to NAND controller
     * @mtd: MTD device structure
     * @buf: data buffer
     * @len: number of bytes to write
     */
    static void omap_write_buf_pref(struct mtd_info *mtd,
    					const u_char *buf, int len)
    {
    	struct omap_nand_info *info = container_of(mtd,
    						struct omap_nand_info, mtd);
    	uint32_t w_count = 0;
    	int i = 0, ret = 0;
    	u16 *p = (u16 *)buf;
    	unsigned long tim, limit;
    
    	/* take care of subpage writes */
    	if (len % 2 != 0) {
    		writeb(*buf, info->nand.IO_ADDR_W);
    		p = (u16 *)(buf + 1);
    		len--;
    	}
    
    	/*  configure and start prefetch transfer */
    	ret = gpmc_prefetch_enable(info->gpmc_cs,
    			PREFETCH_FIFOTHRESHOLD_MAX, 0x0, len, 0x1);
    	if (ret) {
    		/* PFPW engine is busy, use cpu copy method */
    		if (info->nand.options & NAND_BUSWIDTH_16)
    			omap_write_buf16(mtd, (u_char *)p, len);
    		else
    			omap_write_buf8(mtd, (u_char *)p, len);
    	} else {
    		while (len) {
    			w_count = gpmc_read_status(GPMC_PREFETCH_FIFO_CNT);
    			w_count = w_count >> 1;
    			for (i = 0; (i < w_count) && len; i++, len -= 2)
    				iowrite16(*p++, info->nand.IO_ADDR_W);
    		}
    		/* wait for data to flushed-out before reset the prefetch */
    		tim = 0;
    		limit = (loops_per_jiffy *
    					msecs_to_jiffies(OMAP_NAND_TIMEOUT_MS));
    		while (gpmc_read_status(GPMC_PREFETCH_COUNT) && (tim++ < limit))
    			cpu_relax();
    
    		/* disable and stop the PFPW engine */
    		gpmc_prefetch_reset(info->gpmc_cs);
    	}
    }
    
    /*
     * omap_nand_dma_cb: callback on the completion of dma transfer
     * @lch: logical channel
     * @ch_satuts: channel status
     * @data: pointer to completion data structure
     */
    static void omap_nand_dma_cb(int lch, u16 ch_status, void *data)
    {
    	complete((struct completion *) data);
    }
    
    /*
     * omap_nand_dma_transfer: configer and start dma transfer
     * @mtd: MTD device structure
     * @addr: virtual address in RAM of source/destination
     * @len: number of data bytes to be transferred
     * @is_write: flag for read/write operation
     */
    static inline int omap_nand_dma_transfer(struct mtd_info *mtd, void *addr,
    					unsigned int len, int is_write)
    {
    	struct omap_nand_info *info = container_of(mtd,
    					struct omap_nand_info, mtd);
    	enum dma_data_direction dir = is_write ? DMA_TO_DEVICE :
    							DMA_FROM_DEVICE;
    	dma_addr_t dma_addr;
    	int ret;
    	unsigned long tim, limit;
    
    	/* The fifo depth is 64 bytes max.
    	 * But configure the FIFO-threahold to 32 to get a sync at each frame
    	 * and frame length is 32 bytes.
    	 */
    	int buf_len = len >> 6;
    
    	if (addr >= high_memory) {
    		struct page *p1;
    
    		if (((size_t)addr & PAGE_MASK) !=
    			((size_t)(addr + len - 1) & PAGE_MASK))
    			goto out_copy;
    		p1 = vmalloc_to_page(addr);
    		if (!p1)
    			goto out_copy;
    		addr = page_address(p1) + ((size_t)addr & ~PAGE_MASK);
    	}
    
    	dma_addr = dma_map_single(&info->pdev->dev, addr, len, dir);
    	if (dma_mapping_error(&info->pdev->dev, dma_addr)) {
    		dev_err(&info->pdev->dev,
    			"Couldn't DMA map a %d byte buffer\n", len);
    		goto out_copy;
    	}
    
    	if (is_write) {
    	    omap_set_dma_dest_params(info->dma_ch, 0, OMAP_DMA_AMODE_CONSTANT,
    						info->phys_base, 0, 0);
    	    omap_set_dma_src_params(info->dma_ch, 0, OMAP_DMA_AMODE_POST_INC,
    							dma_addr, 0, 0);
    	    omap_set_dma_transfer_params(info->dma_ch, OMAP_DMA_DATA_TYPE_S32,
    					0x10, buf_len, OMAP_DMA_SYNC_FRAME,
    					OMAP24XX_DMA_GPMC, OMAP_DMA_DST_SYNC);
    	} else {
    	    omap_set_dma_src_params(info->dma_ch, 0, OMAP_DMA_AMODE_CONSTANT,
    						info->phys_base, 0, 0);
    	    omap_set_dma_dest_params(info->dma_ch, 0, OMAP_DMA_AMODE_POST_INC,
    							dma_addr, 0, 0);
    	    omap_set_dma_transfer_params(info->dma_ch, OMAP_DMA_DATA_TYPE_S32,
    					0x10, buf_len, OMAP_DMA_SYNC_FRAME,
    					OMAP24XX_DMA_GPMC, OMAP_DMA_SRC_SYNC);
    	}
    	/*  configure and start prefetch transfer */
    	ret = gpmc_prefetch_enable(info->gpmc_cs,
    			PREFETCH_FIFOTHRESHOLD_MAX, 0x1, len, is_write);
    	if (ret)
    		/* PFPW engine is busy, use cpu copy method */
    		goto out_copy;
    
    	init_completion(&info->comp);
    
    	omap_start_dma(info->dma_ch);
    
    	/* setup and start DMA using dma_addr */
    	wait_for_completion(&info->comp);
    	tim = 0;
    	limit = (loops_per_jiffy * msecs_to_jiffies(OMAP_NAND_TIMEOUT_MS));
    	while (gpmc_read_status(GPMC_PREFETCH_COUNT) && (tim++ < limit))
    		cpu_relax();
    
    	/* disable and stop the PFPW engine */
    	gpmc_prefetch_reset(info->gpmc_cs);
    
    	dma_unmap_single(&info->pdev->dev, dma_addr, len, dir);
    	return 0;
    
    out_copy:
    	if (info->nand.options & NAND_BUSWIDTH_16)
    		is_write == 0 ? omap_read_buf16(mtd, (u_char *) addr, len)
    			: omap_write_buf16(mtd, (u_char *) addr, len);
    	else
    		is_write == 0 ? omap_read_buf8(mtd, (u_char *) addr, len)
    			: omap_write_buf8(mtd, (u_char *) addr, len);
    	return 0;
    }
    
    /**
     * omap_read_buf_dma_pref - read data from NAND controller into buffer
     * @mtd: MTD device structure
     * @buf: buffer to store date
     * @len: number of bytes to read
     */
    static void omap_read_buf_dma_pref(struct mtd_info *mtd, u_char *buf, int len)
    {
    	if (len <= mtd->oobsize)
    		omap_read_buf_pref(mtd, buf, len);
    	else
    		/* start transfer in DMA mode */
    		omap_nand_dma_transfer(mtd, buf, len, 0x0);
    }
    
    /**
     * omap_write_buf_dma_pref - write buffer to NAND controller
     * @mtd: MTD device structure
     * @buf: data buffer
     * @len: number of bytes to write
     */
    static void omap_write_buf_dma_pref(struct mtd_info *mtd,
    					const u_char *buf, int len)
    {
    	if (len <= mtd->oobsize)
    		omap_write_buf_pref(mtd, buf, len);
    	else
    		/* start transfer in DMA mode */
    		omap_nand_dma_transfer(mtd, (u_char *) buf, len, 0x1);
    }
    
    /*
     * omap_nand_irq - GMPC irq handler
     * @this_irq: gpmc irq number
     * @dev: omap_nand_info structure pointer is passed here
     */
    static irqreturn_t omap_nand_irq(int this_irq, void *dev)
    {
    	struct omap_nand_info *info = (struct omap_nand_info *) dev;
    	u32 bytes;
    	u32 irq_stat;
    
    	irq_stat = gpmc_read_status(GPMC_GET_IRQ_STATUS);
    	bytes = gpmc_read_status(GPMC_PREFETCH_FIFO_CNT);
    	bytes = bytes  & 0xFFFC; /* io in multiple of 4 bytes */
    	if (info->iomode == OMAP_NAND_IO_WRITE) { /* checks for write io */
    		if (irq_stat & 0x2)
    			goto done;
    
    		if (info->buf_len && (info->buf_len < bytes))
    			bytes = info->buf_len;
    		else if (!info->buf_len)
    			bytes = 0;
    		iowrite32_rep(info->nand.IO_ADDR_W,
    						(u32 *)info->buf, bytes >> 2);
    		info->buf = info->buf + bytes;
    		info->buf_len -= bytes;
    
    	} else {
    		ioread32_rep(info->nand.IO_ADDR_R,
    						(u32 *)info->buf, bytes >> 2);
    		info->buf = info->buf + bytes;
    
    		if (irq_stat & 0x2)
    			goto done;
    	}
    	gpmc_cs_configure(info->gpmc_cs, GPMC_SET_IRQ_STATUS, irq_stat);
    
    	return IRQ_HANDLED;
    
    done:
    	complete(&info->comp);
    	/* disable irq */
    	gpmc_cs_configure(info->gpmc_cs, GPMC_ENABLE_IRQ, 0);
    
    	/* clear status */
    	gpmc_cs_configure(info->gpmc_cs, GPMC_SET_IRQ_STATUS, irq_stat);
    
    	return IRQ_HANDLED;
    }
    
    /*
     * omap_read_buf_irq_pref - read data from NAND controller into buffer
     * @mtd: MTD device structure
     * @buf: buffer to store date
     * @len: number of bytes to read
     */
    static void omap_read_buf_irq_pref(struct mtd_info *mtd, u_char *buf, int len)
    {
    	struct omap_nand_info *info = container_of(mtd,
    						struct omap_nand_info, mtd);
    	int ret = 0;
    
    	if (len <= mtd->oobsize) {
    		omap_read_buf_pref(mtd, buf, len);
    		return;
    	}
    
    	info->iomode = OMAP_NAND_IO_READ;
    	info->buf = buf;
    	init_completion(&info->comp);
    
    	/*  configure and start prefetch transfer */
    	ret = gpmc_prefetch_enable(info->gpmc_cs,
    			PREFETCH_FIFOTHRESHOLD_MAX/2, 0x0, len, 0x0);
    	if (ret)
    		/* PFPW engine is busy, use cpu copy method */
    		goto out_copy;
    
    	info->buf_len = len;
    	/* enable irq */
    	gpmc_cs_configure(info->gpmc_cs, GPMC_ENABLE_IRQ,
    		(GPMC_IRQ_FIFOEVENTENABLE | GPMC_IRQ_COUNT_EVENT));
    
    	/* waiting for read to complete */
    	wait_for_completion(&info->comp);
    
    	/* disable and stop the PFPW engine */
    	gpmc_prefetch_reset(info->gpmc_cs);
    	return;
    
    out_copy:
    	if (info->nand.options & NAND_BUSWIDTH_16)
    		omap_read_buf16(mtd, buf, len);
    	else
    		omap_read_buf8(mtd, buf, len);
    }
    
    /*
     * omap_write_buf_irq_pref - write buffer to NAND controller
     * @mtd: MTD device structure
     * @buf: data buffer
     * @len: number of bytes to write
     */
    static void omap_write_buf_irq_pref(struct mtd_info *mtd,
    					const u_char *buf, int len)
    {
    	struct omap_nand_info *info = container_of(mtd,
    						struct omap_nand_info, mtd);
    	int ret = 0;
    	unsigned long tim, limit;
    
    	if (len <= mtd->oobsize) {
    		omap_write_buf_pref(mtd, buf, len);
    		return;
    	}
    
    	info->iomode = OMAP_NAND_IO_WRITE;
    	info->buf = (u_char *) buf;
    	init_completion(&info->comp);
    
    	/* configure and start prefetch transfer : size=24 */
    	ret = gpmc_prefetch_enable(info->gpmc_cs,
    			(PREFETCH_FIFOTHRESHOLD_MAX * 3) / 8, 0x0, len, 0x1);
    	if (ret)
    		/* PFPW engine is busy, use cpu copy method */
    		goto out_copy;
    
    	info->buf_len = len;
    	/* enable irq */
    	gpmc_cs_configure(info->gpmc_cs, GPMC_ENABLE_IRQ,
    			(GPMC_IRQ_FIFOEVENTENABLE | GPMC_IRQ_COUNT_EVENT));
    
    	/* waiting for write to complete */
    	wait_for_completion(&info->comp);
    	/* wait for data to flushed-out before reset the prefetch */
    	tim = 0;
    	limit = (loops_per_jiffy *  msecs_to_jiffies(OMAP_NAND_TIMEOUT_MS));
    	while (gpmc_read_status(GPMC_PREFETCH_COUNT) && (tim++ < limit))
    		cpu_relax();
    
    	/* disable and stop the PFPW engine */
    	gpmc_prefetch_reset(info->gpmc_cs);
    	return;
    
    out_copy:
    	if (info->nand.options & NAND_BUSWIDTH_16)
    		omap_write_buf16(mtd, buf, len);
    	else
    		omap_write_buf8(mtd, buf, len);
    }
    
    /**
     * omap_verify_buf - Verify chip data against buffer
     * @mtd: MTD device structure
     * @buf: buffer containing the data to compare
     * @len: number of bytes to compare
     */
    static int omap_verify_buf(struct mtd_info *mtd, const u_char * buf, int len)
    {
    	struct omap_nand_info *info = container_of(mtd, struct omap_nand_info,
    							mtd);
    	u16 *p = (u16 *) buf;
    
    	len >>= 1;
    	while (len--) {
    		if (*p++ != cpu_to_le16(readw(info->nand.IO_ADDR_R)))
    			return -EFAULT;
    	}
    
    	return 0;
    }
    
    /**
     * gen_true_ecc - This function will generate true ECC value
     * @ecc_buf: buffer to store ecc code
     *
     * This generated true ECC value can be used when correcting
     * data read from NAND flash memory core
     */
    static void gen_true_ecc(u8 *ecc_buf)
    {
    	u32 tmp = ecc_buf[0] | (ecc_buf[1] << 16) |
    		((ecc_buf[2] & 0xF0) << 20) | ((ecc_buf[2] & 0x0F) << 8);
    
    	ecc_buf[0] = ~(P64o(tmp) | P64e(tmp) | P32o(tmp) | P32e(tmp) |
    			P16o(tmp) | P16e(tmp) | P8o(tmp) | P8e(tmp));
    	ecc_buf[1] = ~(P1024o(tmp) | P1024e(tmp) | P512o(tmp) | P512e(tmp) |
    			P256o(tmp) | P256e(tmp) | P128o(tmp) | P128e(tmp));
    	ecc_buf[2] = ~(P4o(tmp) | P4e(tmp) | P2o(tmp) | P2e(tmp) | P1o(tmp) |
    			P1e(tmp) | P2048o(tmp) | P2048e(tmp));
    }
    
    /**
     * omap_compare_ecc - Detect (2 bits) and correct (1 bit) error in data
     * @ecc_data1:  ecc code from nand spare area
     * @ecc_data2:  ecc code from hardware register obtained from hardware ecc
     * @page_data:  page data
     *
     * This function compares two ECC's and indicates if there is an error.
     * If the error can be corrected it will be corrected to the buffer.
     * If there is no error, %0 is returned. If there is an error but it
     * was corrected, %1 is returned. Otherwise, %-1 is returned.
     */
    static int omap_compare_ecc(u8 *ecc_data1,	/* read from NAND memory */
    			    u8 *ecc_data2,	/* read from register */
    			    u8 *page_data)
    {
    	uint	i;
    	u8	tmp0_bit[8], tmp1_bit[8], tmp2_bit[8];
    	u8	comp0_bit[8], comp1_bit[8], comp2_bit[8];
    	u8	ecc_bit[24];
    	u8	ecc_sum = 0;
    	u8	find_bit = 0;
    	uint	find_byte = 0;
    	int	isEccFF;
    
    	isEccFF = ((*(u32 *)ecc_data1 & 0xFFFFFF) == 0xFFFFFF);
    
    	gen_true_ecc(ecc_data1);
    	gen_true_ecc(ecc_data2);
    
    	for (i = 0; i <= 2; i++) {
    		*(ecc_data1 + i) = ~(*(ecc_data1 + i));
    		*(ecc_data2 + i) = ~(*(ecc_data2 + i));
    	}
    
    	for (i = 0; i < 8; i++) {
    		tmp0_bit[i]     = *ecc_data1 % 2;
    		*ecc_data1	= *ecc_data1 / 2;
    	}
    
    	for (i = 0; i < 8; i++) {
    		tmp1_bit[i]	 = *(ecc_data1 + 1) % 2;
    		*(ecc_data1 + 1) = *(ecc_data1 + 1) / 2;
    	}
    
    	for (i = 0; i < 8; i++) {
    		tmp2_bit[i]	 = *(ecc_data1 + 2) % 2;
    		*(ecc_data1 + 2) = *(ecc_data1 + 2) / 2;
    	}
    
    	for (i = 0; i < 8; i++) {
    		comp0_bit[i]     = *ecc_data2 % 2;
    		*ecc_data2       = *ecc_data2 / 2;
    	}
    
    	for (i = 0; i < 8; i++) {
    		comp1_bit[i]     = *(ecc_data2 + 1) % 2;
    		*(ecc_data2 + 1) = *(ecc_data2 + 1) / 2;
    	}
    
    	for (i = 0; i < 8; i++) {
    		comp2_bit[i]     = *(ecc_data2 + 2) % 2;
    		*(ecc_data2 + 2) = *(ecc_data2 + 2) / 2;
    	}
    
    	for (i = 0; i < 6; i++)
    		ecc_bit[i] = tmp2_bit[i + 2] ^ comp2_bit[i + 2];
    
    	for (i = 0; i < 8; i++)
    		ecc_bit[i + 6] = tmp0_bit[i] ^ comp0_bit[i];
    
    	for (i = 0; i < 8; i++)
    		ecc_bit[i + 14] = tmp1_bit[i] ^ comp1_bit[i];
    
    	ecc_bit[22] = tmp2_bit[0] ^ comp2_bit[0];
    	ecc_bit[23] = tmp2_bit[1] ^ comp2_bit[1];
    
    	for (i = 0; i < 24; i++)
    		ecc_sum += ecc_bit[i];
    
    	switch (ecc_sum) {
    	case 0:
    		/* Not reached because this function is not called if
    		 *  ECC values are equal
    		 */
    		return 0;
    
    	case 1:
    		/* Uncorrectable error */
    		pr_debug("ECC UNCORRECTED_ERROR 1\n");
    		return -1;
    
    	case 11:
    		/* UN-Correctable error */
    		pr_debug("ECC UNCORRECTED_ERROR B\n");
    		return -1;
    
    	case 12:
    		/* Correctable error */
    		find_byte = (ecc_bit[23] << 8) +
    			    (ecc_bit[21] << 7) +
    			    (ecc_bit[19] << 6) +
    			    (ecc_bit[17] << 5) +
    			    (ecc_bit[15] << 4) +
    			    (ecc_bit[13] << 3) +
    			    (ecc_bit[11] << 2) +
    			    (ecc_bit[9]  << 1) +
    			    ecc_bit[7];
    
    		find_bit = (ecc_bit[5] << 2) + (ecc_bit[3] << 1) + ecc_bit[1];
    
    		pr_debug("Correcting single bit ECC error at offset: "
    				"%d, bit: %d\n", find_byte, find_bit);
    
    		page_data[find_byte] ^= (1 << find_bit);
    
    		return 1;
    	default:
    		if (isEccFF) {
    			if (ecc_data2[0] == 0 &&
    			    ecc_data2[1] == 0 &&
    			    ecc_data2[2] == 0)
    				return 0;
    		}
    		pr_debug("UNCORRECTED_ERROR default\n");
    		return -1;
    	}
    }
    
    /**
     * omap_read_page_bch - BCH ecc based page read function
     * @mtd:	mtd info structure
     * @chip:	nand chip info structure
     * @buf:	buffer to store read data
     * @page:	page number to read
     *
     * For BCH ECC scheme, GPMC used for syndrome calculation and ELM module
     * used for error correction.
     */
    static int omap_read_page_bch(struct mtd_info *mtd, struct nand_chip *chip,
    				uint8_t *buf, int page)
    {
    	int i, eccsize = chip->ecc.size;
    	int eccbytes = chip->ecc.bytes;
    	int eccsteps = chip->ecc.steps;
    	uint8_t *p = buf;
    	uint8_t *ecc_calc = chip->buffers->ecccalc;
    	uint8_t *ecc_code = chip->buffers->ecccode;
    	uint32_t *eccpos = chip->ecc.layout->eccpos;
    	uint8_t *oob = &chip->oob_poi[eccpos[0]];
    	uint32_t data_pos;
    	uint32_t oob_pos;
    
    	struct omap_nand_info *info = container_of(mtd, struct omap_nand_info,
    							mtd);
    	data_pos = 0;
    	/* oob area start */
    	oob_pos = (eccsize * eccsteps) + chip->ecc.layout->eccpos[0];
    
    	for (i = 0; eccsteps; eccsteps--, i += eccbytes, p += eccsize,
    				oob += eccbytes) {
    		chip->ecc.hwctl(mtd, NAND_ECC_READ);
    		/* read data */
    		chip->cmdfunc(mtd, NAND_CMD_RNDOUT, data_pos, page);
    		chip->read_buf(mtd, p, eccsize);
    
    		/* read respective ecc from oob area */
    		chip->cmdfunc(mtd, NAND_CMD_RNDOUT, oob_pos, page);
    
    		if (info->ecc_opt == OMAP_ECC_BCH8_CODE_HW)
    			chip->read_buf(mtd, oob, 13);
    		else
    			chip->read_buf(mtd, oob, eccbytes);
    		/* read syndrome */
    		chip->ecc.calculate(mtd, p, &ecc_calc[i]);
    
    		data_pos += eccsize;
    		oob_pos += eccbytes;
    	}
    
    	for (i = 0; i < chip->ecc.total; i++)
    		ecc_code[i] = chip->oob_poi[eccpos[i]];
    
    	eccsteps = chip->ecc.steps;
    	p = buf;
    
    	for (i = 0 ; eccsteps; eccsteps--, i += eccbytes, p += eccsize) {
    		int stat;
    
    		stat = chip->ecc.correct(mtd, p, &ecc_code[i], &ecc_calc[i]);
    
    		if (stat < 0)
    			mtd->ecc_stats.failed++;
    		else
    			mtd->ecc_stats.corrected += stat;
    	}
    	return 0;
    }
    
    /**
     * omap_correct_data - Compares the ECC read with HW generated ECC
     * @mtd: MTD device structure
     * @dat: page data
     * @read_ecc: ecc read from nand flash
     * @calc_ecc: ecc read from HW ECC registers
     *
     * Compares the ecc read from nand spare area with ECC registers values
     * and if ECC's mismatched, it will call 'omap_compare_ecc' for error
     * detection and correction. If there are no errors, %0 is returned. If
     * there were errors and all of the errors were corrected, the number of
     * corrected errors is returned. If uncorrectable errors exist, %-1 is
     * returned.
     */
    static int omap_correct_data(struct mtd_info *mtd, u_char *dat,
    				u_char *read_ecc, u_char *calc_ecc)
    {
    	struct omap_nand_info *info = container_of(mtd, struct omap_nand_info,
    							mtd);
    	int blockCnt = 0, i = 0, ret = 0;
    	int stat = 0;
    	int j, eccsize, eccflag, count;
    	unsigned int err_loc[8];
    
    	/* Ex NAND_ECC_HW12_2048 */
    	if ((info->nand.ecc.mode == NAND_ECC_HW) &&
    			(info->nand.ecc.size  == 2048))
    		blockCnt = 4;
    	else
    		blockCnt = 1;
    
    	switch (info->ecc_opt) {
    	case OMAP_ECC_HAMMING_CODE_HW:
    	case OMAP_ECC_HAMMING_CODE_HW_ROMCODE:
    		for (i = 0; i < blockCnt; i++) {
    			if (memcmp(read_ecc, calc_ecc, 3) != 0) {
    				ret = omap_compare_ecc(read_ecc, calc_ecc, dat);
    				if (ret < 0)
    					return ret;
    
    				/* keep track of number of corrected errors */
    				stat += ret;
    			}
    			read_ecc += 3;
    			calc_ecc += 3;
    			dat      += 512;
    		}
    		break;
    	case OMAP_ECC_BCH8_CODE_HW:
    		eccsize = BCH8_ECC_OOB_BYTES;
    
    		for (i = 0; i < blockCnt; i++) {
    			eccflag = 0;
    			/* check if area is flashed */
    			for (j = 0; (j < eccsize) && (eccflag == 0); j++)
    				if (read_ecc[j] != 0xFF)
    					eccflag = 1;
    
    			if (eccflag == 1) {
    				eccflag = 0;
    				/* check if any ecc error */
    				for (j = 0; (j < eccsize) && (eccflag == 0);
    						j++)
    					if (calc_ecc[j] != 0)
    						eccflag = 1;
    			}
    
    			count = 0;
    			if (eccflag == 1)
    				count  = omap_elm_decode_bch_error(0, calc_ecc,
    						err_loc);
    
    			for (j = 0; j < count; j++) {
    				u32 bit_pos, byte_pos;
    
    				bit_pos   = err_loc[j] % 8;
    				byte_pos  = (BCH8_ECC_MAX - err_loc[j] - 1) / 8;
    				if (err_loc[j] < BCH8_ECC_MAX)
    					dat[byte_pos] ^=
    							1 << bit_pos;
    				/* else, not interested to correct ecc */
    			}
    
    			stat     += count;
    			calc_ecc  = calc_ecc + OMAP_BCH8_ECC_SECT_BYTES;
    			read_ecc  = read_ecc + OMAP_BCH8_ECC_SECT_BYTES;
    			dat      += BCH8_ECC_BYTES;
    		}
    		break;
    	}
    	return stat;
    }
    
    /**
     * omap_calcuate_ecc - Generate non-inverted ECC bytes.
     * @mtd: MTD device structure
     * @dat: The pointer to data on which ecc is computed
     * @ecc_code: The ecc_code buffer
     *
     * Using noninverted ECC can be considered ugly since writing a blank
     * page ie. padding will clear the ECC bytes. This is no problem as long
     * nobody is trying to write data on the seemingly unused page. Reading
     * an erased page will produce an ECC mismatch between generated and read
     * ECC bytes that has to be dealt with separately.
     */
    static int omap_calculate_ecc(struct mtd_info *mtd, const u_char *dat,
    				u_char *ecc_code)
    {
    	struct omap_nand_info *info = container_of(mtd, struct omap_nand_info,
    							mtd);
    	return gpmc_calculate_ecc(info->ecc_opt, info->gpmc_cs, dat, ecc_code);
    }
    
    /**
     * omap_enable_hwecc - This function enables the hardware ecc functionality
     * @mtd: MTD device structure
     * @mode: Read/Write mode
     */
    static void omap_enable_hwecc(struct mtd_info *mtd, int mode)
    {
    	struct omap_nand_info *info = container_of(mtd, struct omap_nand_info,
    							mtd);
    	struct nand_chip *chip = mtd->priv;
    	unsigned int dev_width = (chip->options & NAND_BUSWIDTH_16) ? 1 : 0;
    
    	gpmc_enable_hwecc(info->ecc_opt, info->gpmc_cs, mode,
    				dev_width, info->nand.ecc.size);
    }
    
    /**
     * omap_wait - wait until the command is done
     * @mtd: MTD device structure
     * @chip: NAND Chip structure
     *
     * Wait function is called during Program and erase operations and
     * the way it is called from MTD layer, we should wait till the NAND
     * chip is ready after the programming/erase operation has completed.
     *
     * Erase can take up to 400ms and program up to 20ms according to
     * general NAND and SmartMedia specs
     */
    static int omap_wait(struct mtd_info *mtd, struct nand_chip *chip)
    {
    	struct nand_chip *this = mtd->priv;
    	struct omap_nand_info *info = container_of(mtd, struct omap_nand_info,
    							mtd);
    	unsigned long timeo = jiffies;
    	int status = NAND_STATUS_FAIL, state = this->state;
    
    	if (state == FL_ERASING)
    		timeo += (HZ * 400) / 1000;
    	else
    		timeo += (HZ * 20) / 1000;
    
    	gpmc_nand_write(info->gpmc_cs,
    			GPMC_NAND_COMMAND, (NAND_CMD_STATUS & 0xFF));
    	while (time_before(jiffies, timeo)) {
    		status = gpmc_nand_read(info->gpmc_cs, GPMC_NAND_DATA);
    		if (status & NAND_STATUS_READY)
    			break;
    		cond_resched();
    	}
    	return status;
    }
    
    /**
     * omap_dev_ready - calls the platform specific dev_ready function
     * @mtd: MTD device structure
     */
    static int omap_dev_ready(struct mtd_info *mtd)
    {
    	unsigned int val = 0;
    	struct omap_nand_info *info = container_of(mtd, struct omap_nand_info,
    							mtd);
    
    	val = gpmc_read_status(GPMC_GET_IRQ_STATUS);
    	if ((val & 0x100) == 0x100) {
    		/* Clear IRQ Interrupt */
    		val |= 0x100;
    		val &= ~(0x0);
    		gpmc_cs_configure(info->gpmc_cs, GPMC_SET_IRQ_STATUS, val);
    	} else {
    		unsigned int cnt = 0;
    		while (cnt++ < 0x1FF) {
    			if  ((val & 0x100) == 0x100)
    				return 0;
    			val = gpmc_read_status(GPMC_GET_IRQ_STATUS);
    		}
    	}
    
    	return 1;
    }
    
    static int __devinit omap_nand_probe(struct platform_device *pdev)
    {
    	struct omap_nand_info		*info;
    	struct omap_nand_platform_data	*pdata;
    	int				err;
    	int				i, offset;
    
    	pdata = pdev->dev.platform_data;
    	if (pdata == NULL) {
    		dev_err(&pdev->dev, "platform data missing\n");
    		return -ENODEV;
    	}
    
    	info = kzalloc(sizeof(struct omap_nand_info), GFP_KERNEL);
    	if (!info)
    		return -ENOMEM;
    
    	platform_set_drvdata(pdev, info);
    
    	spin_lock_init(&info->controller.lock);
    	init_waitqueue_head(&info->controller.wq);
    
    	info->pdev = pdev;
    
    	info->gpmc_cs		= pdata->cs;
    	info->phys_base		= pdata->phys_base;
    
    	info->mtd.priv		= &info->nand;
    	info->mtd.name		= dev_name(&pdev->dev);
    	info->mtd.owner		= THIS_MODULE;
    	info->ecc_opt		= pdata->ecc_opt;
    
    	info->nand.options	= pdata->devsize;
    	info->nand.options	|= NAND_SKIP_BBTSCAN;
    
    	/*
    	 * If ELM feature is used in OMAP NAND driver, then configure it
    	 */
    	if (pdata->elm_used) {
    		if (pdata->ecc_opt == OMAP_ECC_BCH8_CODE_HW)
    			omap_configure_elm(&info->mtd, OMAP_BCH8_ECC);
    	}
    
    	if (pdata->ctrlr_suspend)
    		info->ctrlr_suspend = pdata->ctrlr_suspend;
    	if (pdata->ctrlr_resume)
    		info->ctrlr_resume = pdata->ctrlr_resume;
    
    	/* NAND write protect off */
    	gpmc_cs_configure(info->gpmc_cs, GPMC_CONFIG_WP, 0);
    
    	if (!request_mem_region(info->phys_base, NAND_IO_SIZE,
    				pdev->dev.driver->name)) {
    		err = -EBUSY;
    		goto out_free_info;
    	}
    
    	info->nand.IO_ADDR_R = ioremap(info->phys_base, NAND_IO_SIZE);
    	if (!info->nand.IO_ADDR_R) {
    		err = -ENOMEM;
    		goto out_release_mem_region;
    	}
    
    	info->nand.controller = &info->controller;
    
    	info->nand.IO_ADDR_W = info->nand.IO_ADDR_R;
    	info->nand.cmd_ctrl  = omap_hwcontrol;
    
    	/*
    	 * If RDY/BSY line is connected to OMAP then use the omap ready
    	 * funcrtion and the generic nand_wait function which reads the status
    	 * register after monitoring the RDY/BSY line.Otherwise use a standard
    	 * chip delay which is slightly more than tR (AC Timing) of the NAND
    	 * device and read status register until you get a failure or success
    	 */
    	if (pdata->dev_ready) {
    		info->nand.dev_ready = omap_dev_ready;
    		info->nand.chip_delay = 0;
    	} else {
    		info->nand.waitfunc = omap_wait;
    		info->nand.chip_delay = 50;
    	}
    
    	switch (pdata->xfer_type) {
    	case NAND_OMAP_PREFETCH_POLLED:
    		info->nand.read_buf   = omap_read_buf_pref;
    		info->nand.write_buf  = omap_write_buf_pref;
    		break;
    
    	case NAND_OMAP_POLLED:
    		if (info->nand.options & NAND_BUSWIDTH_16) {
    			info->nand.read_buf   = omap_read_buf16;
    			info->nand.write_buf  = omap_write_buf16;
    		} else {
    			info->nand.read_buf   = omap_read_buf8;
    			info->nand.write_buf  = omap_write_buf8;
    		}
    		break;
    
    	case NAND_OMAP_PREFETCH_DMA:
    		err = omap_request_dma(OMAP24XX_DMA_GPMC, "NAND",
    				omap_nand_dma_cb, &info->comp, &info->dma_ch);
    		if (err < 0) {
    			info->dma_ch = -1;
    			dev_err(&pdev->dev, "DMA request failed!\n");
    			goto out_release_mem_region;
    		} else {
    			omap_set_dma_dest_burst_mode(info->dma_ch,
    					OMAP_DMA_DATA_BURST_16);
    			omap_set_dma_src_burst_mode(info->dma_ch,
    					OMAP_DMA_DATA_BURST_16);
    
    			info->nand.read_buf   = omap_read_buf_dma_pref;
    			info->nand.write_buf  = omap_write_buf_dma_pref;
    		}
    		break;
    
    	case NAND_OMAP_PREFETCH_IRQ:
    		err = request_irq(pdata->gpmc_irq,
    				omap_nand_irq, IRQF_SHARED, "gpmc-nand", info);
    		if (err) {
    			dev_err(&pdev->dev, "requesting irq(%d) error:%d",
    							pdata->gpmc_irq, err);
    			goto out_release_mem_region;
    		} else {
    			info->gpmc_irq	     = pdata->gpmc_irq;
    			info->nand.read_buf  = omap_read_buf_irq_pref;
    			info->nand.write_buf = omap_write_buf_irq_pref;
    		}
    		break;
    
    	default:
    		dev_err(&pdev->dev,
    			"xfer_type(%d) not supported!\n", pdata->xfer_type);
    		err = -EINVAL;
    		goto out_release_mem_region;
    	}
    
    	info->nand.verify_buf = omap_verify_buf;
    
    	/* selsect the ecc type */
    	if (pdata->ecc_opt == OMAP_ECC_HAMMING_CODE_DEFAULT)
    		info->nand.ecc.mode = NAND_ECC_SOFT;
    	else {
    		if (pdata->ecc_opt == OMAP_ECC_BCH4_CODE_HW) {
    			info->nand.ecc.bytes    = 4*7;
    			info->nand.ecc.size     = 4*512;
    		} else if (pdata->ecc_opt == OMAP_ECC_BCH8_CODE_HW) {
    			info->nand.ecc.bytes     = OMAP_BCH8_ECC_SECT_BYTES;
    			info->nand.ecc.size      = 512;
    			info->nand.ecc.read_page = omap_read_page_bch;
    		} else {
    			info->nand.ecc.bytes    = 3;
    			info->nand.ecc.size     = 512;
    		}
    
    		info->nand.ecc.calculate        = omap_calculate_ecc;
    		info->nand.ecc.hwctl            = omap_enable_hwecc;
    		info->nand.ecc.correct          = omap_correct_data;
    		info->nand.ecc.mode             = NAND_ECC_HW;
    	}
    
    	/* DIP switches on some boards change between 8 and 16 bit
    	 * bus widths for flash.  Try the other width if the first try fails.
    	 */
    
    	if (nand_scan_ident(&info->mtd, 1, NULL)) {
    		info->nand.options ^= NAND_BUSWIDTH_16;
    		if (nand_scan_ident(&info->mtd, 1, NULL)) {
    			err = -ENXIO;
    			goto out_release_mem_region;
    		}
    	}
    
    
    
    
    	/* select ecc lyout */
    	if (info->nand.ecc.mode != NAND_ECC_SOFT) {
    
    		if (!(info->nand.options & NAND_BUSWIDTH_16))
    			info->nand.badblock_pattern = &bb_descrip_flashbased;
    
    		offset = JFFS2_CLEAN_MARKER_OFFSET;
    
    		if (info->mtd.oobsize == 64)
    			omap_oobinfo.eccbytes = info->nand.ecc.bytes *
    						2048/info->nand.ecc.size;
    		else
    			omap_oobinfo.eccbytes = info->nand.ecc.bytes;
    
    		if (pdata->ecc_opt == OMAP_ECC_HAMMING_CODE_HW_ROMCODE) {
    			omap_oobinfo.oobfree->offset =
    						offset + omap_oobinfo.eccbytes;
    			omap_oobinfo.oobfree->length = info->mtd.oobsize -
    				(offset + omap_oobinfo.eccbytes);
    		} else if (pdata->ecc_opt == OMAP_ECC_BCH8_CODE_HW) {
    			offset = BCH_ECC_POS; /* Synchronize with U-boot */
    			omap_oobinfo.oobfree->offset =
    				BCH_JFFS2_CLEAN_MARKER_OFFSET;
    			omap_oobinfo.oobfree->length = info->mtd.oobsize -
    						offset - omap_oobinfo.eccbytes;
    		} else {
    			omap_oobinfo.oobfree->offset = offset;
    			omap_oobinfo.oobfree->length = info->mtd.oobsize -
    						offset - omap_oobinfo.eccbytes;
    			/*
    			offset is calculated considering the following :
    			1) 12 bytes ECC for 512 byte access and 24 bytes ECC for
    			256 byte access in OOB_64 can be supported
    			2)Ecc bytes lie to the end of OOB area.
    			3)Ecc layout must match with u-boot's ECC layout.
    			*/
    			offset = info->mtd.oobsize - MAX_HWECC_BYTES_OOB_64;
    		}
    
    		for (i = 0; i < omap_oobinfo.eccbytes; i++)
    			omap_oobinfo.eccpos[i] = i+offset;
    
    		info->nand.ecc.layout = &omap_oobinfo;
    	}
    //	omap_oobinfo.oobfree->length = 38;
    /*
    	pr_notice("%d,%d,%d,%d\n\n\n\n\n\n",
    				omap_oobinfo.eccbytes,
    				omap_oobinfo.oobfree->offset,
    				omap_oobinfo.oobfree->length,
    				omap_oobinfo.eccpos[0]);*/
    	/* second phase scan */
    	if (nand_scan_tail(&info->mtd)) {
    		err = -ENXIO;
    		goto out_release_mem_region;
    	}
    
    
    	mtd_device_parse_register(&info->mtd, NULL, 0,
    			pdata->parts, pdata->nr_parts);
    
    	platform_set_drvdata(pdev, &info->mtd);
    
    
    	return 0;
    
    out_release_mem_region:
    	release_mem_region(info->phys_base, NAND_IO_SIZE);
    out_free_info:
    	kfree(info);
    
    	return err;
    }
    
    static int omap_nand_remove(struct platform_device *pdev)
    {
    	struct mtd_info *mtd = platform_get_drvdata(pdev);
    	struct omap_nand_info *info = container_of(mtd, struct omap_nand_info,
    							mtd);
    
    	platform_set_drvdata(pdev, NULL);
    	if (info->dma_ch != -1)
    		omap_free_dma(info->dma_ch);
    
    	if (info->gpmc_irq)
    		free_irq(info->gpmc_irq, info);
    
    	/* Release NAND device, its internal structures and partitions */
    	nand_release(&info->mtd);
    	iounmap(info->nand.IO_ADDR_R);
    	release_mem_region(info->phys_base, NAND_IO_SIZE);
    	kfree(&info->mtd);
    	return 0;
    }
    
    #ifdef CONFIG_PM
    static int omap_nand_suspend(struct platform_device *pdev, pm_message_t state)
    {
    	struct mtd_info *mtd = platform_get_drvdata(pdev);
    	struct omap_nand_info *info = container_of(mtd, struct omap_nand_info,
    							mtd);
    
    	mtd->suspend(mtd);
    
    	if (info->ctrlr_suspend)
    		info->ctrlr_suspend();
    
    	return 0;
    }
    
    static int omap_nand_resume(struct platform_device *pdev)
    {
    	struct mtd_info *mtd = platform_get_drvdata(pdev);
    	struct omap_nand_info *info = container_of(mtd, struct omap_nand_info,
    							mtd);
    
    	if (info->ctrlr_resume)
    		info->ctrlr_resume();
    
    	return 0;
    }
    #endif
    
    static struct platform_driver omap_nand_driver = {
    	.probe		= omap_nand_probe,
    	.remove		= omap_nand_remove,
    #ifdef CONFIG_PM
    	.suspend	= omap_nand_suspend,
    	.resume		= omap_nand_resume,
    #endif
    	.driver		= {
    		.name	= DRIVER_NAME,
    		.owner	= THIS_MODULE,
    	},
    };
    
    static int __init omap_nand_init(void)
    {
    	pr_info("%s driver initializing\n", DRIVER_NAME);
    
    	return platform_driver_register(&omap_nand_driver);
    }
    
    static void __exit omap_nand_exit(void)
    {
    	platform_driver_unregister(&omap_nand_driver);
    }
    
    module_init(omap_nand_init);
    module_exit(omap_nand_exit);
    
    MODULE_ALIAS("platform:" DRIVER_NAME);
    MODULE_LICENSE("GPL");
    MODULE_DESCRIPTION("Glue layer for NAND flash on TI OMAP boards");
    

    nand driver from 3.2.0 kernel attached

  • I am looking into this. That 3.2 kernel is very old. Can you look at the latest SDK 04.02.00.09?

    Steve K.
  • Hi Steve

        thanks for the help.Please inform me once you have any updates.

        we maintain quite a number of products both new and old. Some run on 3.2.0 and a few run on 4.4.32 kernel.So it's not possible(not technically.but stratigically) for us to migrate to newer kernel....because there are so many products out there in customer's hands.

        Both 4.4.32 kernel and 3.2.0 kernel don't have the log regarding bbt when the kernel is starting up.I don't know if it's me that's configuring the kernel in a wrong way..? or it's the driver itself.

        But i do have the SDK relatively new with the version of 04.00.00.04.So i looked into it a little bit.

        And the code look like:

     if (info->flash_bbt)
      nand_chip->bbt_options |= NAND_BBT_USE_FLASH;

     normally.the nand driver will decide the info->flash_bbt value depending on the dts configuration.

    take mxc_nand.c for example:

    pdata->flash_bbt = of_get_nand_on_flash_bbt(np);

    above is where it can decide the flash_bbt  value and then enable the NAND_BBT_USE_FLASH.And then scan for the bbt and so on.

     and here is the weird part:

    in the sdk 04.00.00.04 kernel driver(actually it's basically the same as 4.4.32 kernel)

     omap_nand_probe()->omap_get_dt_info():

    next:
          of_get_nand_on_flash_bbt(child);

    yes it did called. But the return value of of_get_nand_on_flash_bbt is discarded.

    so i don't understand what's this mean here?

    Because we have 2 kinds of products using the different kernel.

    I will split the discussion here:

    1.Regarding 3.2.0 kernel:

    there's definication like:

    static struct nand_bbt_descr bb_descrip_flashbased = {
     .options = NAND_BBT_SCANEMPTY | NAND_BBT_SCANALLPAGES,
     .offs = 0,
     .len = 1,
     .pattern = scan_ff_pattern,
    };

    and in omap_nand_probe().Simply:

    info->nand.options |= NAND_SKIP_BBTSCAN;

    and did not look for any choice made in the platform_data. i guess.

    2.Regarding 4.4.32 kernel:

    it's much like the code in sdk 04.00.00.04

    next:
          of_get_nand_on_flash_bbt(child);

    did called. But the return value of of_get_nand_on_flash_bbt is discarded.

    So it seems that in the dts, there should be a declaration of nand-on-flash-bbt;

    but the am3354 driver did not actually read the return value of of_get_nand_on_flash_bbt(),which referring to whether "nand-on-flash-bbt;" is defined or not in the dts.

    also this "nand-on-flash-bbt;" is nowhere to be found in any am335x-***.dts files.

    I need to straighten it out for both 3.2.0 and 4.4.32 kernel.As it's important for us to make sure the nand flash is working in a correct way.

    thank you again and please get me posted!

    yan dong

  • could anyone help me please?

  • Yan Dong,

    Steve hasn't been able to look into this further at this point so I wanted to try to provide some feedback. I don't believe we utilized the Bad Block Table at this time in our drivers. We still use the older method of Bad Block Markers stored in the OOB area. I will reply back here if I learn differently.
  • Hi RonB:

        noted.

        i actually need a summery information about how many bad blocks in total are there right now in the nand flash.

        i guess i need to setup the bad block table by my own .Maybe put the table in the RAM . i guess.

        thank you for the feedback!

    yan dong

      

  • Yan Dong,

    I've confirmed that we don't use BBT in our NAND driver.

    Another idea you might find helpful is to consider the filesystem (e.g. UBIFS). It will usually have some way to keep up with bad blocks as well and might already build something like a BBT.
  • thanks RonB for the suggestion!