This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/PROCESSOR-SDK-AM437X: Custom board library project

Part Number: PROCESSOR-SDK-AM437X

Tool/software: TI-RTOS

Hi,

I need to create a custom board library.

I´ve followed the steps describe in processors.wiki.ti.com/.../Adding_Custom_Board_Library_Target_to_Processor_SDK_RTOS_makefiles but has not worked out. The instructions are not complete, as stated at the bottom of the page (Additional steps for AM335x/AM437x users).

There too many files to change, which can cause a little bit of stress if you have to reproduce the development envoriment in several machines.

I am wondering if I can create a CCS projet for the board library, or even incorporate the required files on my current project.

I beleive my board library project would be based on the folder 'board' at 'pdk_am437x_1_0_7\packages\ti\'. I think the libriaries are in c:\ti\pdk_am437x_1_0_7\packages\ti\board\lib\'

Do you see any problem with this solution? Is there any compiler/linker options different from a application project? Have you done it before?

There is another folder 'board' in 'pdk_am437x_1_0_7\packages\ti\starterware\'. It is where the pin mux files are. Why? Is it used in other parts of the software?


regards,
Marcio.