Part Number: TDA2EG
Other Parts Discussed in Thread: DS90UB964-Q1
Hi
In the Vision SDK usacases, the default video input interface is the VIP module(vin1a,1b...), which is a parallel interface. The "Single Channel Capture Use Case" and "Multi-channel LVDS 2D Surround view" usecases all use this interface.
But for the TDA2Ex soc, it also has the camera serial interface (CSI2, 6 DL) which is better than the traditional parallel interface VIP. So My question is how to use the CSI2 as the camera input in the Vision SDK usecase? (My custom board based on TDA2Ex has the "DS90UB964-Q1" to generate the CSI2 signal.)
Thanks
xuanbo