Other Parts Discussed in Thread: OMAP-L138
Hello,
I got a question on the OMAP-L138 DSP Core memory map, according to SPRS586J (OMAP-L138 data manual) chapter 3.5 Tabel 3-4 Top level Memory Map, at address 0x00700000 and 0x11700000 we have two segments which both are called DSP L2 ROM. It also happens to DSP L2 RAM, DSP L1D RAM and DSP L1P RAM. The only difference shown by the table is the DSP L2 ROM at 0x0070000 is only accessible by DSP, if I understand it correctly.
I am wondering what's the difference between DSP L2 ROM at 0x00700000 and 0x11700000? Is any of them accessible by the ARM core?
Regards,
Albert