Hi,
I would like to measure the ISR and IST interrupt delays on Windows Embedded Compact 7. I found that ILTiming tool in Platform Builder can be used for interrupt delay measurement on earlier version of Windows Embedded.(ex. CE 6.0, CE 5.0) Is this tool also enabled for Compact 7? If not, which tool can I use to measure ISR and IST delays? I'm using TMDS3530EVM as a target board.