Part Number: AM3352
Tool/software: Linux
Hi All,
we made a customized board with AM3352 processor, 1GB DDR3 and 8GB eMMC flash. we made u-boot.bin , MLO, zImage , beaglebone-black.dts and Filesystem. we can able to boot successfully boot this setup through SD Card. we have made partitions in eMMC flash as on SD card. we copied the MLO and u-boot.img in one partition as on SD Card and we can able to boot through eMMC Flash. But when we try to boot Linux through eMMC the bellow issue we are facing :
U-Boot SPL 2017.11-rc3-00022-g43ede0b-dirty (Nov 07 2017 - 13:14:21)
Trying to boot from MMC2
*** Warning - bad CRC, using default environment
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2017.01-00319-geae4602-dirty (Feb 06 2018 - 14:18:47 +0530)
CPU : AM3352
NIOT - IMSS
DRAM: 1 GiB
WARNING: Caches not enabled
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Error - No Valid Environment Area found
*** Warning - bad CRC, using default environment
In: serial@44e09000
Out: serial@44e09000
Err: serial@44e09000
<ethaddr> not set. Validating first E-fuse MAC
Net: Enabling MII Mode ....Done.
i = 5
Detected PHY ID = 0x221450
Phy ID = 0x221450
cpsw connected to Generic PHY
cpsw
Hit any key to stop autoboot: 0
MMC: no card present
MMC: no card present
MMC: no card present
MMC: no card present
MMC: no card present
MMC: no card present
## Error: "bootcmd_nand0" not defined
starting USB...
USB0: Port not available.
*** mii_reg = 0x7808
mac_control = 0x8021
link up on port 0, speed 100, full duplex
MAC Control = 0x8021
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
BOOTP broadcast 5
BOOTP broadcast 6
BOOTP broadcast 7
BOOTP broadcast 8
BOOTP broadcast 9
BOOTP broadcast 10
BOOTP broadcast 11
BOOTP broadcast 12
BOOTP broadcast 13
we are suspecting it can be due to boot args ? Can any one provide any ideas to resolve this issue ? As it is an urgent one .
Thanks in Advance.
Regards,
Avinash N