Tool/software: TI-RTOS
Hello,
I have created usecase as,
UseCase: chains_test52
Capture -> Dup
Dup -> Alg_FrameDifference(DSP1) -> Alg_DrawBlob(IPU1_1)
Dup -> Alg_DrawBlob -> Display
Note:-
1. The algplugin "Alg_DrawBlob" is receiving input from two queues ( one is Dup link and another is Alg_FrameDifference), and gives output one queue.
2. Alg_FrameDifference and Alg_DrawBlob links are working fine.(without Dup link in single pipeline)
3. Sdk configuration: PROCESSOR_SDK_VISION_03_00_00_00, SYS-BIOS
So problem is,
1st frame is getting processed completely .
But after 1st frame, data/frame is not getting from "Dup" link.
( One frame meaning that , create params for "Alg_FrameDifference" is noOfOutFrames and I have set it as 1)
Do you have any pointer to this issue?
Regards,
Kajal Karande.