Part Number: TMS320DM8127
Using IPNC_RDK_3.8.0 with AR0331 sensor.
I realized that in our proprietary usecase (based on the multichannel_triStream usecase) the WDR-link was not included.
When I inserted the link into the usecase (between the CameraLink and VNF-Link (is this the right place?), the program stopped on an assertion that the CameraLink outputs SYSTEM_DF_YUV420SP_UV and the WDR_Link needs FVID2_DF_BAYER_RAW as input. Is this true? Is this really what the CameraLink outputs?
I'm a bit confused, since in IPNC_RDK_V3.8.0/Source/ipnc_rdk/ipnc_mcfw/mcfw/src_bios6/links_m3vpss/camera/cameraLink_drv.c I print out the videoDataFormat (pInst->sensorVideoModeArgs.videoDataFormat)
and it's 0x3000 (12288) or SYSTEM_DF_BAYER_RAW.
Also, when I capture a RAW frame using the DCC tool, I get Bayer 12-bit.
I do know that the input to the DSP for Video Analytics is in YUV420 format (after the VNF link) - when does this format change? In which link?
Thanks for any ideas.
Mechi