Part Number: AM5728
Tool/software: Linux
I need to composite 2 DMABUFs captured from 2 different VIP ports on the AM5728. I am using the ti-gc320-tests git repository and the Vivante GC320 PDF documentation as examples.
So far, I can feed DMABUFs from the VIPs into the GC320 and successfully do things like Pixel Format Conversion, Scaling, and Rotation. What I need to do now is compositing.
Specifically, I am studying the example code in:
ti-gc320-test/tests/src/test/hal/common/UnitTest/units/gal2D/MultiSourceBlitRotation/101/101.c
When I implement this code into my existing test application, I always get the error: "gcvSTATUS_NOT_SUPPORTED" when I call gco2D_MultiSourceBlit. Here is the function in my test application:
/**
* gc320 renderCompositedFrames()
* Purpose: Perform a render cycle for compositing 2 input rames together
*
* @param inputBuffer1 - DMABUF type input buffer
* @param DMABUF type input buffer
*
* @return inputBuffer2 - Return bool success or failure
*/
gctBOOL Gc320::renderCompositedFrames(dmabuf_buffer *inputBuffer1, dmabuf_buffer *inputBuffer2) {
gceSTATUS status;
// Destination Rectangle
gcsRECT targetRect;
gcsRECT sourceVLRect;
gcsRECT sourceIRRect;
// Destination Rectangle
targetRect.left = 0;
targetRect.top = 0;
targetRect.right = FRAME_WIDTH; // These affect the output image ( destination rect )
targetRect.bottom = FRAME_HEIGHT; // These affect the output image ( destination rect )
// VL Source Rectangle
sourceVLRect.left = 0;
sourceVLRect.top = 0;
sourceVLRect.right = FRAME_WIDTH; // These affect the input image ( source rect )
sourceVLRect.bottom = FRAME_HEIGHT; // These affect the input image ( source rect )
// IR Source Rectangle
sourceIRRect.left = 0;
sourceIRRect.top = 0;
sourceIRRect.right = FRAME_WIDTH; // These affect the input image ( source rect )
sourceIRRect.bottom = FRAME_HEIGHT; // These affect the input image ( source rect )
// Set the underlying buffer for VL
void *VLDataPtr = omap_bo_map(inputBuffer1->bo[0]); // mmap the DMABUF
configureYuYvSourceSurfaceForVL(VLDataPtr);
// Set the underlying buffer for IR
void *IRDataPtr = omap_bo_map(inputBuffer2->bo[0]); // mmap the DMABUF
configureYuYvSourceSurfaceForIR(IRDataPtr);
// clear dest temp with grey color
gcmONERROR(Gal2DCleanSurface(m_Hal, m_TempDstSurf, COLOR_ARGB8(0x00, 0x80, 0x80, 0x80)));
// Index 1 for VL and index 2 for IR
////////////////////// VL //////////////////////////////////////////
gcmONERROR(gco2D_SetCurrentSourceIndex(m_Engine2d, 0));
gcmONERROR(gco2D_SetGenericSource(
m_Engine2d,
(gctUINT32_PTR)&m_VLSrcVirtAddr, 1,
(gctUINT32_PTR)&m_VLSrcStride, 1,
gcvLINEAR,
m_VLSrcFormat,
gcvSURF_0_DEGREE,
(gctUINT32)inputBuffer1->width,
(gctUINT32)inputBuffer1->height));
gcmONERROR(gco2D_SetSource(m_Engine2d, &sourceVLRect));
gcmONERROR(gco2D_SetROP(m_Engine2d, 0xCC, 0xCC));
// disable mirror
gcmONERROR(gco2D_SetBitBlitMirror(m_Engine2d, gcvFALSE, gcvFALSE));
////////////////////// IR //////////////////////////////////////////
gcmONERROR(gco2D_SetCurrentSourceIndex(m_Engine2d, 1));
gcmONERROR(gco2D_SetGenericSource(
m_Engine2d,
(gctUINT32_PTR)&m_IRSrcVirtAddr, 1,
(gctUINT32_PTR)&m_IRSrcStride, 1,
gcvLINEAR,
m_IRSrcFormat,
gcvSURF_0_DEGREE,
(gctUINT32)inputBuffer2->width,
(gctUINT32)inputBuffer2->height));
gcmONERROR(gco2D_SetSource(m_Engine2d, &sourceIRRect));
gcmONERROR(gco2D_SetROP(m_Engine2d, 0xCC, 0xCC));
// disable mirror
gcmONERROR(gco2D_SetBitBlitMirror(m_Engine2d, gcvFALSE, gcvFALSE));
////////////////////////////////////////////////////////////////////
// disable mirror
gcmONERROR(gco2D_SetBitBlitMirror(m_Engine2d, gcvFALSE, gcvFALSE));
gcmONERROR(gco2D_SetClipping(m_Engine2d, &targetRect));
gcmONERROR(gco2D_SetGenericTarget(
m_Engine2d,
(gctUINT32_PTR)&m_TempDstPhysAddr, 1,
(gctUINT32_PTR)&m_TempDstStride, 1,
gcvLINEAR,
m_TempDstFormat,
gcvSURF_0_DEGREE,
m_TempDstWidth,
m_TempDstHeight));
gcmONERROR(gco2D_MultiSourceBlit(m_Engine2d, 0xF, &targetRect, 1));
// disable mirror
gcmONERROR(gco2D_SetBitBlitMirror(m_Engine2d, gcvFALSE, gcvFALSE));
gcmONERROR(gco2D_Flush(m_Engine2d));
/* draw result to display surface. */
gcmONERROR(gco2D_SetGenericSource(
m_Engine2d,
(gctUINT32_PTR)&m_TempDstPhysAddr, 1,
(gctUINT32_PTR)&m_TempDstStride, 1,
gcvLINEAR,
m_TempDstFormat,
gcvSURF_0_DEGREE,
m_TempDstWidth,
m_TempDstHeight));
gcmONERROR(gco2D_SetSource(m_Engine2d, &targetRect));
gcmONERROR(gco2D_SetGenericTarget(
m_Engine2d,
(gctUINT32_PTR)&m_TempDstPhysAddr, 1,
(gctUINT32_PTR)&m_TempDstStride, 1,
gcvLINEAR,
m_TempDstFormat,
gcvSURF_0_DEGREE,
m_TempDstWidth,
m_TempDstHeight));
gcmONERROR(gco2D_SetStretchRectFactors(
m_Engine2d,
&targetRect,
&targetRect
));
gcmONERROR(gco2D_StretchBlit(
m_Engine2d,
1,
&targetRect,
0xCC, 0xCC,
m_DstFormat
));
gcmONERROR(gco2D_Flush(m_Engine2d));
gcmONERROR(gcoHAL_Commit(m_Hal, gcvTRUE));
return gcvTRUE;
OnError:
fprintf(stderr,"%s(%d) failed:%s\n",__FUNCTION__, __LINE__, gcoOS_DebugStatus2Name(status));
return gcvFALSE;
}
Is multisource blitting not supported? If it is, what is wrong with the code above? Thank you for the support.
The documentation states that it is supported:
Linux Kernel Version:
uname -r 4.4.41
GAL Version:
GC320 IRQ: 304 Galcore version 5.0.11.33433
GC320 IRQ: 304
[318156.999191] Galcore version 5.0.11.33433