This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDSLCDK6748: requesting compiler for ccs

Part Number: TMDSLCDK6748
Other Parts Discussed in Thread: OMAP-L138

Tool/software: Code Composer Studio

I bought OMAP-L138 LCDK two years back for my DSP class, using CCSv6.1.1. Had bad experience. some boards work some do not, boards get into reset modes and do not come out. very very flickry.

Now I find that you have new CCS v7.4. I have downloaded but I need the support files, Legacy COFF or relevant files, I also need a full seetings and code for an example of blinking LED or generating a sinewave project.

Please provide guidance.

Prof. Jai P Agrawal

agrawajp@pnw.edu

  • Hello,

    Processor SDK is our latest supported software offering for OMAP-L138:

    Driver examples can be found within the PDK, and need to be built using scripts, refer to the following wiki for details on this.

    For documentation, you may refer to: