This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TCIEVMK2X: Error while building processor sdk

Part Number: TCIEVMK2X

Tool/software: Linux

Hi ,I am taking following link as reference to build Processor SDK

http://processors.wiki.ti.com/index.php/Processor_SDK_Building_The_SDK

But i am getting following error after the command

MACHINE=k2hk-evm bitbake arago-core-tisdk-image

WARNING: hevc-arm-decoder-01.00.00.01-r3 do_fetch: Failed to fetch URL gforge.ti.com/.../REL.HEVC.D.ARM.OBJ.01.00.00.01.tar.gz, attempting MIRRORS if available
ERROR: hevc-arm-decoder-01.00.00.01-r3 do_fetch: Fetcher failure: Fetch command export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-DcFrvfrc4h"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/oe-core/scripts:/home/administrator/ti_TCI_yocto_BSP/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin/arm-linux-gnueabi:/home/administrator/ti_TCI_yocto_BSP/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/k2hk-evm/usr/bin/crossscripts:/home/administrator/ti_TCI_yocto_BSP/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/sbin:/home/administrator/ti_TCI_yocto_BSP/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/administrator/ti_TCI_yocto_BSP/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/sbin:/home/administrator/ti_TCI_yocto_BSP/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/bin:/home/administrator/gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf/bin:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/meta-ros/scripts:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/meta-browser/scripts:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/oe-core/scripts:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/bitbake/bin:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/meta-ros/scripts:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/meta-browser/scripts:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/oe-core/scripts:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/bitbake/bin:/home/administrator/gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf/bin:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/meta-ros/scripts:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/meta-browser/scripts:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/oe-core/scripts:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/bitbake/bin:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/meta-ros/scripts:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/meta-browser/scripts:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/oe-core/scripts:/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/bitbake/bin:/home/administrator/gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf/bin:/home/administrator/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games:/snap/bin"; export HOME="/home/administrator"; /usr/bin/env wget -t 2 -T 30 -nv --passive-ftp --no-check-certificate -P /home/administrator/ti_TCI_yocto_BSP/tisdk/downloads 'gforge.ti.com/.../REL.HEVC.D.ARM.OBJ.01.00.00.01.tar.gz' --progress=dot -v failed with exit code 4, output:
--2018-02-07 10:00:33--  gforge.ti.com/.../REL.HEVC.D.ARM.OBJ.01.00.00.01.tar.gz
Resolving gforge.ti.com (gforge.ti.com)... 174.143.205.12
Connecting to gforge.ti.com (gforge.ti.com)|174.143.205.12|:443... failed: Connection timed out.
Retrying.

--2018-02-07 10:01:05--  (try: 2)  gforge.ti.com/.../REL.HEVC.D.ARM.OBJ.01.00.00.01.tar.gz
Connecting to gforge.ti.com (gforge.ti.com)|174.143.205.12|:443... failed: Connection timed out.
Giving up.


ERROR: hevc-arm-decoder-01.00.00.01-r3 do_fetch: Fetcher failure for URL: 'gforge.ti.com/.../REL.HEVC.D.ARM.OBJ.01.00.00.01.tar.gz'. Unable to fetch URL from any source.
ERROR: hevc-arm-decoder-01.00.00.01-r3 do_fetch: Function failed: base_do_fetch
ERROR: Logfile of failure stored in: /home/administrator/ti_TCI_yocto_BSP/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/hevc-arm-decoder/01.00.00.01-r3/temp/log.do_fetch.24423
ERROR: Task (/home/administrator/ti_TCI_yocto_BSP/tisdk/sources/meta-arago/meta-arago-extras/recipes-multimedia/hevc-arm-decoder/hevc-arm-decoder_01.00.00.01.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2923 tasks of which 2914 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
  /home/administrator/ti_TCI_yocto_BSP/tisdk/sources/meta-arago/meta-arago-extras/recipes-multimedia/hevc-arm-decoder/hevc-arm-decoder_01.00.00.01.bb:do_fetch


Please resolve the issue

Regards
Sameer

  • HI, Sameer,

    Fetch error usually happens when the url becomes obsolete or other reasons. When user uses the Processor SDK, it has been a few months since the process of releasing it. The open source URLs has been moving to new versions during this period of time. I suggest you to use the snapshot approach as described in section 3.3 of the guide. Give it a try if that wasn't the way you built the image and see if that works for you.

    Rex
  • Hi, Sameer,

    I have not seen you respond to this thread and assume it worked for you using snapshot. Please click "Resolved" button if that is the case. Thanks!

    Rex