Other Parts Discussed in Thread: MATHLIB, CCSTUDIO
Tool/software: TI-RTOS
Hi
We use pdkProjectCreate to output the project exampls from pdk_am57xx_1_0_7 ,there is a problem and can not create the project we want . the list is as follows:
C:\Users\HePu-He>C:\ti\pdk_am57xx_1_0_7\packages\pdksetupenv.bat
Optional parameter not configured : CG_XML_BIN_INSTALL_PATH
REQUIRED for xdc release build
Example: set CG_XML_BIN_INSTALL_PATH=C:/ti/cg_xml/bin
Optional parameter not configured : DOXYGEN_INSTALL_PATH
REQUIRED for xdc release build
Example: set DOXYGEN_INSTALL_PATH=C:/ti/Doxygen/doxygen/1.5.1-p1/bin
**************************************************************************
Environment Configuration:
LIMIT_SOCS : am571x am572x
LIMIT_BOARDS : evmAM572x idkAM571x idkAM572x
PDK_INSTALL_PATH : /ti/PDK_AM~2/packages
C6X_GEN_INSTALL_PATH : C:/ti/ti-cgt-c6000_8.1.3
TOOLCHAIN_PATH_GCC : C:/ti/gcc-arm-none-eabi-4_9-2015q3
TOOLCHAIN_PATH_A15 : C:/ti/gcc-arm-none-eabi-4_9-2015q3
TOOLCHAIN_PATH_A8 : C:/ti/gcc-arm-none-eabi-4_9-2015q3
TOOLCHAIN_PATH_A9 : C:/ti/gcc-arm-none-eabi-4_9-2015q3
TOOLCHAIN_PATH_M4 : C:/ti/ti-cgt-arm_16.9.2.LTS
TOOLCHAIN_PATH_Arm9 : C:/ti/ti-cgt-arm_16.9.2.LTS
TOOLCHAIN_PATH_EVE : C:/ti/arp32_1.0.8
CL_PRU_INSTALL_PATH : C:/ti/ti-cgt-pru_2.1.5
UTILS_INSTALL_DIR : C:/ti/xdctools_3_32_01_22_core/bin
FPULIB_PATH : C:/ti/gcc-arm-none-eabi-4_9-2015q3/lib/gcc/arm-none-eabi/4.9.3/fpu
CROSS_TOOL_PRFX : arm-none-eabi-
XDC_INSTALL_PATH : C:/ti/xdctools_3_32_01_22_core
BIOS_INSTALL_PATH : C:/ti/bios_6_46_05_55
IPC_INSTALL_PATH : C:/ti/ipc_3_46_00_02
EDMA3LLD_BIOS6_INSTALLDIR : C:/ti/edma3_lld_2_12_04_28
NDK_INSTALL_PATH : C:/ti/ndk_2_25_01_11
IMGLIB_INSTALL_PATH : C:/ti/imglib_c66x_3_1_1_0
DSPLIB_INSTALL_PATH : C:/ti/dsplib_c66x_3_4_0_0
MATHLIB_INSTALL_PATH : C:/ti/mathlib_c66x_3_1_1_0
UIA_INSTALL_PATH : C:/ti/uia_2_00_06_52
**************************************************************************
Changing to short name to support directory names containing spaces
current directory: /ti/PDK_AM~2/packages
PDK BUILD ENVIRONMENT CONFIGURED
**************************************************************************
C:\ti\PDK_AM~2\packages>pdkProjectCreate AM571x evmAM571x little mcasp dsp
=========================================================================
Configuration:
SOC : AM571x
BOARD : evmAM571x
ENDIAN : little
MODULE : mcasp
PROCESSOR : dsp
PDK_SHORT_NAME : C:\ti\PDK_AM~2\packages\
=========================================================================
Checking Configuration...
Complete
=========================================================================
PDK_PARTNO : AM571X
PDK_ECLIPSE_ID : com.ti.pdk.am57xx
RTSC_PLATFORM_NAME : ti.platforms.idkAM571X
RTSC_TARGET : ti.targets.elf.C66
CCS_DEVICE : "com.ti.ccstudio.deviceModel.C6000.GenericC64xPlusDevice"
*****************************************************************************
Detecting all projects in PDK and importing them in the workspace C:\ti\PDK_AM~2\packages\\MyExampleProjects
找不到文件
No projects detected
Project generation complete
*****************************************************************************
C:\ti\PDK_AM~2\packages>
We do not know what is the problem and how to make them correct ? Thank you for your help!