Part Number: AM3352
hi,
I Use AM335X to match NOR flash have some problems.
We use the AM335X EVM board, connect the external NOR flash, it cold start to run the boot and app in nor flash. (we do not run the system)
The problem now is that when the chip is re powered, system boot is configured as "11000",but AM335X is not read successfully through SPI0 to NOR flash.
But when the hot started, boot and app are burned to NOR flash, which can be started by flash
What is the amount of data that AM335X reads to NOR flash when the hot starts up, and is a block of the flash? Or how many K byte
Does TI's AM335X EVM board support access to NOR flash via SPI0?
thanks.