Part Number: TMDSICE3359
Hi,
- Am using TMDSICE3359 evaluation board loaded with Profinet RT stack provided by TI.
- To validate the device for PNIO certification I am running AutomatedRtTester_v2.34.0.4_RC software from PNIO test bundle (2017-04-05_PN-test).
- Some of the tests like "Pdev_Records, Pdev_checkoneport, DCP-DCP_Router, DCP-DCP_OPTIONS_SUBOPTIONS, DCP-DCP_2" are FAILED.
- So I would like to know what shall I do to make it PASS?.
- Am using GSDML-V2.33-MOLEX_TI-AM335x_RT-MRP-20170904.xml GSDML file.
- Is there any GSDML file available which is already tested and cleared ? Is there any Profinet RT certification test report available?
- Is there any GSDML file available for single port device ? Or for single port what changes need to be done in the existing GSDML file ?
Kindly give suggestions for all my queries since am new to this environment not able to move further.
Regards,
Subeesh