This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3359: Large EtherCAT frame handling

Part Number: AM3359

On behalf of customer:

 

Question:

Can PRU-ICSS handle divided frame that over than 1514Byte?

 

Background:

It seems that when access of one Synch Manager of one Slave be divided as 2 frame, then physical address of 2nd frame access are used same address of 1st frame access.  In other words, those divided 2 frame cannot be access correctly.

 

If SM3 Inputs=2048Byte, EtherCAT Master divide SM3 Inputs=2048Byte into 2 frame of 934Byte and 1114Byte, because of not to exceed MTU(1514Byte).  In this situation, the customer expect 2nd Frame have offset=934 in physical memory, however, in fact, 2nd frame have offset=0.

 

Best regards,

Gou