Other Parts Discussed in Thread: TMS320DM8127
Dear all,
The compyny I working on is interested in DM8127 processor for further products. We a looking now at TMS320DM8127 Camera Starter Kit for first developing tests.
We are very interesting in latency reduction in the following chain: Camera --> ISP --> Encoder --> Network --> Decoder --> Display
According to http://www.ti.com/lit/wp/spry301/spry301.pdf there are low latency FPV Drone applications possible, if we would split each frame in slices.
In particular example the latency reduction is up to factor 3 (from 120 ms to 40 ms).
Therefore following questions to this publications and especially to DM8127:
- Does DM8127 supports frame slice encoding?
- Which developing software do we need for slice encoding and does it included in TMS320DM8127 Camera Starter Kit?
- Can the produced bitstream be decoded on other devices than DM8127 and under what conformity conditions?
- Under frame in to slices splitting condition: Will be the encoding Interlaced or Progressive?
- Are the any real tests for TMS320DM8127 Camera Starter Kit or comparable system with latency information provided?
Many thanks,
Alex