Part Number: TMDSLCDK138
Other Parts Discussed in Thread: OMAP-L138
Tool/software: Linux
Hi,
I was able boot the board with sd card. but when i try to boot now the following will happen,
I2C: ready
DRAM: 128 MiB
WARNING: Caches not enabled
NAND: 512 MiB
MMC: davinci: 0
In: serial
Out: serial
Err: serial
Invalid MAC address read.
Net: DaVinci-EMAC
Warning: DaVinci-EMAC (eth0) using random MAC address - 6a:c2:e0:61:ba:87
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
** Unable to read file uEnv.txt **
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
** File not found /boot/zImage **
=>
I can boot up another board with same SD card.
what is the problem?
Regards
Allwyn