Part Number: TDA2EVM5777
Other Parts Discussed in Thread: TDA2SX
Tool/software: Linux
Hello,
Is there example Linux software for a PCIe echo application running on TDA2x Linux which has the PCIe module configured as the default PCIe RC device? I am running PROCESSOR_SDK_VISION_03_01_00_00 linux on the tda2evm5777 Vayu EVM.
I want to connect the Vayu EVM to a PCIe End Point device. The PCIe End Point device is running as a PCIe EP device with an echo application. The Vision SDK prebuilt Linux TDA2x on Vayu EVM detects the external PCIe EP device but I do not know how to transmit data so that I can and receive the echo from that device. How can I echo out to the PCIe device and listen for the return?
Thank you for your help. I have not been able to find any documentation on how to test Linux PCIe RC comms to an EP device. I only find documentation on how to test Linux End Point Connection, but not Root Complex. I am following the documentation under: PROCESSOR_SDK_VISION_03_01_00_00/ti_components/os_tools/linux/kernel/omap/Documentation/PCI...