Part Number: TMDXEVM3358
Tool/software: Code Composer Studio
Hello,
I am unable to boot AM335x EVM board with SD card.
I have used starterware library as base and modified it as per my requirement.
I am renaming 'boot_ti.bin' of MMCSD release to 'MLO' and 'buzzerBeep_ti.bin' to 'app'.
I have formated SD card with FAT file system and copied both the files MLO and app in root.
After safely ejecting SD card from PC i have plugged it in EVM board and turned it on.
There is not any messages appearing on UART on power up and even after some time.
Also there is no sign of execution of my program.
Below is the SYSBOOTSW status :
SYSBOOT[7:0] = 0001 0111
SYSBOOT[15:8] = 0100 0000
EVM board is in profile 2.
With same settings if I copy default files which were present in SD card when I purchased EVM board, I can see booting U-boot on UART and LCD is also displaying some icons.
As per my observation there is an issue with .bin files but I can not figure out what exactly is the issue.
Please help.
Thank you in advance.