This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/IPNC-RDK-CSK: DM38x Timer and PWM functionality

Part Number: IPNC-RDK-CSK

Tool/software: Linux

I am trying to get PWM output on the TIMX_IO pins, but there doesn't seem to be a PWM driver in the IPNC RDK. In addition it looks like only timer1 and timer2 are defined in the ti81xx.dtsi, which is referenced in the dm38x-csk.dts file. Is this observation incorrect, or should I be able to add a pwm such that it shows up in /sys/class/pwm and controlled as described here:  processors.wiki.ti.com/.../Linux_Core_PWM_User's_Guide