This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kernel not getting up



Hi everybody.

Sometimes, when I boot my board (hawkboard) with standard u-boot and kernel, the booting process on the board stops at this point:

## Booting kernel from Legacy Image at c0700000 ...
   Image Name:   Linux-2.6.32-rc6
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1939152 Bytes =  1.8 MB
   Load Address: c0008000
   Entry Point:  c0008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

After few search, I found out that the kernel stops in the fonction stext of head.S file ($(LINUX_SOURCE_DIR)/arch/arm/kernel). Because the booting process randomly stops, I don't manage to find why sometimes it stops in this function. Is anyone have an idea about it?
ps: I'm using Linux kernel 2.6.32

Thanks in advance
Armand